A 5-way joystick (left, right, up, down, press) interface using 5 GPIOs.
Functions | |
static __always_inline int | is_joystick_down (void) |
This function test it the joystick is down. More... | |
static __always_inline int | is_joystick_left (void) |
This function test it the joystick is on the left. More... | |
static __always_inline int | is_joystick_pressed (void) |
This function test it the joystick is pressed. More... | |
static __always_inline int | is_joystick_right (void) |
This function test it the joystick is on the right. More... | |
static __always_inline int | is_joystick_up (void) |
This function test it the joystick is up. More... | |
|
static |
This function test it the joystick is down.
true
if the joystick is down, otherwise 0
. References gpio_get_pin_value(), GPIO_JOYSTICK_DOWN, and GPIO_JOYSTICK_DOWN_PRESSED.
Referenced by is_usb_mouse_event().
|
static |
This function test it the joystick is on the left.
true
if the joystick is on the left, otherwise 0
. References gpio_get_pin_value(), GPIO_JOYSTICK_LEFT, and GPIO_JOYSTICK_LEFT_PRESSED.
Referenced by is_usb_mouse_event().
|
static |
This function test it the joystick is pressed.
true
if the joystick is pressed, otherwise 0
. References gpio_get_pin_value(), GPIO_JOYSTICK_PUSH, and GPIO_JOYSTICK_PUSH_PRESSED.
Referenced by is_usb_mouse_event().
|
static |
This function test it the joystick is on the right.
true
if the joystick is on the right, otherwise 0
. References gpio_get_pin_value(), GPIO_JOYSTICK_RIGHT, and GPIO_JOYSTICK_RIGHT_PRESSED.
Referenced by is_usb_mouse_event().
|
static |
This function test it the joystick is up.
true
if the joystick is up, otherwise 0
. References gpio_get_pin_value(), GPIO_JOYSTICK_UP, and GPIO_JOYSTICK_UP_PRESSED.
Referenced by is_usb_mouse_event().