USB Device Descriptor.
#include <usb_descriptors.h>
Data Fields | |
uint16_t | bcdDevice |
Device release number. More... | |
uint8_t | bDescriptorType |
DEVICE descriptor type. More... | |
uint8_t | bDeviceClass |
Class code assigned by the USB. More... | |
uint8_t | bDeviceProtocol |
Protocol code assigned by the USB. More... | |
uint8_t | bDeviceSubClass |
Subclass code assigned by the USB. More... | |
uint8_t | bLength |
Size of this descriptor in bytes. More... | |
uint8_t | bMaxPacketSize0 |
Max packet size for EP0. More... | |
uint8_t | bNumConfigurations |
Number of possible configurations. More... | |
uint16_t | bscUSB |
Binary Coded Decimal Spec. release. More... | |
uint16_t | idProduct |
Product ID assigned by the manufacturer. More... | |
uint16_t | idVendor |
Vendor ID. ATMEL = 0x03EB. More... | |
uint8_t | iManufacturer |
Index of manufacturer string descriptor. More... | |
uint8_t | iProduct |
Index of product string descriptor. More... | |
uint8_t | iSerialNumber |
Index of serial string descriptor. More... | |
uint16_t S_usb_device_descriptor::bcdDevice |
Device release number.
uint8_t S_usb_device_descriptor::bDescriptorType |
DEVICE descriptor type.
uint8_t S_usb_device_descriptor::bDeviceClass |
Class code assigned by the USB.
uint8_t S_usb_device_descriptor::bDeviceProtocol |
Protocol code assigned by the USB.
uint8_t S_usb_device_descriptor::bDeviceSubClass |
Subclass code assigned by the USB.
uint8_t S_usb_device_descriptor::bLength |
Size of this descriptor in bytes.
uint8_t S_usb_device_descriptor::bMaxPacketSize0 |
Max packet size for EP0.
uint8_t S_usb_device_descriptor::bNumConfigurations |
Number of possible configurations.
uint16_t S_usb_device_descriptor::bscUSB |
Binary Coded Decimal Spec. release.
uint16_t S_usb_device_descriptor::idProduct |
Product ID assigned by the manufacturer.
uint16_t S_usb_device_descriptor::idVendor |
Vendor ID. ATMEL = 0x03EB.
uint8_t S_usb_device_descriptor::iManufacturer |
Index of manufacturer string descriptor.
uint8_t S_usb_device_descriptor::iProduct |
Index of product string descriptor.
uint8_t S_usb_device_descriptor::iSerialNumber |
Index of serial string descriptor.