Graphic Widget Toolkit library example application.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | MAXTOUCH_TWI_ADDRESS 0x4a |
Address of the mXT143E on TWI bus. More... | |
Functions | |
int | main (void) |
Main application function. More... | |
static void | mxt_init (struct mxt_device *device) |
Set maXTouch configuration. More... | |
static bool | read_touch_event (struct mxt_device *device, struct win_pointer_event *win_touch_event) |
Convert touch events from the touchscreen into window pointer events. More... | |
static void | setup_gui_root_window (void) |
Configure the root GUI window. More... | |
static void | show_out_of_memory_error (void) |
Show an out of memory error on the display. More... | |
#define MAXTOUCH_TWI_ADDRESS 0x4a |
Address of the mXT143E on TWI bus.
Referenced by mxt_init().
int main | ( | void | ) |
Main application function.
This function calls all the necessary initialization functions before launching the calculator widget and entering the main work loop.
The main work loop is responsible for handling the low level user input, so it reads touch data from the mXT143E Xplained, translates and passes it on to the window system's event queue.
All the processing for the calculator is done by the calculator widget's event handler function app_calc_handler(). This function is called by the window system when it maps a user input event to an interaction with the calculator, i.e., a button press.
References app_widget_launch(), board_init(), gfx_init, membag_init(), mxt_init(), read_touch_event(), setup_gui_root_window(), show_out_of_memory_error(), sysclk_init(), win_init(), win_process_events(), win_queue_pointer_event(), and win_reset_root_geometry().
|
static |
Set maXTouch configuration.
This function writes a set of predefined, optimal maXTouch configuration data to the mXT143E Xplained.
device | Pointer to mxt_device struct |
References Assert, delay_ms, MAXTOUCH_TWI_ADDRESS, MXT143E_XPLAINED_CHG, MXT_GEN_ACQUISITIONCONFIG_T8, MXT_GEN_COMMANDPROCESSOR_CALIBRATE, MXT_GEN_COMMANDPROCESSOR_RESET, MXT_GEN_COMMANDPROCESSOR_T6, MXT_GEN_POWERCONFIG_T7, mxt_get_object_address(), mxt_init_device(), MXT_PROCG_TOUCHSUPPRESSION_T48, MXT_RESET_TIME, MXT_TOUCH_MULTITOUCHSCREEN_T9, MXT_TWI_SPEED, mxt_write_config_object(), mxt_write_config_reg(), twi_options::speed, STATUS_OK, TWI_INTERFACE, twi_master_setup(), and UNUSED.
Referenced by main().
|
static |
Convert touch events from the touchscreen into window pointer events.
Reads touch events in from the touchscreen and converts them into a Window Manager pointer event, for enqueuing into the window event queue.
References win_pointer_event::buttons, gfx_get_height(), gfx_get_width(), win_pointer_event::is_relative, mxt_is_message_pending(), MXT_MOVE_EVENT, MXT_PRESS_EVENT, mxt_read_touch_event(), MXT_RELEASE_EVENT, win_pointer_event::pos, mxt_touch_event::status, STATUS_OK, win_pointer_event::type, WIN_POINTER_MOVE, WIN_POINTER_PRESS, WIN_POINTER_RELEASE, WIN_TOUCH_BUTTON, mxt_touch_event::x, win_point::x, mxt_touch_event::y, and win_point::y.
Referenced by main().
|
static |
Configure the root GUI window.
Configures the root window background to be a tiled version of the Atmel company logo, and sets it as being visible.
References atmel_logo_small, win_attributes::background, WIN_ATTR_BACKGROUND, win_get_attributes(), win_get_root(), win_root, win_set_attributes(), and win_show().
Referenced by main().
|
static |
Show an out of memory error on the display.
Shows a full screen error when called, signaling that the system ran out of memory when initializing a WTK application.
References GFX_COLOR_BLACK, GFX_COLOR_RED, GFX_COLOR_TRANSPARENT, gfx_draw_filled_rect, gfx_draw_string_aligned(), gfx_get_height(), gfx_get_width(), gfx_set_clipping(), sysfont, TEXT_ALIGN_CENTER, and TEXT_POS_CENTER.
Referenced by main().