This is an example application for the mXT143E Xplained, designed to demonstrate multi-touch sensing with maXTouch devices.
This example has been tested with the mXT143E Xplained on the following boards:
This example can track up to 8 touches and will visualize the tracking for the user by drawing a uniquely colored square around each finger.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.