This is the low level driver for the HX8347A display controller.
It provides basic functions for initializing, writing and reading the controller. In addition to hardware control and use of the LCD controller internal functions.
Before writing data to the display call hx8347a_init() which will set up the physical interface and the display. A configuration file conf_hx8347a.h is needed to define which interface to use, pin connections and communication speed.
An example conf_hx8347a.h file for the XMEGA could look like:
This driver depends on the following modules:
Macros | |
#define | HX8347A_COLOR(r, g, b) |
This macro generates a 16-bit native color for the display from a 24-bit RGB value. More... | |
#define | HX8347A_DEFAULT_HEIGHT 320 |
Height of display using default orientation. More... | |
#define | HX8347A_DEFAULT_WIDTH 240 |
Width of display using default orientation. More... | |
#define | HX8347A_FLIP_X 1 |
Bit mask for flipping X for hx8347a_set_orientation() More... | |
#define | HX8347A_FLIP_Y 2 |
Bit mask for flipping Y for hx8347a_set_orientation() More... | |
#define | HX8347A_SWITCH_XY 4 |
Bit mask for swapping X and Y for hx8347a_set_orientation() More... | |
#define | HX8347A_SWITCH_XY_HEIGHT 240 |
Height of display using swapped X/Y orientation. More... | |
#define | HX8347A_SWITCH_XY_WIDTH 320 |
Width of display using swapped X/Y orientation. More... | |
Typedefs | |
typedef uint16_t | hx8347a_color_t |
typedef int16_t | hx8347a_coord_t |
Register manipulation functions | |
void | hx8347a_write_register (uint8_t address, uint8_t value) |
Write a specific register in the controller with a single byte. More... | |
uint8_t | hx8347a_read_register (uint8_t address) |
Read the value of a specific register in the controller. More... | |
void | hx8347a_clear_register (uint8_t address, uint8_t bitmask) |
Helper function for easier register access. More... | |
void | hx8347a_set_register (uint8_t address, uint8_t bitmask) |
Helper function for easier register access. More... | |
Controller primitive graphical functions | |
hx8347a_color_t | hx8347a_read_gram (void) |
Read a single color from the graphical memory. More... | |
void | hx8347a_write_gram (hx8347a_color_t color) |
Write the graphical memory with a single color pixel. More... | |
void | hx8347a_set_top_left_limit (hx8347a_coord_t x, hx8347a_coord_t y) |
Set the display top left drawing limit. More... | |
void | hx8347a_set_bottom_right_limit (hx8347a_coord_t x, hx8347a_coord_t y) |
Set the display bottom right drawing limit. More... | |
void | hx8347a_set_limits (hx8347a_coord_t start_x, hx8347a_coord_t start_y, hx8347a_coord_t end_x, hx8347a_coord_t end_y) |
Set the fully display drawing limits. More... | |
void | hx8347a_set_orientation (uint8_t flags) |
Set the display orientation. More... | |
void | hx8347a_copy_pixels_to_screen (const hx8347a_color_t *pixels, uint32_t count) |
Copy pixels from SRAM to the screen. More... | |
void | hx8347a_copy_progmem_pixels_to_screen (hx8347a_color_t PROGMEM_PTR_T pixels, uint32_t count) |
Copy pixels from progmem to the screen. More... | |
void | hx8347a_copy_pixels_from_screen (hx8347a_color_t *pixels, uint32_t count) |
Copy pixels from the screen to a pixel buffer. More... | |
void | hx8347a_duplicate_pixel (const hx8347a_color_t color, uint32_t count) |
Write a set color to the screen. More... | |
Controller and display initialization and management | |
void | hx8347a_init (void) |
Initialize the controller. More... | |
void | hx8347a_exit_standby (void) |
Send display commands to exit standby mode. More... | |
void | hx8347a_reset_display (void) |
Reset the display using the digital control interface. More... | |
static __always_inline void | hx8347a_backlight_on (void) |
Function to turn on the display back light. More... | |
static __always_inline void | hx8347a_backlight_off (void) |
Function to turn off the display back light. More... | |
#define HX8347A_COLOR | ( | r, | |
g, | |||
b | |||
) |
This macro generates a 16-bit native color for the display from a 24-bit RGB value.
Referenced by hx8347a_copy_pixels_from_screen(), and hx8347a_read_gram().
#define HX8347A_DEFAULT_HEIGHT 320 |
Height of display using default orientation.
Referenced by main().
#define HX8347A_DEFAULT_WIDTH 240 |
Width of display using default orientation.
Referenced by main().
#define HX8347A_FLIP_X 1 |
Bit mask for flipping X for hx8347a_set_orientation()
Referenced by hx8347a_set_orientation().
#define HX8347A_FLIP_Y 2 |
Bit mask for flipping Y for hx8347a_set_orientation()
Referenced by hx8347a_set_orientation().
#define HX8347A_SWITCH_XY 4 |
Bit mask for swapping X and Y for hx8347a_set_orientation()
Referenced by hx8347a_set_orientation().
#define HX8347A_SWITCH_XY_HEIGHT 240 |
Height of display using swapped X/Y orientation.
#define HX8347A_SWITCH_XY_WIDTH 320 |
Width of display using swapped X/Y orientation.
typedef uint16_t hx8347a_color_t |
typedef int16_t hx8347a_coord_t |
|
static |
Function to turn off the display back light.
Use this function to simply set the pin controlling the back light low to turn off the back light.
References CONF_HX8347A_BACKLIGHT_PIN, and gpio_set_pin_low.
|
static |
Function to turn on the display back light.
Use this function to simply set the pin controlling the back light high to turn on the back light.
References CONF_HX8347A_BACKLIGHT_PIN, and gpio_set_pin_high.
Referenced by main().
void hx8347a_clear_register | ( | uint8_t | address, |
uint8_t | bitmask | ||
) |
Helper function for easier register access.
Use this function to clear specific bits in the controller registers.
address | the address of the register to clear |
bitmask | the bitmask of the specific bits to clear |
References hx8347a_read_register(), and hx8347a_write_register().
Referenced by hx8347a_exit_standby().
void hx8347a_copy_pixels_from_screen | ( | hx8347a_color_t * | pixels, |
uint32_t | count | ||
) |
Copy pixels from the screen to a pixel buffer.
Use this function to copy pixels from the display to an internal SRAM buffer. Limits have to be set prior to calling this function, e.g.:
pixels | pointer to the pixel buffer to read to |
count | number of pixels to read |
References Assert, HX8347A_COLOR, hx8347a_deselect_chip(), hx8347a_read_byte(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, and HX8347A_START_READREG.
void hx8347a_copy_pixels_to_screen | ( | const hx8347a_color_t * | pixels, |
uint32_t | count | ||
) |
Copy pixels from SRAM to the screen.
Used to copy a large quantitative of data to the screen in one go. Limits have to be set prior to calling this function, e.g.:
pixels | pointer to the pixel data |
count | number of pixels to copy to the screen |
References Assert, hx8347a_deselect_chip(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, HX8347A_START_WRITEREG, and hx8347a_write_packet().
void hx8347a_copy_progmem_pixels_to_screen | ( | hx8347a_color_t PROGMEM_PTR_T | pixels, |
uint32_t | count | ||
) |
Copy pixels from progmem to the screen.
This function can be used to copy data from program memory (flash) to the display. Limits have to be set prior to calling this function, e.g.:
pixels | pointer to the progmem data |
count | number of pixels to write |
References Assert, hx8347a_deselect_chip(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, HX8347A_START_WRITEREG, PROGMEM_PTR_T, and PROGMEM_READ_BYTE.
void hx8347a_duplicate_pixel | ( | const hx8347a_color_t | color, |
uint32_t | count | ||
) |
Write a set color to the screen.
Use this function to write a certain number of pixels to the same color within a set limit. Limits have to be set prior to calling this function, e.g.:
color | the color to write to the display |
count | the number of pixels to write with this color |
References Assert, hx8347a_deselect_chip(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, HX8347A_START_WRITEREG, and hx8347a_write_packet().
Referenced by main().
void hx8347a_exit_standby | ( | void | ) |
Send display commands to exit standby mode.
This function is used to exit the display standby mode, which is the default mode after a reset signal to the display.
References delay_ms, hx8347a_clear_register(), HX8347A_OSC_EN, HX8347A_OSCCTRL1, HX8347A_POWERCTRL1, hx8347a_set_register(), and HX8347A_STB.
Referenced by hx8347a_init().
void hx8347a_init | ( | void | ) |
Initialize the controller.
Used to initialize the HX8347A display controller by setting up the hardware interface, and setting up the controller according to the manufacturer's description. It also set up the screen orientation to the default state (portrait).
References hx8347a_controller_init_registers(), hx8347a_exit_standby(), hx8347a_interface_init(), and hx8347a_reset_display().
Referenced by main().
hx8347a_color_t hx8347a_read_gram | ( | void | ) |
Read a single color from the graphical memory.
Use this function to read a color from the graphical memory of the controller. Limits have to be set prior to calling this function, e.g.:
hx8347a_color_t | the read color pixel |
References HX8347A_COLOR, hx8347a_deselect_chip(), hx8347a_read_byte(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, and HX8347A_START_READREG.
uint8_t hx8347a_read_register | ( | uint8_t | address | ) |
Read the value of a specific register in the controller.
Use this function to get the value of a specific register in the display controller.
address | the address of the register to read |
References hx8347a_deselect_chip(), hx8347a_read_byte(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), and HX8347A_START_READREG.
Referenced by hx8347a_clear_register(), hx8347a_set_orientation(), and hx8347a_set_register().
void hx8347a_reset_display | ( | void | ) |
Reset the display using the digital control interface.
Controls the reset pin of the display controller to reset the display.
References CONF_HX8347A_RESET_PIN, delay_ms, gpio_set_pin_high, and gpio_set_pin_low.
Referenced by hx8347a_init().
void hx8347a_set_bottom_right_limit | ( | hx8347a_coord_t | x, |
hx8347a_coord_t | y | ||
) |
Set the display bottom right drawing limit.
Use this function to set the bottom right corner of the drawing limit box.
x | the x coordinate of the bottom right corner |
y | the y coordinate of the bottom right corner |
References HX8347A_COLENDHIGH, HX8347A_COLENDLOW, HX8347A_ROWENDHIGH, HX8347A_ROWENDLOW, and hx8347a_write_register().
Referenced by hx8347a_set_limits(), and main().
void hx8347a_set_limits | ( | hx8347a_coord_t | start_x, |
hx8347a_coord_t | start_y, | ||
hx8347a_coord_t | end_x, | ||
hx8347a_coord_t | end_y | ||
) |
Set the fully display drawing limits.
Use this function to set the full drawing limit box.
start_x | the x coordinate of the top left corner |
start_y | the y coordinate of the top left corner |
end_x | the x coordinate of the bottom right corner |
end_y | the y coordinate of the bottom right corner |
References hx8347a_set_bottom_right_limit(), and hx8347a_set_top_left_limit().
void hx8347a_set_orientation | ( | uint8_t | flags | ) |
Set the display orientation.
This is used for orienting the display in different directions, the most obvious once are landscape or portrait mode.
Example of usage (for setting landscape mode):
Or use the GFX defines:
flags | different flags used to define what orientation to use. |
References HX8347A_FLIP_X, HX8347A_FLIP_X_MASK, HX8347A_FLIP_Y, HX8347A_FLIP_Y_MASK, HX8347A_MEMACCESSCTRL, hx8347a_read_register(), HX8347A_SWITCH_XY, HX8347A_SWITCH_XY_MASK, and hx8347a_write_register().
void hx8347a_set_register | ( | uint8_t | address, |
uint8_t | bitmask | ||
) |
Helper function for easier register access.
Use this function to set specific bits in the controller registers.
address | the address of the controller register to set |
bitmask | the bitmask describing which bit to set |
References hx8347a_read_register(), and hx8347a_write_register().
Referenced by hx8347a_exit_standby().
void hx8347a_set_top_left_limit | ( | hx8347a_coord_t | x, |
hx8347a_coord_t | y | ||
) |
Set the display top left drawing limit.
Use this function to set the top left limit of the drawing limit box.
x | the x coordinate of the top left corner |
y | the y coordinate of the top left corner |
References HX8347A_COLSTARTHIGH, HX8347A_COLSTARTLOW, HX8347A_ROWSTARTHIGH, HX8347A_ROWSTARTLOW, and hx8347a_write_register().
Referenced by hx8347a_set_limits(), and main().
void hx8347a_write_gram | ( | hx8347a_color_t | color | ) |
Write the graphical memory with a single color pixel.
Use this function to write a single color pixel to the controller memory. Limits have to be set prior to calling this function, e.g.:
color | the color pixel to write to the screen |
References Assert, hx8347a_deselect_chip(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), HX8347A_SRAMWRITE, and HX8347A_START_WRITEREG.
void hx8347a_write_register | ( | uint8_t | address, |
uint8_t | value | ||
) |
Write a specific register in the controller with a single byte.
Use this function to write a value to a specific register in the display controller.
address | the address of the register to write |
value | the value to be written |
References hx8347a_deselect_chip(), hx8347a_select_chip(), hx8347a_select_register(), hx8347a_send_byte(), and HX8347A_START_WRITEREG.
Referenced by hx8347a_clear_register(), hx8347a_controller_init_registers(), hx8347a_set_bottom_right_limit(), hx8347a_set_orientation(), hx8347a_set_register(), and hx8347a_set_top_left_limit().