This simple example shows how to use the ILI9341 Display Controller Component Driver for interfacing the ILI9341 display controller.
The ILI9341 low level component driver API can be found here.
All devices with some sort of SPI interface, e.g. SPI or USART in SPI mode.
This example show how to use the functions provided by the low level component driver to draw very simple graphics to the screen.
First it uses the function ili9341_duplicate_pixel to draw a color to the screen 20 times. Then it uses ili9341_copy_pixels_to_screen to copy a 40 x 40 single color pixmap to the screen at different locations.
For any advanced drawing of graphics please use the higher level GFX service.
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.