Microchip® Advanced Software Framework

ioport_compat.h File Reference

XMEGA legacy IOPORT software compatibility driver interface header file.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "../ioport.h"

Macros

Initial Output State Flags
#define IOPORT_INIT_LOW   (0 << 1)
 
#define IOPORT_INIT_HIGH   (1 << 1)
 
Input/Sense Configuration Flags
#define IOPORT_BOTHEDGES   (0 << 8)
 
#define IOPORT_RISING   (1 << 8)
 
#define IOPORT_FALLING   (2 << 8)
 
#define IOPORT_LEVEL   (3 << 8)
 
#define IOPORT_FORCE_ENABLE   (6 << 8)
 
#define IOPORT_INPUT_DISABLE   (7 << 8)
 
Output and Pull Configuration Flags
#define IOPORT_TOTEM   (0 << 11)
 
#define IOPORT_BUSKEEPER   (1 << 11)
 
#define IOPORT_PULL_DOWN   (2 << 11)
 
#define IOPORT_PULL_UP   (3 << 11)
 
#define IOPORT_WIRED_OR   (4 << 11)
 
#define IOPORT_WIRED_AND   (5 << 11)
 
#define IOPORT_WIRED_OR_PULL_DOWN   (6 << 11)
 
#define IOPORT_WIRED_AND_PULL_UP   (7 << 11)
 
Inverted I/O Configuration Flags
#define IOPORT_INV_ENABLED   (1 << 14)
 
#define IOPORT_INV_DISABLE   (0 << 14)
 
Slew Rate Limit Configuration Flags
#define IOPORT_SRL_ENABLED   (1 << 15)
 
#define IOPORT_SRL_DISABLED   (0 << 15)
 
PORT fields structure offset

These macros are used to compute the field offset number with the PORT_t structure.

#define PORT_DIR   0x00
 
#define PORT_DIRSET   0x01
 
#define PORT_DIRCLR   0x02
 
#define PORT_DIRTGL   0x03
 
#define PORT_OUT   0x04
 
#define PORT_OUTSET   0x05
 
#define PORT_OUTCLR   0x06
 
#define PORT_OUTTGL   0x07
 
#define PORT_IN   0x08
 
#define PORT_INTCTRL   0x09
 
#define PORT_INT0MASK   0x0A
 
#define PORT_INT1MASK   0x0B
 
#define PORT_INTFLAGS   0x0C
 
#define PORT_PIN0CTRL   0x10
 
#define PORT_PIN1CTRL   0x11
 
#define PORT_PIN2CTRL   0x12
 
#define PORT_PIN3CTRL   0x13
 
#define PORT_PIN4CTRL   0x14
 
#define PORT_PIN5CTRL   0x15
 
#define PORT_PIN6CTRL   0x16
 
#define PORT_PIN7CTRL   0x17
 

Typedefs

typedef uint8_t pin_mask_t
 A pin mask. More...
 
typedef uint8_t port_id_t
 A port id. More...
 
typedef uint16_t port_pin_flags_t
 Pin configuration flags. More...
 
typedef uint8_t port_pin_t
 A PORT pin. More...
 

Functions

static void ioport_configure_group (port_id_t port, pin_mask_t pin_mask, port_pin_flags_t flags)
 Configure a group of I/O pins on a specified port number. More...
 
static void ioport_configure_pin (port_pin_t pin, port_pin_flags_t flags)
 Select the port function for a single pin. More...
 
void ioport_configure_port_pin (void *port, pin_mask_t pin_mask, port_pin_flags_t flags)
 Configure the IO PORT pin function for a set of pins on a port. More...
 
static bool ioport_get_value (port_pin_t pin)
 Read the current state of a PORT pin. More...
 
static PORT_t * ioport_id_pin_to_port (port_id_t port)
 
static bool ioport_pin_is_high (port_pin_t pin)
 Read the current state of a PORT pin and test high level. More...
 
static bool ioport_pin_is_low (port_pin_t pin)
 Read the current state of a PORT pin and test high level. More...
 
static PORT_t * ioport_pin_to_port (port_pin_t pin)
 
static void ioport_set_group_high (port_id_t port_id, pin_mask_t port_mask)
 Drives a group of I/O pin of a port to high level. More...
 
static void ioport_set_group_low (port_id_t port_id, pin_mask_t port_mask)
 Drives a group of I/O pin of a port to low level. More...
 
static void ioport_set_pin_high (port_pin_t pin)
 Drive a PORT pin to a high level. More...
 
static void ioport_set_pin_low (port_pin_t pin)
 Drive a PORT pin to a low level. More...
 
static void ioport_set_value (port_pin_t pin, bool value)
 Drive a PORT pin to a given state. More...
 
static void ioport_tgl_group (port_id_t port_id, pin_mask_t port_mask)
 Toggles a group of I/O pin of a port. More...
 
static void ioport_toggle_pin (port_pin_t pin)
 Toggle the current state of a PORT pin. More...
 

#define IOPORT_BOTHEDGES   (0 << 8)

Sense Both Edges

#define IOPORT_BUSKEEPER   (1 << 11)

Bus Keeper

#define IOPORT_FALLING   (2 << 8)

Sense Falling Edge

#define IOPORT_FORCE_ENABLE   (6 << 8)

Sense Force Input Enable Low Level

#define IOPORT_INIT_HIGH   (1 << 1)

Initial Output State High

Referenced by board_init(), and ioport_configure_port_pin().

#define IOPORT_INIT_LOW   (0 << 1)

Initial Output State Low

#define IOPORT_INPUT_DISABLE   (7 << 8)

Input Buffer Disabled

#define IOPORT_INV_DISABLE   (0 << 14)

I/O is Not Inverted

#define IOPORT_INV_ENABLED   (1 << 14)

I/O is Inverted

#define IOPORT_LEVEL   (3 << 8)

Sense Low Level

#define IOPORT_PULL_DOWN   (2 << 11)

Pull-Down (when input)

#define IOPORT_PULL_UP   (3 << 11)

Pull-Up (when input)

Referenced by board_init().

#define IOPORT_RISING   (1 << 8)

Sense Rising Edge

#define IOPORT_SRL_DISABLED   (0 << 15)

Slew Rate Limit Disabled

#define IOPORT_SRL_ENABLED   (1 << 15)

Slew Rate Limit Enabled

#define IOPORT_TOTEM   (0 << 11)

Normal push/pull output

#define IOPORT_WIRED_AND   (5 << 11)

Wired AND

#define IOPORT_WIRED_AND_PULL_UP   (7 << 11)

Wired AND and Pull-Up

#define IOPORT_WIRED_OR   (4 << 11)

Wired OR

#define IOPORT_WIRED_OR_PULL_DOWN   (6 << 11)

Wired OR and Pull-Down

#define PORT_DIR   0x00

Data Direction

#define PORT_DIRCLR   0x02

Data Direction Clear

Referenced by ioport_configure_port_pin().

#define PORT_DIRSET   0x01

Data Direction Set

Referenced by ioport_configure_port_pin().

#define PORT_DIRTGL   0x03

Data Direction Toggle

#define PORT_IN   0x08

Data Input Value

#define PORT_INT0MASK   0x0A

Interrupt 0 Mask

#define PORT_INT1MASK   0x0B

Interrupt 1 Mask

#define PORT_INTCTRL   0x09

Interrupt Control

#define PORT_INTFLAGS   0x0C

Interrupt Flags

#define PORT_OUT   0x04

Data Output Value

#define PORT_OUTCLR   0x06

Data Output Value Clear

Referenced by ioport_configure_port_pin().

#define PORT_OUTSET   0x05

Data Output Value Set

Referenced by ioport_configure_port_pin().

#define PORT_OUTTGL   0x07

Data Output Value Toggle

#define PORT_PIN0CTRL   0x10

Pin 0 Configuration

Referenced by ioport_configure_port_pin().

#define PORT_PIN1CTRL   0x11

Pin 1 Configuration

#define PORT_PIN2CTRL   0x12

Pin 2 Configuration

#define PORT_PIN3CTRL   0x13

Pin 3 Configuration

#define PORT_PIN4CTRL   0x14

Pin 4 Configuration

#define PORT_PIN5CTRL   0x15

Pin 5 Configuration

#define PORT_PIN6CTRL   0x16

Pin 6 Configuration

#define PORT_PIN7CTRL   0x17

Pin 7 Configuration

typedef uint8_t pin_mask_t

A pin mask.

This type is used to describe the port pin mask on the part.

typedef uint8_t port_id_t

A port id.

This type is used to describe the port id on the part (0 is PORTA).

typedef uint16_t port_pin_flags_t

Pin configuration flags.

This is a bitmask containing configuration flags for the pins that shall be configured.

typedef uint8_t port_pin_t

A PORT pin.

This type is used to describe the PORT pins on the part.

static void ioport_configure_group ( port_id_t  port,
pin_mask_t  pin_mask,
port_pin_flags_t  flags 
)
inlinestatic

Configure a group of I/O pins on a specified port number.

Parameters
portThe port number
pin_maskThe pin mask to configure
flagsBitmask of flags specifying additional configuration parameters.

References arch_ioport_port_to_base(), and ioport_configure_port_pin().

static void ioport_configure_pin ( port_pin_t  pin,
port_pin_flags_t  flags 
)
inlinestatic

Select the port function for a single pin.

Parameters
pinThe pin to configure
flagsBitmask of flags specifying additional configuration parameters.

References arch_ioport_pin_to_base(), arch_ioport_pin_to_mask(), and ioport_configure_port_pin().

Referenced by board_init().

void ioport_configure_port_pin ( void *  port,
pin_mask_t  pin_mask,
port_pin_flags_t  flags 
)

Configure the IO PORT pin function for a set of pins on a port.

Parameters
portPointer to the port
pin_maskMask containing the pins that should be configured
flagsBitmask of flags specifying additional configuration parameters.

References IOPORT_DIR_OUTPUT, IOPORT_INIT_HIGH, PORT_DIRCLR, PORT_DIRSET, PORT_OUTCLR, PORT_OUTSET, and PORT_PIN0CTRL.

Referenced by ioport_configure_group(), and ioport_configure_pin().

static bool ioport_get_value ( port_pin_t  pin)
inlinestatic

Read the current state of a PORT pin.

Parameters
pinA number identifying the pin to read.
Return values
trueThe pin is currently high (close to Vdd)
falseThe pin is currently low (close to Vss)

References arch_ioport_get_pin_level().

static PORT_t* ioport_id_pin_to_port ( port_id_t  port)
inlinestatic
static bool ioport_pin_is_high ( port_pin_t  pin)
inlinestatic

Read the current state of a PORT pin and test high level.

Parameters
pinA number identifying the pin to read.
Return values
trueThe pin is currently high (close to Vdd)
falseThe pin is currently low (close to Vss)

References arch_ioport_get_pin_level().

static bool ioport_pin_is_low ( port_pin_t  pin)
inlinestatic

Read the current state of a PORT pin and test high level.

Parameters
pinA number identifying the pin to read.
Return values
trueThe pin is currently high (close to Vdd)
falseThe pin is currently low (close to Vss)

References arch_ioport_get_pin_level().

static PORT_t* ioport_pin_to_port ( port_pin_t  pin)
inlinestatic
static void ioport_set_group_high ( port_id_t  port_id,
pin_mask_t  port_mask 
)
inlinestatic

Drives a group of I/O pin of a port to high level.

Parameters
port_idThe port number.
port_maskThe mask.

References arch_ioport_set_port_level().

static void ioport_set_group_low ( port_id_t  port_id,
pin_mask_t  port_mask 
)
inlinestatic

Drives a group of I/O pin of a port to low level.

Parameters
port_idThe port number.
port_maskThe mask.

References arch_ioport_set_port_level().

static void ioport_set_pin_high ( port_pin_t  pin)
inlinestatic

Drive a PORT pin to a high level.

This function will only have an effect if pin is configured as an output.

Parameters
pinA number identifying the pin to act on.

References arch_ioport_set_pin_level().

Referenced by spi_deselect_device().

static void ioport_set_pin_low ( port_pin_t  pin)
inlinestatic

Drive a PORT pin to a low level.

This function will only have an effect if pin is configured as an output.

Parameters
pinA number identifying the pin to act on.

References arch_ioport_set_pin_level().

Referenced by spi_select_device().

static void ioport_set_value ( port_pin_t  pin,
bool  value 
)
inlinestatic

Drive a PORT pin to a given state.

This function will only have an effect if pin is configured as an output.

Parameters
pinA number identifying the pin to act on.
valueThe desired state of the pin. true means drive the pin high (towards Vdd), while false means drive the pin low (towards Vss).

References arch_ioport_set_pin_level().

static void ioport_tgl_group ( port_id_t  port_id,
pin_mask_t  port_mask 
)
inlinestatic

Toggles a group of I/O pin of a port.

Parameters
port_idThe port number.
port_maskThe mask.

References arch_ioport_toggle_port_level().

static void ioport_toggle_pin ( port_pin_t  pin)
inlinestatic

Toggle the current state of a PORT pin.

Parameters
pinA number identifying the pin to act on.

References arch_ioport_toggle_pin_level().