Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Two-Wire Interface (TWI)

Driver for the TWI (Two-Wire Interface).

This driver provides access to the main features of the TWI controller. The TWI interconnects components on a unique two-wire bus. The TWI is programmable as a master or a slave with sequential or single-byte access. Multiple master capability is supported.

Usage
  1. Enable the TWI peripheral clock in the PMC.
  2. Enable the required TWI PIOs (see pio.h).
  3. Enable TWI master mode by calling twi_enable_master_mode if it is a master on the I2C bus.
  4. Configure the TWI in master mode by calling twi_master_init.
  5. Send data to a slave device on the I2C bus by calling twi_master_write.
  6. Receive data from a slave device on the I2C bus by calling the twi_master_read.
  7. Enable TWI slave mode by calling twi_enable_slave_mode if it is a slave on the I2C bus.
  8. Configure the TWI in slave mode by calling twi_slave_init.

Macros

#define I2C_FAST_MODE_SPEED   400000
 
#define LOW_LEVEL_TIME_LIMIT   384000
 
#define TWI_CLK_CALC_ARGU   4
 
#define TWI_CLK_DIV_MAX   0xFF
 
#define TWI_CLK_DIV_MIN   7
 
#define TWI_CLK_DIVIDER   2
 
#define TWI_WP_KEY_VALUE   TWI_WPMR_WPKEY_PASSWD
 

Functions

void twi_disable_interrupt (Twi *p_twi, uint32_t ul_sources)
 Disable TWI interrupts. More...
 
void twi_disable_master_mode (Twi *p_twi)
 Disable TWI master mode. More...
 
void twi_disable_slave_mode (Twi *p_twi)
 Disable TWI slave mode. More...
 
void twi_enable_interrupt (Twi *p_twi, uint32_t ul_sources)
 Enable TWI interrupts. More...
 
void twi_enable_master_mode (Twi *p_twi)
 Enable TWI master mode. More...
 
void twi_enable_slave_mode (Twi *p_twi)
 Enable TWI slave mode. More...
 
uint32_t twi_get_interrupt_mask (Twi *p_twi)
 Read TWI interrupt mask. More...
 
uint32_t twi_get_interrupt_status (Twi *p_twi)
 Get TWI interrupt status. More...
 
Pdc * twi_get_pdc_base (Twi *p_twi)
 Get TWI PDC base address. More...
 
uint32_t twi_master_init (Twi *p_twi, const twi_options_t *p_opt)
 Initialize TWI master mode. More...
 
uint32_t twi_master_read (Twi *p_twi, twi_packet_t *p_packet)
 Read multiple bytes from a TWI compatible slave device. More...
 
uint32_t twi_master_write (Twi *p_twi, twi_packet_t *p_packet)
 Write multiple bytes to a TWI compatible slave device. More...
 
uint32_t twi_mk_addr (const uint8_t *addr, int len)
 Construct the TWI module address register field. More...
 
uint32_t twi_probe (Twi *p_twi, uint8_t uc_slave_addr)
 Test if a chip answers a given I2C address. More...
 
uint8_t twi_read_byte (Twi *p_twi)
 Reads a byte from the TWI bus. More...
 
void twi_reset (Twi *p_twi)
 Reset TWI. More...
 
void twi_set_slave_addr (Twi *p_twi, uint32_t ul_device_addr)
 Set TWI slave address. More...
 
uint32_t twi_set_speed (Twi *p_twi, uint32_t ul_speed, uint32_t ul_mck)
 Set the I2C bus speed in conjunction with the clock frequency. More...
 
void twi_slave_init (Twi *p_twi, uint32_t ul_device_addr)
 Initialize TWI slave mode. More...
 
uint32_t twi_slave_read (Twi *p_twi, uint8_t *p_data)
 Read data from master. More...
 
uint32_t twi_slave_write (Twi *p_twi, uint8_t *p_data)
 Write data to TWI bus. More...
 
void twi_write_byte (Twi *p_twi, uint8_t uc_byte)
 Sends a byte of data to one of the TWI slaves on the bus. More...
 

#define I2C_FAST_MODE_SPEED   400000

Referenced by twi_set_speed().

#define LOW_LEVEL_TIME_LIMIT   384000

Referenced by twi_set_speed().

#define TWI_CLK_CALC_ARGU   4

Referenced by twi_set_speed().

#define TWI_CLK_DIV_MAX   0xFF

Referenced by twi_set_speed().

#define TWI_CLK_DIV_MIN   7

Referenced by twi_set_speed().

#define TWI_CLK_DIVIDER   2

Referenced by twi_set_speed().

#define TWI_WP_KEY_VALUE   TWI_WPMR_WPKEY_PASSWD

void twi_disable_interrupt ( Twi *  p_twi,
uint32_t  ul_sources 
)

Disable TWI interrupts.

Parameters
p_twiPointer to a TWI instance.
ul_sourcesInterrupts to be disabled.
void twi_disable_master_mode ( Twi *  p_twi)

Disable TWI master mode.

Parameters
p_twiPointer to a TWI instance.
void twi_disable_slave_mode ( Twi *  p_twi)

Disable TWI slave mode.

Parameters
p_twiPointer to a TWI instance.
void twi_enable_interrupt ( Twi *  p_twi,
uint32_t  ul_sources 
)

Enable TWI interrupts.

Parameters
p_twiPointer to a TWI instance.
ul_sourcesInterrupts to be enabled.
void twi_enable_master_mode ( Twi *  p_twi)

Enable TWI master mode.

Parameters
p_twiPointer to a TWI instance.

Referenced by twi_master_init().

void twi_enable_slave_mode ( Twi *  p_twi)

Enable TWI slave mode.

Parameters
p_twiPointer to a TWI instance.

Referenced by twi_slave_init().

uint32_t twi_get_interrupt_mask ( Twi *  p_twi)

Read TWI interrupt mask.

Parameters
p_twiPointer to a TWI instance.
Returns
The interrupt mask value.
uint32_t twi_get_interrupt_status ( Twi *  p_twi)

Get TWI interrupt status.

Parameters
p_twiPointer to a TWI instance.
Return values
TWIinterrupt status.
Pdc* twi_get_pdc_base ( Twi *  p_twi)

Get TWI PDC base address.

Parameters
p_twiPointer to a TWI instance.
Returns
TWI PDC registers base for PDC driver to access.

References Assert.

uint32_t twi_master_init ( Twi *  p_twi,
const twi_options_t p_opt 
)

Initialize TWI master mode.

Parameters
p_twiPointer to a TWI instance.
p_optOptions for initializing the TWI module (see twi_options_t).
Returns
TWI_SUCCESS if initialization is complete, error code otherwise.

References FAIL, twi_options::master_clk, twi_options::smbus, twi_options::speed, twi_enable_master_mode(), TWI_INVALID_ARGUMENT, twi_reset(), twi_set_speed(), and TWI_SUCCESS.

Referenced by twi_master_setup().

uint32_t twi_master_read ( Twi *  p_twi,
twi_packet_t p_packet 
)

Read multiple bytes from a TWI compatible slave device.

Note
This function will NOT return until all data has been read or error occurs.
Parameters
p_twiPointer to a TWI instance.
p_packetPacket information and data (see twi_packet_t).
Returns
TWI_SUCCESS if all bytes were read, error code otherwise.

References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, TWI_ERROR_TIMEOUT, TWI_INVALID_ARGUMENT, twi_mk_addr(), TWI_RECEIVE_NACK, TWI_SUCCESS, and TWI_TIMEOUT.

Referenced by at24cxx_read_byte(), at24cxx_read_continuous(), and at24cxx_read_page().

uint32_t twi_master_write ( Twi *  p_twi,
twi_packet_t p_packet 
)

Write multiple bytes to a TWI compatible slave device.

Note
This function will NOT return until all data has been written or error occurred.
Parameters
p_twiPointer to a TWI instance.
p_packetPacket information and data (see twi_packet_t).
Returns
TWI_SUCCESS if all bytes were written, error code otherwise.

References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, TWI_INVALID_ARGUMENT, twi_mk_addr(), TWI_RECEIVE_NACK, and TWI_SUCCESS.

Referenced by at24cxx_acknowledge_polling(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), and twi_probe().

uint32_t twi_mk_addr ( const uint8_t *  addr,
int  len 
)

Construct the TWI module address register field.

The TWI module address register is sent out MSB first. And the size controls which byte is the MSB to start with.

Please see the device datasheet for details on this.

Referenced by twi_master_read(), and twi_master_write().

uint32_t twi_probe ( Twi *  p_twi,
uint8_t  uc_slave_addr 
)

Test if a chip answers a given I2C address.

Parameters
p_twiPointer to a TWI instance.
uc_slave_addrAddress of the remote chip to search for.
Returns
TWI_SUCCESS if a chip was found, error code otherwise.

References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, and twi_master_write().

uint8_t twi_read_byte ( Twi *  p_twi)

Reads a byte from the TWI bus.

Parameters
p_twiPointer to a TWI instance.
Returns
The byte read.
void twi_reset ( Twi *  p_twi)

Reset TWI.

Parameters
p_twiPointer to a TWI instance.

Referenced by twi_master_init(), and twi_slave_init().

void twi_set_slave_addr ( Twi *  p_twi,
uint32_t  ul_device_addr 
)

Set TWI slave address.

Parameters
p_twiPointer to a TWI instance.
ul_device_addrDevice address of the SAM slave device on the I2C bus.
uint32_t twi_set_speed ( Twi *  p_twi,
uint32_t  ul_speed,
uint32_t  ul_mck 
)

Set the I2C bus speed in conjunction with the clock frequency.

Parameters
p_twiPointer to a TWI instance.
ul_speedThe desired I2C bus speed (in Hz).
ul_mckMain clock of the device (in Hz).
Return values
PASSNew speed setting is accepted.
FAILNew speed setting is rejected.

References FAIL, I2C_FAST_MODE_SPEED, LOW_LEVEL_TIME_LIMIT, PASS, TWI_CLK_CALC_ARGU, TWI_CLK_DIV_MAX, TWI_CLK_DIV_MIN, and TWI_CLK_DIVIDER.

Referenced by twi_master_init().

void twi_slave_init ( Twi *  p_twi,
uint32_t  ul_device_addr 
)

Initialize TWI slave mode.

Parameters
p_twiPointer to a TWI instance.
ul_device_addrDevice address of the SAM slave device on the I2C bus.

References twi_enable_slave_mode(), and twi_reset().

Referenced by twi_slave_setup().

uint32_t twi_slave_read ( Twi *  p_twi,
uint8_t *  p_data 
)

Read data from master.

Note
This function will NOT return until master sends a STOP condition.
Parameters
p_twiPointer to a TWI instance.
p_dataPointer to the data buffer where data received will be stored.
Returns
Number of bytes read.
uint32_t twi_slave_write ( Twi *  p_twi,
uint8_t *  p_data 
)

Write data to TWI bus.

Note
This function will NOT return until master sends a STOP condition.
Parameters
p_twiPointer to a TWI instance.
p_dataPointer to the data buffer to be sent.
Returns
Number of bytes written.
void twi_write_byte ( Twi *  p_twi,
uint8_t  uc_byte 
)

Sends a byte of data to one of the TWI slaves on the bus.

Parameters
p_twiPointer to a TWI instance.
byteThe byte to send.