Raw flash operation.
This file contains definitions and functions for raw NAND Flash operation.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include "nand_flash_raw.h"
#include "conf_board.h"
#include "gpio.h"
#include "smc.h"
#include "pmc.h"
#include "dmac.h"
#include "delay.h"
Macros | |
#define | CONF_NF_ADDRESS_CYCLE_CMD NFCADDR_CMD_ACYCLE_FIVE |
#define | MODEL(raw) ((struct nand_flash_model *)raw) |
#define | READ_DATA16(raw) (*((volatile uint16_t *)raw->data_address)) |
#define | READ_DATA8(raw) (*((volatile uint8_t *)raw->data_address)) |
Functions | |
static uint32_t | check_status (const struct nand_flash_raw *raw) |
Check if program or erase operation is completed in current operation. More... | |
static uint32_t | copy_page (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t source_page, uint16_t dest_block, uint16_t dest_page) |
Copy the data in a page of the NAND Flash device to an other page on that same chip. More... | |
static uint32_t | erase_block (const struct nand_flash_raw *raw, uint16_t block) |
Erase the specified block of the NAND Flash chip. More... | |
uint32_t | nand_flash_raw_copy_block (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t dest_block) |
Copy the data of one whole block of a NAND Flash device to another block. More... | |
uint32_t | nand_flash_raw_copy_page (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t source_page, uint16_t dest_block, uint16_t dest_page) |
Copy the data in a page of the NAND Flash device to an other page on that same chip. More... | |
uint32_t | nand_flash_raw_erase_block (const struct nand_flash_raw *raw, uint16_t block) |
Erase the specified block of the device, retrying several time if it fails. More... | |
uint32_t | nand_flash_raw_initialize (struct nand_flash_raw *raw, const struct nand_flash_model *model, uint32_t command_address, uint32_t address_address, uint32_t data_address) |
Initialize a nand_flash_raw instance based on the given model and physical interface. More... | |
uint32_t | nand_flash_raw_read_id (const struct nand_flash_raw *raw) |
Reads and returns the identifiers of a NAND Flash chip. More... | |
void | nand_flash_raw_read_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, uint8_t *data, uint8_t *spare) |
Read the data and/or the spare areas of a page of a NAND Flash into the provided buffers. More... | |
void | nand_flash_raw_reset (const struct nand_flash_raw *raw) |
Reset a NAND Flash device. More... | |
uint32_t | nand_flash_raw_write_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, uint8_t *data, uint8_t *spare) |
Write the data and/or the spare areas of a page of a NAND Flash into the provided buffers. More... | |
static void | nfc_copy_data_from_internal_sram (uint8_t *data, uint32_t sram_offset, uint16_t size) |
Copy data from the NFC sram to the provided buffer. More... | |
static void | nfc_copy_data_to_internal_sram (uint8_t *data, uint32_t sram_offset, uint16_t size) |
Send data to the NFC sram from the provided buffer. More... | |
static void | nfc_translate_address (const struct nand_flash_raw *raw, uint32_t column_address, uint32_t row_address, uint32_t *p_address_cycle0, uint32_t *p_address_cycle1234, uint32_t five_address) |
Translate the given column and row address into first and other (1-4) address cycles. More... | |
static uint32_t | write_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, void *data, void *spare) |
Write the data and/or the spare area of a page on a NAND Flash chip. More... | |
#define CONF_NF_ADDRESS_CYCLE_CMD NFCADDR_CMD_ACYCLE_FIVE |
Referenced by copy_page(), nand_flash_raw_read_page(), and write_page().
#define MODEL | ( | raw | ) | ((struct nand_flash_model *)raw) |
Referenced by copy_page(), erase_block(), nand_flash_raw_copy_block(), nand_flash_raw_read_page(), nfc_translate_address(), and write_page().
#define READ_DATA16 | ( | raw | ) | (*((volatile uint16_t *)raw->data_address)) |
#define READ_DATA8 | ( | raw | ) | (*((volatile uint8_t *)raw->data_address)) |
Referenced by check_status(), and nand_flash_raw_read_id().
|
static |
Check if program or erase operation is completed in current operation.
raw | Pointer to a nand_flash_raw instance. |
References BOARD_NAND_CS, NAND_COMMAND_STATUS, NAND_STATUS_ERROR, NAND_STATUS_READY, NFCADDR_CMD_ACYCLE_NONE, NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, READ_DATA8, and smc_nfc_send_command().
Referenced by copy_page(), erase_block(), and write_page().
|
static |
Copy the data in a page of the NAND Flash device to an other page on that same chip.
raw | Pointer to a nand_flash_raw instance. |
source_block | Source block number. |
source_page | Source page number inside the source block. |
dest_block | Destination block number. |
dest_page | Destination page number inside the destination block. |
References BOARD_NAND_CS, check_status(), CONF_NF_ADDRESS_CYCLE_CMD, CONF_NF_NEED_FIVE_ADDRESS_CYCLES, MODEL, NAND_COMMAND_COPYBACK_PROGRAM_1, NAND_COMMAND_COPYBACK_PROGRAM_2, NAND_COMMAND_COPYBACK_READ_1, NAND_COMMAND_COPYBACK_READ_2, NAND_COMMON_ERROR_CANNOTCOPY, NAND_COMMON_ERROR_CANNOTWRITE, NAND_COMMON_MAX_PAGE_SIZE, NAND_COMMON_MAX_PAGE_SPARE_SIZE, nand_flash_model_copy_back(), nand_flash_model_get_block_size_in_pages(), nand_flash_raw_read_page(), nand_flash_raw_write_page(), nfc_translate_address(), NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, NFCADDR_CMD_VCMD2, smc_nfc_get_status(), and smc_nfc_send_command().
Referenced by nand_flash_raw_copy_page().
|
static |
Erase the specified block of the NAND Flash chip.
raw | Pointer to a nand_flash_raw instance. |
block | Number of the physical block to erase. |
References BOARD_NAND_CS, check_status(), delay_ms, MODEL, NAND_COMMAND_ERASE_1, NAND_COMMAND_ERASE_2, NAND_COMMON_ERROR_CANNOTERASE, nand_flash_model_get_block_size_in_pages(), nfc_translate_address(), NFCADDR_CMD_ACYCLE_THREE, NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, NFCADDR_CMD_VCMD2, smc_nfc_get_status(), and smc_nfc_send_command().
Referenced by nand_flash_raw_erase_block().
uint32_t nand_flash_raw_copy_block | ( | const struct nand_flash_raw * | raw, |
uint16_t | source_block, | ||
uint16_t | dest_block | ||
) |
Copy the data of one whole block of a NAND Flash device to another block.
raw | Pointer to a nand_flash_raw instance. |
source_block | Source block number. |
dest_block | Destination block number. |
References Assert, MODEL, NAND_COMMON_ERROR_BADBLOCK, nand_flash_model_get_block_size_in_pages(), and nand_flash_raw_copy_page().
uint32_t nand_flash_raw_copy_page | ( | const struct nand_flash_raw * | raw, |
uint16_t | source_block, | ||
uint16_t | source_page, | ||
uint16_t | dest_block, | ||
uint16_t | dest_page | ||
) |
Copy the data in a page of the NAND Flash device to an other page on that same chip.
raw | Pointer to a nand_flash_raw instance. |
source_block | Source block number. |
source_page | Source page number inside the source block. |
dest_block | Destination block number. |
dest_page | Destination page number inside the destination block. |
References CONF_NF_COPY_NUM_TRY, copy_page(), and NAND_COMMON_ERROR_BADBLOCK.
Referenced by nand_flash_raw_copy_block().
uint32_t nand_flash_raw_erase_block | ( | const struct nand_flash_raw * | raw, |
uint16_t | block | ||
) |
Erase the specified block of the device, retrying several time if it fails.
raw | Pointer to a nand_flash_raw instance. |
block | Number of the physical block to erase. |
References CONF_NF_ERASE_NUM_TRY, erase_block(), and NAND_COMMON_ERROR_BADBLOCK.
Referenced by main().
uint32_t nand_flash_raw_initialize | ( | struct nand_flash_raw * | raw, |
const struct nand_flash_model * | model, | ||
uint32_t | command_address, | ||
uint32_t | address_address, | ||
uint32_t | data_address | ||
) |
Initialize a nand_flash_raw instance based on the given model and physical interface.
raw | Pointer to a nand_flash_raw instance. |
model | Pointer to the underlying nand chip model. Can be 0. |
command_address | Address at which commands are sent. |
address_address | Address at which addresses are sent. |
data_address | Address at which data is sent. |
References nand_flash_raw::address_address, BOARD_NAND_CS, nand_flash_raw::command_address, CONF_NF_BUSWIDTH, CONF_NF_CYCLE_TIMING, CONF_NF_DMA_CHANNEL, CONF_NF_PULSE_TIMING, CONF_NF_SETUP_TIMING, CONF_NF_TIMING, nand_flash_raw::data_address, data_address, delay_ms, dmac_channel_set_configuration(), dmac_enable(), dmac_init(), DMAC_PRIORITY_ROUND_ROBIN, dmac_set_priority_mode(), nand_flash_raw::model, NAND_COMMON_ERROR_UNKNOWNMODEL, nand_flash_model_find(), nand_flash_model_list, NAND_FLASH_MODEL_LIST_SIZE, nand_flash_raw_read_id(), nand_flash_raw_reset(), nand_flash_model::page_size_in_bytes, pmc_enable_periph_clk(), smc_nfc_enable(), smc_nfc_init(), smc_set_cycle_timing(), smc_set_mode(), smc_set_nand_timing(), smc_set_pulse_timing(), and smc_set_setup_timing().
Referenced by main(), and nand_flash_ecc_initialize().
uint32_t nand_flash_raw_read_id | ( | const struct nand_flash_raw * | raw | ) |
Reads and returns the identifiers of a NAND Flash chip.
raw | Pointer to a nand_flash_raw instance. |
References BOARD_NAND_CS, delay_us, NAND_COMMAND_READID, NFCADDR_CMD_ACYCLE_ONE, NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, READ_DATA8, and smc_nfc_send_command().
Referenced by nand_flash_raw_initialize().
void nand_flash_raw_read_page | ( | const struct nand_flash_raw * | raw, |
uint16_t | block, | ||
uint16_t | page, | ||
uint8_t * | data, | ||
uint8_t * | spare | ||
) |
Read the data and/or the spare areas of a page of a NAND Flash into the provided buffers.
raw | Pointer to a nand_flash_raw instance. |
block | Number of the physical block to read. |
page | Number of the page to read inside the given block. |
data | Buffer where the data area will be read. |
spare | Buffer where the spare area will be read. |
References BOARD_NAND_CS, CONF_NF_ADDRESS_CYCLE_CMD, CONF_NF_NEED_FIVE_ADDRESS_CYCLES, MODEL, NAND_COMMAND_READ_1, NAND_COMMAND_READ_2, NAND_COMMAND_READ_A, nand_flash_model_get_block_size_in_pages(), nand_flash_model_get_page_data_size(), nand_flash_model_get_page_spare_size(), nand_flash_model_small_block(), nfc_copy_data_from_internal_sram(), nfc_translate_address(), NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, NFCADDR_CMD_NFCEN, NFCADDR_CMD_VCMD2, smc_nfc_disable_spare_read(), smc_nfc_enable_spare_read(), smc_nfc_get_status(), and smc_nfc_send_command().
Referenced by copy_page(), and nand_flash_ecc_read_page().
void nand_flash_raw_reset | ( | const struct nand_flash_raw * | raw | ) |
Reset a NAND Flash device.
raw | Pointer to a nand_flash_raw instance. |
References BOARD_NAND_CS, NAND_COMMAND_RESET, NFCADDR_CMD_ACYCLE_NONE, NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFCCMD, smc_nfc_get_status(), smc_nfc_send_command(), and UNUSED.
Referenced by nand_flash_raw_initialize().
uint32_t nand_flash_raw_write_page | ( | const struct nand_flash_raw * | raw, |
uint16_t | block, | ||
uint16_t | page, | ||
uint8_t * | data, | ||
uint8_t * | spare | ||
) |
Write the data and/or the spare areas of a page of a NAND Flash into the provided buffers.
raw | Pointer to a nand_flash_raw instance. |
block | Number of the physical block to write resides. |
page | Number of the page to write inside the given block. |
data | Buffer where the data area will be stored. |
spare | Buffer where the spare area will be stored. |
References CONF_NF_WRITE_NUM_TRY, NAND_COMMON_ERROR_BADBLOCK, and write_page().
Referenced by copy_page(), and nand_flash_ecc_write_page().
|
static |
Copy data from the NFC sram to the provided buffer.
data | Buffer where the data area will be stored. |
sram_offset | NFC internal sram start offset. |
size | Number of data bytes to receive. |
References CONF_NF_DMA_CHANNEL, dmac_channel_enable(), dmac_channel_is_transfer_done(), dmac_channel_single_buf_transfer_init(), dma_transfer_descriptor_t::ul_ctrlA, dma_transfer_descriptor_t::ul_ctrlB, dma_transfer_descriptor_t::ul_descriptor_addr, dma_transfer_descriptor_t::ul_destination_addr, and dma_transfer_descriptor_t::ul_source_addr.
Referenced by nand_flash_raw_read_page().
|
static |
Send data to the NFC sram from the provided buffer.
data | Pointer to where the data stored. |
sram_offset | NFC internal sram start offset. |
size | Number of data bytes to send. |
References CONF_NF_DMA_CHANNEL, dmac_channel_enable(), dmac_channel_is_transfer_done(), dmac_channel_single_buf_transfer_init(), dma_transfer_descriptor_t::ul_ctrlA, dma_transfer_descriptor_t::ul_ctrlB, dma_transfer_descriptor_t::ul_descriptor_addr, dma_transfer_descriptor_t::ul_destination_addr, and dma_transfer_descriptor_t::ul_source_addr.
Referenced by write_page().
|
static |
Translate the given column and row address into first and other (1-4) address cycles.
The resulting values are stored in the provided variables if they are not null.
raw | Pointer to a nand_flash_raw instance. |
column_address | Column address to translate. |
row_address | Row address to translate. |
p_address_cycle0 | First address cycle. |
p_address_cycle1234 | four address cycles. |
five_address | Flag for five address cycles. |
References MODEL, nand_flash_model_get_data_bus_width(), nand_flash_model_get_device_size_in_pages(), and nand_flash_model_get_page_data_size().
Referenced by copy_page(), erase_block(), nand_flash_raw_read_page(), and write_page().
|
static |
Write the data and/or the spare area of a page on a NAND Flash chip.
raw | Pointer to a nand_flash_raw instance. |
block | Number of the physical block to erase. |
page | Number of the page to write inside the given block. |
data | Buffer containing the data area. |
spare | Buffer containing the spare area. |
Note: special case when ECC parity generation. ECC results are available as soon as the counter reaches the end of the main area. But when reach page_size for an example, it could not generate last ECC_PR, The workaround enable SPARE_WRITE, whatever real spare area write or not.
References BOARD_NAND_CS, check_status(), CONF_NF_ADDRESS_CYCLE_CMD, CONF_NF_NEED_FIVE_ADDRESS_CYCLES, MODEL, NAND_COMMAND_WRITE_1, NAND_COMMAND_WRITE_2, NAND_COMMON_ERROR_CANNOTWRITE, nand_flash_model_get_block_size_in_pages(), nand_flash_model_get_page_data_size(), nand_flash_model_get_page_spare_size(), nfc_copy_data_to_internal_sram(), nfc_translate_address(), NFCADDR_CMD_ACYCLE_NONE, NFCADDR_CMD_CSID, NFCADDR_CMD_NFC_READ, NFCADDR_CMD_NFC_WIRTE, NFCADDR_CMD_NFCCMD, NFCADDR_CMD_NFCEN, smc_nfc_disable_spare_write(), smc_nfc_enable_spare_write(), smc_nfc_get_status(), and smc_nfc_send_command().
Referenced by nand_flash_raw_write_page().