Purpose
This NAND Flash software ECC example show how to read and write data with software ECC from/to a NAND Flash connected to the chip.
Description
The required steps are:
-
Initialize NAND Flash.
-
Find a good block by erase function.
-
Prepare a buffer.
-
Write the buffer into a NAND Flash page by software ECC function.
-
Read the page by software ECC function and check data is correct.
Usage
- On the computer, open and configure a terminal application (e.g. HyperTerminal on Microsoft Windows) with these settings:
- 115200 bauds
- 8 bits of data
- No parity
- 1 stop bit
- No flow control
- Start the application.
- In the terminal window, the following text should appear:
-- NAND Flash With Software ECC Example --
-- xxxxxx-xx
-- Compiled: xxx xx xxxx xx:xx:xx --
-I- NAND Flash driver initialized
-I- Size of the whole device in bytes : 0xxxxxxxx
-I- Size in bytes of one single block of a device : 0xxxxxx
-I- Number of blocks in the entire device : 0xxxx
-I- Size of the data area of a page in bytes : 0xxxx
-I- Number of pages in the entire device : 0xxx