Microchip® Advanced Software Framework

mpu.h File Reference

SAMV70/SAMV71/SAME70/SAMS70-XULTRA board mpu config.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"

Macros

#define ARM_MODE_USR   0x10
 
#define DTCM_END_ADDRESS   0x203FFFFFUL
 
#define DTCM_START_ADDRESS   0x20000000UL
 
#define EXT_EBI_END_ADDRESS   0x6FFFFFFFUL
 
#define EXT_EBI_START_ADDRESS   0x60000000UL
 
#define IFLASH_END_ADDRESS   0x005FFFFFUL
 
#define IFLASH_PRIVILEGE_END_ADDRESS   (IFLASH_START_ADDRESS + 0xFFF)
 
#define IFLASH_PRIVILEGE_START_ADDRESS   (IFLASH_START_ADDRESS)
 
#define IFLASH_START_ADDRESS   0x00400000UL
 
#define IFLASH_UNPRIVILEGE_END_ADDRESS   (IFLASH_END_ADDRESS)
 
#define IFLASH_UNPRIVILEGE_START_ADDRESS   (IFLASH_PRIVILEGE_END_ADDRESS + 1)
 
#define INNER_NORMAL_WB_NWA_TYPE(x)   (( 0x04 << MPU_RASR_TEX_Pos ) | ( ENABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos ))
 
#define INNER_NORMAL_WB_RWA_TYPE(x)   (( 0x04 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos ))
 
#define INNER_OUTER_NORMAL_NOCACHE_TYPE(x)   ((0x01 << MPU_RASR_TEX_Pos) | (DISABLE << MPU_RASR_C_Pos) | (DISABLE << MPU_RASR_B_Pos) | (x << MPU_RASR_S_Pos))
 
#define ITCM_END_ADDRESS   0x003FFFFFUL
 
#define ITCM_START_ADDRESS   0x00000000UL
 
#define MPU_AP_FULL_ACCESS   ( 0x03 << MPU_RASR_AP_Pos )
 
#define MPU_AP_NO_ACCESS   ( 0x00 << MPU_RASR_AP_Pos )
 
#define MPU_AP_PRIVILEGED_READ_WRITE   ( 0x01 << MPU_RASR_AP_Pos )
 
#define MPU_AP_PRIVILEGED_READONLY   ( 0x05 << MPU_RASR_AP_Pos )
 
#define MPU_AP_READONLY   ( 0x06 << MPU_RASR_AP_Pos )
 
#define MPU_AP_READONLY2   ( 0x07 << MPU_RASR_AP_Pos )
 
#define MPU_AP_RES   ( 0x04 << MPU_RASR_AP_Pos )
 
#define MPU_AP_UNPRIVILEGED_READONLY   ( 0x02 << MPU_RASR_AP_Pos )
 
#define MPU_DEFAULT_DTCM_REGION   ( 3 )
 
#define MPU_DEFAULT_IFLASH_REGION   ( 2 )
 
#define MPU_DEFAULT_ITCM_REGION   ( 1 )
 
#define MPU_DEFAULT_SDRAM_REGION   ( 8 )
 
#define MPU_DEFAULT_SRAM_REGION_1   ( 4 )
 
#define MPU_DEFAULT_SRAM_REGION_2   ( 5 )
 
#define MPU_ENABLE   ( 0x1 << MPU_CTRL_ENABLE_Pos)
 
#define MPU_EXT_EBI_REGION   ( 7 )
 
#define MPU_HFNMIENA   ( 0x1 << MPU_CTRL_HFNMIENA_Pos )
 
#define MPU_PERIPHERALS_REGION   ( 6 )
 
#define MPU_PRIVDEFENA   ( 0x1 << MPU_CTRL_PRIVDEFENA_Pos )
 
#define MPU_QSPIMEM_REGION   ( 9 )
 
#define MPU_REGION_BUFFERABLE   ( 0x01 << MPU_RASR_B_Pos )
 
#define MPU_REGION_CACHEABLE   ( 0x01 << MPU_RASR_C_Pos )
 
#define MPU_REGION_DISABLE   ( 0x0 )
 
#define MPU_REGION_ENABLE   ( 0x01 )
 
#define MPU_REGION_EXECUTE_NEVER   ( 0x01 << MPU_RASR_XN_Pos )
 
#define MPU_REGION_SHAREABLE   ( 0x01 << MPU_RASR_S_Pos )
 
#define MPU_REGION_VALID   ( 0x10 )
 
#define MPU_TEX_B000   ( 0x00 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B001   ( 0x01 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B010   ( 0x02 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B011   ( 0x03 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B100   ( 0x04 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B101   ( 0x05 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B110   ( 0x06 << MPU_RASR_TEX_Pos )
 
#define MPU_TEX_B111   ( 0x07 << MPU_RASR_TEX_Pos )
 
#define MPU_USBHSRAM_REGION   ( 10 )
 
#define NON_SHAREABLE   0
 
#define PERIPHERALS_END_ADDRESS   0x5FFFFFFFUL
 
#define PERIPHERALS_START_ADDRESS   0x40000000UL
 
#define PRIVILEGE_MODE   0
 
#define QSPI_END_ADDRESS   0x9FFFFFFFUL
 
#define QSPI_START_ADDRESS   0x80000000UL
 
#define SDRAM_END_ADDRESS   0x7FFFFFFFUL
 
#define SDRAM_START_ADDRESS   0x70000000UL
 
#define SHAREABLE   1
 
#define SHAREABLE_DEVICE_TYPE   (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ))
 
#define SRAM_END_ADDRESS   0x2045FFFFUL
 
#define SRAM_FIRST_END_ADDRESS   (SRAM_FIRST_START_ADDRESS + 0x3FFFF)
 
#define SRAM_FIRST_START_ADDRESS   (SRAM_START_ADDRESS)
 
#define SRAM_SECOND_END_ADDRESS   (SRAM_END_ADDRESS)
 
#define SRAM_SECOND_START_ADDRESS   (SRAM_FIRST_END_ADDRESS + 1)
 
#define SRAM_START_ADDRESS   0x20400000UL
 
#define STRONGLY_ORDERED_SHAREABLE_TYPE   (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( DISABLE << MPU_RASR_B_Pos ))
 
#define USBHSRAM_END_ADDRESS   0xA01FFFFFUL
 
#define USBHSRAM_START_ADDRESS   0xA0100000UL
 
#define USER_MODE   1
 

Functions

uint32_t mpu_cal_mpu_region_size (uint32_t dw_actual_size_in_bytes)
 Calculate region size for the RASR. More...
 
void mpu_disable_region (void)
 Disable the current active region. More...
 
void mpu_enable (uint32_t dw_mpu_enable)
 Enables the MPU module. More...
 
void mpu_set_region (uint32_t dw_region_base_addr, uint32_t dw_region_attr)
 Setup a memory region. More...
 
void mpu_set_region_num (uint32_t dw_region_num)
 Set active memory region. More...
 
void mpu_update_regions (uint32_t dw_region_num, uint32_t dw_region_base_addr, uint32_t dw_region_attr)
 Update MPU regions. More...
 

#define ARM_MODE_USR   0x10
#define DTCM_END_ADDRESS   0x203FFFFFUL

Referenced by _setup_memory_region().

#define DTCM_START_ADDRESS   0x20000000UL

Referenced by _setup_memory_region().

#define EXT_EBI_END_ADDRESS   0x6FFFFFFFUL

Referenced by _setup_memory_region().

#define EXT_EBI_START_ADDRESS   0x60000000UL

Referenced by _setup_memory_region().

#define IFLASH_END_ADDRESS   0x005FFFFFUL

Referenced by _setup_memory_region().

#define IFLASH_PRIVILEGE_END_ADDRESS   (IFLASH_START_ADDRESS + 0xFFF)
#define IFLASH_PRIVILEGE_START_ADDRESS   (IFLASH_START_ADDRESS)
#define IFLASH_START_ADDRESS   0x00400000UL

Referenced by _setup_memory_region().

#define IFLASH_UNPRIVILEGE_END_ADDRESS   (IFLASH_END_ADDRESS)
#define IFLASH_UNPRIVILEGE_START_ADDRESS   (IFLASH_PRIVILEGE_END_ADDRESS + 1)
#define INNER_NORMAL_WB_NWA_TYPE (   x)    (( 0x04 << MPU_RASR_TEX_Pos ) | ( ENABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos ))

Referenced by _setup_memory_region().

#define INNER_NORMAL_WB_RWA_TYPE (   x)    (( 0x04 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos ))

Referenced by _setup_memory_region().

#define INNER_OUTER_NORMAL_NOCACHE_TYPE (   x)    ((0x01 << MPU_RASR_TEX_Pos) | (DISABLE << MPU_RASR_C_Pos) | (DISABLE << MPU_RASR_B_Pos) | (x << MPU_RASR_S_Pos))

Referenced by _setup_memory_region().

#define ITCM_END_ADDRESS   0x003FFFFFUL

Referenced by _setup_memory_region().

#define ITCM_START_ADDRESS   0x00000000UL

Referenced by _setup_memory_region().

#define MPU_AP_FULL_ACCESS   ( 0x03 << MPU_RASR_AP_Pos )

Referenced by _setup_memory_region().

#define MPU_AP_NO_ACCESS   ( 0x00 << MPU_RASR_AP_Pos )
#define MPU_AP_PRIVILEGED_READ_WRITE   ( 0x01 << MPU_RASR_AP_Pos )

Referenced by _setup_memory_region().

#define MPU_AP_PRIVILEGED_READONLY   ( 0x05 << MPU_RASR_AP_Pos )
#define MPU_AP_READONLY   ( 0x06 << MPU_RASR_AP_Pos )

Referenced by _setup_memory_region().

#define MPU_AP_READONLY2   ( 0x07 << MPU_RASR_AP_Pos )
#define MPU_AP_RES   ( 0x04 << MPU_RASR_AP_Pos )
#define MPU_AP_UNPRIVILEGED_READONLY   ( 0x02 << MPU_RASR_AP_Pos )
#define MPU_DEFAULT_DTCM_REGION   ( 3 )

Referenced by _setup_memory_region().

#define MPU_DEFAULT_IFLASH_REGION   ( 2 )

Referenced by _setup_memory_region().

#define MPU_DEFAULT_ITCM_REGION   ( 1 )

Referenced by _setup_memory_region().

#define MPU_DEFAULT_SDRAM_REGION   ( 8 )

Referenced by _setup_memory_region().

#define MPU_DEFAULT_SRAM_REGION_1   ( 4 )

Referenced by _setup_memory_region().

#define MPU_DEFAULT_SRAM_REGION_2   ( 5 )

Referenced by _setup_memory_region().

#define MPU_ENABLE   ( 0x1 << MPU_CTRL_ENABLE_Pos)

Referenced by _setup_memory_region().

#define MPU_EXT_EBI_REGION   ( 7 )

Referenced by _setup_memory_region().

#define MPU_HFNMIENA   ( 0x1 << MPU_CTRL_HFNMIENA_Pos )
#define MPU_PERIPHERALS_REGION   ( 6 )

Referenced by _setup_memory_region().

#define MPU_PRIVDEFENA   ( 0x1 << MPU_CTRL_PRIVDEFENA_Pos )

Referenced by _setup_memory_region().

#define MPU_QSPIMEM_REGION   ( 9 )

Referenced by _setup_memory_region().

#define MPU_REGION_BUFFERABLE   ( 0x01 << MPU_RASR_B_Pos )
#define MPU_REGION_CACHEABLE   ( 0x01 << MPU_RASR_C_Pos )
#define MPU_REGION_DISABLE   ( 0x0 )
#define MPU_REGION_ENABLE   ( 0x01 )

Referenced by _setup_memory_region().

#define MPU_REGION_EXECUTE_NEVER   ( 0x01 << MPU_RASR_XN_Pos )

Referenced by _setup_memory_region().

#define MPU_REGION_SHAREABLE   ( 0x01 << MPU_RASR_S_Pos )
#define MPU_REGION_VALID   ( 0x10 )

Referenced by _setup_memory_region().

#define MPU_TEX_B000   ( 0x00 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B001   ( 0x01 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B010   ( 0x02 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B011   ( 0x03 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B100   ( 0x04 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B101   ( 0x05 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B110   ( 0x06 << MPU_RASR_TEX_Pos )
#define MPU_TEX_B111   ( 0x07 << MPU_RASR_TEX_Pos )
#define MPU_USBHSRAM_REGION   ( 10 )

Referenced by _setup_memory_region().

#define NON_SHAREABLE   0

Referenced by _setup_memory_region().

#define PERIPHERALS_END_ADDRESS   0x5FFFFFFFUL

Referenced by _setup_memory_region().

#define PERIPHERALS_START_ADDRESS   0x40000000UL

Referenced by _setup_memory_region().

#define PRIVILEGE_MODE   0
#define QSPI_END_ADDRESS   0x9FFFFFFFUL

Referenced by _setup_memory_region().

#define QSPI_START_ADDRESS   0x80000000UL

Referenced by _setup_memory_region().

#define SDRAM_END_ADDRESS   0x7FFFFFFFUL

Referenced by _setup_memory_region().

#define SDRAM_START_ADDRESS   0x70000000UL

Referenced by _setup_memory_region().

#define SHAREABLE   1

Referenced by _setup_memory_region().

#define SHAREABLE_DEVICE_TYPE   (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ))

Referenced by _setup_memory_region().

#define SRAM_END_ADDRESS   0x2045FFFFUL
#define SRAM_FIRST_END_ADDRESS   (SRAM_FIRST_START_ADDRESS + 0x3FFFF)

Referenced by _setup_memory_region().

#define SRAM_FIRST_START_ADDRESS   (SRAM_START_ADDRESS)

Referenced by _setup_memory_region().

#define SRAM_SECOND_END_ADDRESS   (SRAM_END_ADDRESS)

Referenced by _setup_memory_region().

#define SRAM_SECOND_START_ADDRESS   (SRAM_FIRST_END_ADDRESS + 1)

Referenced by _setup_memory_region().

#define SRAM_START_ADDRESS   0x20400000UL
#define STRONGLY_ORDERED_SHAREABLE_TYPE   (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( DISABLE << MPU_RASR_B_Pos ))

Referenced by _setup_memory_region().

#define USBHSRAM_END_ADDRESS   0xA01FFFFFUL

Referenced by _setup_memory_region().

#define USBHSRAM_START_ADDRESS   0xA0100000UL

Referenced by _setup_memory_region().

#define USER_MODE   1