This example shows how to implement the SD/MMC stack with the FatFS. It will mount the file system and write a file in the card.
The example outputs the information through the standard output (stdio). To know the output used on the board, look in the conf_example.h file and connect a terminal to the correct port.
While using Xplained Pro evaluation kits, please attach I/O1 Xplained Pro extension board to EXT1.