SAMV71-XULTRA board init.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
#include "board.h"
#include "conf_board.h"
#include "ioport.h"
#include "pio.h"
#include "mpu.h"
Macros | |
#define | ioport_set_pin_input_mode(pin, mode, sense) |
Set input mode for one single IOPORT pin. More... | |
#define | ioport_set_pin_peripheral_mode(pin, mode) |
Set peripheral mode for one single IOPORT pin. More... | |
#define | ioport_set_port_peripheral_mode(port, masks, mode) |
Set peripheral mode for IOPORT pins. More... | |
Functions | |
static void | _setup_memory_region (void) |
Default memory map Address range Memory region Memory type Shareability Cache policy 0x00000000- 0x1FFFFFFF Code Normal Non-shareable WT 0x20000000- 0x3FFFFFFF SRAM Normal Non-shareable WBWA 0x40000000- 0x5FFFFFFF Peripheral Device Non-shareable - 0x60000000- 0x7FFFFFFF RAM Normal Non-shareable WBWA 0x80000000- 0x9FFFFFFF RAM Normal Non-shareable WT 0xA0000000- 0xBFFFFFFF Device Device Shareable 0xC0000000- 0xDFFFFFFF Device Device Non Shareable 0xE0000000- 0xFFFFFFFF System - -. More... | |
void | board_init (void) |
This function initializes the board target resources. More... | |
static void | tcm_disable (void) |
TCM memory Disable. More... | |
#define ioport_set_pin_input_mode | ( | pin, | |
mode, | |||
sense | |||
) |
Set input mode for one single IOPORT pin.
It will configure port mode and disable pin mode (but enable peripheral).
pin | IOPORT pin to configure |
mode | Mode masks to configure for the specified pin (IOPORT Modes) |
sense | Sense for interrupt detection (ioport_sense) |
Referenced by board_init().
#define ioport_set_pin_peripheral_mode | ( | pin, | |
mode | |||
) |
Set peripheral mode for one single IOPORT pin.
It will configure port mode and disable pin mode (but enable peripheral).
pin | IOPORT pin to configure |
mode | Mode masks to configure for the specified pin (IOPORT Modes) |
Referenced by board_init().
#define ioport_set_port_peripheral_mode | ( | port, | |
masks, | |||
mode | |||
) |
Set peripheral mode for IOPORT pins.
It will configure port mode and disable pin mode (but enable peripheral).
port | IOPORT port to configure |
masks | IOPORT pin masks to configure |
mode | Mode masks to configure for the specified pin (IOPORT Modes) |
|
static |
Default memory map Address range Memory region Memory type Shareability Cache policy 0x00000000- 0x1FFFFFFF Code Normal Non-shareable WT 0x20000000- 0x3FFFFFFF SRAM Normal Non-shareable WBWA 0x40000000- 0x5FFFFFFF Peripheral Device Non-shareable - 0x60000000- 0x7FFFFFFF RAM Normal Non-shareable WBWA 0x80000000- 0x9FFFFFFF RAM Normal Non-shareable WT 0xA0000000- 0xBFFFFFFF Device Device Shareable 0xC0000000- 0xDFFFFFFF Device Device Non Shareable 0xE0000000- 0xFFFFFFFF System - -.
Set up a memory region.
ITCM memory region — Normal START_Addr:- 0x00000000UL END_Addr:- 0x00400000UL
Internal flash memory region — Normal read-only (update to Strongly ordered in write accesses) START_Addr:- 0x00400000UL END_Addr:- 0x00600000UL
DTCM memory region — Normal START_Addr:- 0x20000000L END_Addr:- 0x20400000UL
SRAM Cacheable memory region — Normal START_Addr:- 0x20400000UL END_Addr:- 0x2043FFFFUL
Internal SRAM second partition memory region — Normal START_Addr:- 0x20440000UL END_Addr:- 0x2045FFFFUL
Peripheral memory region — DEVICE Shareable START_Addr:- 0x40000000UL END_Addr:- 0x5FFFFFFFUL
External EBI memory memory region — Strongly Ordered START_Addr:- 0x60000000UL END_Addr:- 0x6FFFFFFFUL
SDRAM cacheable memory region — Normal START_Addr:- 0x70000000UL END_Addr:- 0x7FFFFFFFUL
QSPI memory region — Strongly ordered START_Addr:- 0x80000000UL END_Addr:- 0x9FFFFFFFUL
USB RAM Memory region — Device START_Addr:- 0xA0100000UL END_Addr:- 0xA01FFFFFUL
References DTCM_END_ADDRESS, DTCM_START_ADDRESS, EXT_EBI_END_ADDRESS, EXT_EBI_START_ADDRESS, IFLASH_END_ADDRESS, IFLASH_START_ADDRESS, INNER_NORMAL_WB_NWA_TYPE, INNER_NORMAL_WB_RWA_TYPE, INNER_OUTER_NORMAL_NOCACHE_TYPE, ITCM_END_ADDRESS, ITCM_START_ADDRESS, MPU_AP_FULL_ACCESS, MPU_AP_PRIVILEGED_READ_WRITE, MPU_AP_READONLY, mpu_cal_mpu_region_size(), MPU_DEFAULT_DTCM_REGION, MPU_DEFAULT_IFLASH_REGION, MPU_DEFAULT_ITCM_REGION, MPU_DEFAULT_SDRAM_REGION, MPU_DEFAULT_SRAM_REGION_1, MPU_DEFAULT_SRAM_REGION_2, MPU_ENABLE, mpu_enable(), MPU_EXT_EBI_REGION, MPU_PERIPHERALS_REGION, MPU_PRIVDEFENA, MPU_QSPIMEM_REGION, MPU_REGION_ENABLE, MPU_REGION_EXECUTE_NEVER, MPU_REGION_VALID, mpu_set_region(), MPU_USBHSRAM_REGION, NON_SHAREABLE, PERIPHERALS_END_ADDRESS, PERIPHERALS_START_ADDRESS, QSPI_END_ADDRESS, QSPI_START_ADDRESS, SDRAM_END_ADDRESS, SDRAM_START_ADDRESS, SHAREABLE, SHAREABLE_DEVICE_TYPE, SRAM_FIRST_END_ADDRESS, SRAM_FIRST_START_ADDRESS, SRAM_SECOND_END_ADDRESS, SRAM_SECOND_START_ADDRESS, STRONGLY_ORDERED_SHAREABLE_TYPE, USBHSRAM_END_ADDRESS, and USBHSRAM_START_ADDRESS.
Referenced by board_init().
|
inlinestatic |