Board configuration.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | CONF_BOARD_COM_PORT |
Enable Com Port. More... | |
#define | CONF_BOARD_SPI |
Enable the SPI PINs. More... | |
#define | CONF_BOARD_SPI_NPCS3 |
#define | DATA_FLASH_LED_EXAMPLE_0_ACTIVE_LEVEL LED0_ACTIVE_LEVEL |
#define | DATA_FLASH_LED_EXAMPLE_0_GPIO LED0_GPIO |
LED used for the example. More... | |
#define | DATA_FLASH_LED_EXAMPLE_0_INACTIVE_LEVEL LED0_INACTIVE_LEVEL |
#define | DATA_FLASH_LED_EXAMPLE_1_ACTIVE_LEVEL LED0_ACTIVE_LEVEL |
#define | DATA_FLASH_LED_EXAMPLE_1_GPIO LED0_GPIO |
#define | DATA_FLASH_LED_EXAMPLE_1_INACTIVE_LEVEL LED0_INACTIVE_LEVEL |
#define CONF_BOARD_COM_PORT |
Enable Com Port.
#define CONF_BOARD_SPI |
Enable the SPI PINs.
#define CONF_BOARD_SPI_NPCS3 |
#define DATA_FLASH_LED_EXAMPLE_0_ACTIVE_LEVEL LED0_ACTIVE_LEVEL |
#define DATA_FLASH_LED_EXAMPLE_0_GPIO LED0_GPIO |
LED used for the example.
#define DATA_FLASH_LED_EXAMPLE_0_INACTIVE_LEVEL LED0_INACTIVE_LEVEL |
#define DATA_FLASH_LED_EXAMPLE_1_ACTIVE_LEVEL LED0_ACTIVE_LEVEL |
#define DATA_FLASH_LED_EXAMPLE_1_GPIO LED0_GPIO |
#define DATA_FLASH_LED_EXAMPLE_1_INACTIVE_LEVEL LED0_INACTIVE_LEVEL |