Microchip® Advanced Software Framework

conf_board.h File Reference

Board configuration.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Macros

#define CONF_BOARD_COM_PORT
 Enable Com Port. More...
 
#define CONF_BOARD_SPI
 Enable the SPI PINs. More...
 
#define CONF_BOARD_SPI_NPCS2
 
#define DATA_FLASH_LED_EXAMPLE_0_ACTIVE_LEVEL   LED0_ACTIVE_LEVEL
 
#define DATA_FLASH_LED_EXAMPLE_0_GPIO   LED0_GPIO
 LED used for the example. More...
 
#define DATA_FLASH_LED_EXAMPLE_0_INACTIVE_LEVEL   LED0_INACTIVE_LEVEL
 
#define DATA_FLASH_LED_EXAMPLE_1_ACTIVE_LEVEL   LED0_ACTIVE_LEVEL
 
#define DATA_FLASH_LED_EXAMPLE_1_GPIO   LED0_GPIO
 
#define DATA_FLASH_LED_EXAMPLE_1_INACTIVE_LEVEL   LED0_INACTIVE_LEVEL
 

#define CONF_BOARD_COM_PORT

Enable Com Port.

#define CONF_BOARD_SPI

Enable the SPI PINs.

#define CONF_BOARD_SPI_NPCS2
#define DATA_FLASH_LED_EXAMPLE_0_ACTIVE_LEVEL   LED0_ACTIVE_LEVEL
#define DATA_FLASH_LED_EXAMPLE_0_GPIO   LED0_GPIO

LED used for the example.

#define DATA_FLASH_LED_EXAMPLE_0_INACTIVE_LEVEL   LED0_INACTIVE_LEVEL
#define DATA_FLASH_LED_EXAMPLE_1_ACTIVE_LEVEL   LED0_ACTIVE_LEVEL
#define DATA_FLASH_LED_EXAMPLE_1_GPIO   LED0_GPIO
#define DATA_FLASH_LED_EXAMPLE_1_INACTIVE_LEVEL   LED0_INACTIVE_LEVEL