Microchip® Advanced Software Framework

conf_board.h File Reference

Board configuration.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Macros

#define CONF_BOARD_SPI
 Enable the SPI PINs. More...
 
#define CONF_BOARD_SPI_NPCS3
 
#define CONF_BOARD_UART_CONSOLE
 Enable Com Port. More...
 
#define DATA_FLASH_LED_EXAMPLE_0   LED0
 LED used for the example. More...
 
#define DATA_FLASH_LED_EXAMPLE_1   LED0
 

#define CONF_BOARD_SPI

Enable the SPI PINs.

#define CONF_BOARD_SPI_NPCS3
#define CONF_BOARD_UART_CONSOLE

Enable Com Port.

#define DATA_FLASH_LED_EXAMPLE_0   LED0

LED used for the example.

#define DATA_FLASH_LED_EXAMPLE_1   LED0