Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
PLL Management

This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs.

A PLL will take an input signal (the source), optionally divide the frequency by a configurable divider, and then multiply the frequency by a configurable multiplier.

Some devices don't support input dividers; specifying any other divisor than 1 on these devices will result in an assertion failure. Other devices may have various restrictions to the frequency range of the input and output signals.

Example: Setting up PLL0 with default parameters

The following example shows how to configure and enable PLL0 using the default parameters specified using the configuration symbols listed above.

To configure, enable PLL0 using the default parameters and to disable a specific feature like Wide Bandwidth Mode (a UC3A3-specific PLL option.), you can use this initialization process.

struct pll_config pllcfg;
if (pll_is_locked(pll_id)) {
return; // Pll already running
}
pll_enable_source(CONFIG_PLL0_SOURCE);
pll_config_defaults(&pllcfg, 0);
pll_config_set_option(&pllcfg, PLL_OPT_WBM_DISABLE);
pll_enable(&pllcfg, 0);

When the last function call returns, PLL0 is ready to be used as the main system clock source.

Configuration Symbols

Each PLL has a set of default parameters determined by the following configuration symbols in the application's configuration file:

These configuration symbols determine the result of calling pll_config_defaults() and pll_get_default_rate().

Data Structures

struct  pll_config
 Hardware-specific representation of PLL configuration. More...
 

Enumerations

enum  pll_source {
  PLL_SRC_RC2MHZ = OSC_PLLSRC_RC2M_gc,
  PLL_SRC_RC32MHZ = OSC_PLLSRC_RC32M_gc,
  PLL_SRC_XOSC = OSC_PLLSRC_XOSC_gc
}
 PLL clock source. More...
 

Functions

static uint32_t pll_get_default_rate_priv (enum pll_source src, unsigned int mul, unsigned int div)
 Return clock rate for specified PLL settings. More...
 

Chip-specific PLL characteristics

#define NR_PLLS   1
 Number of on-chip PLLs. More...
 
#define PLL_MIN_HZ   10000000UL
 Minimum frequency that the PLL can generate. More...
 
#define PLL_MAX_HZ   200000000UL
 Maximum frequency that the PLL can generate. More...
 
#define PLL_NR_OPTIONS   0
 Number of PLL option bits. More...
 

PLL configuration

static void pll_config_init (struct pll_config *cfg, enum pll_source src, unsigned int div, unsigned int mul)
 Initialize PLL configuration from standard parameters. More...
 
static void pll_config_read (struct pll_config *cfg, unsigned int pll_id)
 Read the currently active configuration of pll_id. More...
 
static void pll_config_write (const struct pll_config *cfg, unsigned int pll_id)
 Activate the configuration cfg on pll_id. More...
 
#define pll_config_defaults(cfg, pll_id)
 Initialize PLL configuration using default parameters. More...
 
#define pll_get_default_rate(pll_id)
 Get the default rate in Hz of pll_id. More...
 

Interaction with the PLL hardware

static int pll_wait_for_lock (unsigned int pll_id)
 Wait for PLL pll_id to become locked. More...
 
static void pll_enable (const struct pll_config *cfg, unsigned int pll_id)
 Activate the configuration cfg and enable PLL pll_id. More...
 
static void pll_disable (unsigned int pll_id)
 Disable the PLL identified by pll_id. More...
 
static bool pll_is_locked (unsigned int pll_id)
 Determine whether the PLL is locked or not. More...
 
static void pll_enable_source (enum pll_source src)
 Enable the source of the pll. More...
 
static void pll_enable_config_defaults (unsigned int pll_id)
 Enable the pll with the default configuration. More...
 

#define NR_PLLS   1
#define pll_config_defaults (   cfg,
  pll_id 
)
Value:
CONFIG_PLL##pll_id##_SOURCE, \
CONFIG_PLL##pll_id##_DIV, \
CONFIG_PLL##pll_id##_MUL)
static void pll_config_init(struct pll_config *cfg, enum pll_source src, unsigned int div, unsigned int mul)
Initialize PLL configuration from standard parameters.
Definition: xmega/pll.h:128

Initialize PLL configuration using default parameters.

After this function returns, cfg will contain a configuration which will make the PLL run at (CONFIG_PLLx_MUL / CONFIG_PLLx_DIV) times the frequency of CONFIG_PLLx_SOURCE.

Parameters
cfgThe PLL configuration to be initialized.
pll_idUse defaults for this PLL.
#define pll_get_default_rate (   pll_id)
Value:
pll_get_default_rate_priv(CONFIG_PLL##pll_id##_SOURCE, \
CONFIG_PLL##pll_id##_MUL, \
CONFIG_PLL##pll_id##_DIV)
static uint32_t pll_get_default_rate_priv(enum pll_source src, unsigned int mul, unsigned int div)
Return clock rate for specified PLL settings.
Definition: xmega/pll.h:79

Get the default rate in Hz of pll_id.

Referenced by sysclk_get_main_hz().

#define PLL_MAX_HZ   200000000UL

Maximum frequency that the PLL can generate.

Referenced by pll_get_default_rate_priv().

#define PLL_MIN_HZ   10000000UL

Minimum frequency that the PLL can generate.

Referenced by pll_get_default_rate_priv().

#define PLL_NR_OPTIONS   0

Number of PLL option bits.

enum pll_source

PLL clock source.

Enumerator
PLL_SRC_RC2MHZ 

2 MHz Internal RC Oscillator

PLL_SRC_RC32MHZ 

32 MHz Internal RC Oscillator

PLL_SRC_XOSC 

External Clock Source.

void pll_config_init ( struct pll_config cfg,
enum pll_source  src,
unsigned int  div,
unsigned int  mul 
)
inlinestatic

Initialize PLL configuration from standard parameters.

Note
The XMEGA PLL hardware uses hard-wired input dividers, so the user must ensure that div is set as follows:
  • If src is PLL_SRC_32MHZ, div must be set to 4.
  • Otherwise, div must be set to 1.
This function may be defined inline because it is assumed to be called very few times, and usually with constant parameters. Inlining it will in such cases reduce the code size significantly.
Parameters
cfgThe PLL configuration to be initialized.
srcThe oscillator to be used as input to the PLL.
divPLL input divider.
mulPLL loop divider (i.e. multiplier).
Returns
A configuration which will make the PLL run at (mul / div) times the frequency of src

References Assert, pll_config::ctrl, and PLL_SRC_RC32MHZ.

Referenced by pll_enable_config_defaults().

void pll_config_read ( struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Read the currently active configuration of pll_id.

Parameters
cfgThe configuration object into which to store the currently active configuration.
pll_idThe ID of the PLL to be accessed.

References Assert, pll_config::ctrl, and NR_PLLS.

void pll_config_write ( const struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Activate the configuration cfg on pll_id.

Parameters
cfgThe configuration object representing the PLL configuration to be activated.
pll_idThe ID of the PLL to be updated.

References Assert, pll_config::ctrl, and NR_PLLS.

Referenced by pll_enable().

void pll_disable ( unsigned int  pll_id)
inlinestatic

Disable the PLL identified by pll_id.

Note
This will not automatically disable the reference oscillator that is configured for the PLL.

After this function is called, the PLL identified by pll_id will be disabled. The PLL configuration stored in hardware may be affected by this, so if the caller needs to restore the same configuration later, it should either do a pll_config_read() before disabling the PLL, or remember the last configuration written to the PLL.

Parameters
pll_idThe ID of the PLL to be disabled.

References Assert, cpu_irq_restore(), cpu_irq_save(), and NR_PLLS.

void pll_enable ( const struct pll_config cfg,
unsigned int  pll_id 
)
inlinestatic

Activate the configuration cfg and enable PLL pll_id.

Note
If a different PLL reference oscillator than those enabled by sysclk_init() is used, the user must ensure that the desired reference is enabled prior to calling this function.
Parameters
cfgThe PLL configuration to be activated.
pll_idThe ID of the PLL to be enabled.

References Assert, cpu_irq_restore(), cpu_irq_save(), NR_PLLS, and pll_config_write().

Referenced by pll_enable_config_defaults().

void pll_enable_config_defaults ( unsigned int  pll_id)
inlinestatic

Enable the pll with the default configuration.

PLL is enabled, if the PLL is not already locked.

Parameters
pll_idThe ID of the PLL to enable.

References Assert, pll_config_init(), pll_enable(), pll_enable_source(), and pll_is_locked().

Referenced by sysclk_init().

void pll_enable_source ( enum pll_source  src)
inlinestatic

Enable the source of the pll.

The source is enabled, if the source is not already running.

Parameters
srcThe ID of the PLL source to enable.

References Assert, osc_enable(), osc_enable_autocalibration(), OSC_ID_RC32MHZ, OSC_ID_USBSOF, OSC_ID_XOSC, osc_is_ready(), osc_wait_ready(), PLL_SRC_RC2MHZ, PLL_SRC_RC32MHZ, and PLL_SRC_XOSC.

Referenced by pll_enable_config_defaults().

static uint32_t pll_get_default_rate_priv ( enum pll_source  src,
unsigned int  mul,
unsigned int  div 
)
inlinestatic

Return clock rate for specified PLL settings.

Note
Due to the hardware implementation of the PLL, div must be 4 if the 32 MHz RC oscillator is used as reference and 1 otherwise. The reference must be above 440 kHz, and the output between 10 and 200 MHz.
Parameters
srcID of the PLL's reference source oscillator.
mulMultiplier for the PLL.
divDivisor for the PLL.
Return values
Outputclock rate from PLL.

References Assert, CONFIG_OSC_RC32_CAL, osc_get_rate(), OSC_ID_XOSC, PLL_MAX_HZ, PLL_MIN_HZ, PLL_SRC_RC2MHZ, PLL_SRC_RC32MHZ, and PLL_SRC_XOSC.

bool pll_is_locked ( unsigned int  pll_id)
inlinestatic

Determine whether the PLL is locked or not.

Parameters
pll_idThe ID of the PLL to check.
Return values
trueThe PLL is locked and ready to use as a clock source
falseThe PLL is not yet locked, or has not been enabled.

References Assert, and NR_PLLS.

Referenced by pll_enable_config_defaults(), and pll_wait_for_lock().

static int pll_wait_for_lock ( unsigned int  pll_id)
inlinestatic

Wait for PLL pll_id to become locked.

Todo:
Use a timeout to avoid waiting forever and hanging the system
Parameters
pll_idThe ID of the PLL to wait for.
Return values
STATUS_OKThe PLL is now locked.
ERR_TIMEOUTTimed out waiting for PLL to become locked.

References Assert, NR_PLLS, and pll_is_locked().