License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
"SAM4S-XPLAINED - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM4S-XPLAINED - Board informations" | This page lists several definition related to the board description |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the System Clock Management service (SAM4S) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Advanced use case - Peripheral Bus Clock Management (SAM4S) | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for USB device mouse module (UDI mouse) | This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID mouse in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for the maXTouch component | This is the quick start guide for the maXTouch component The guide will give you a step-by-step introduction on how to setup and use the component to be able to read touch responses from the maXTouch Xplained kit |
Quickstart guide for Common service TWI | This is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the graphics service | This is the quick start guide for the Graphics (GFX) service", with step-by-step instructions on how to configure and use it for a specific use case |
Quick Start Guide for the ILI9341 Display Controller Component Driver | This is the quick start guide for the ILI9341 Display Controller Component Driver, with step-by-step instructions on how to configure and use the component driver for specific use cases |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Quickstart guide for SAM SPI driver | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Peripheral DMA Controller | |
Examples for Peripheral DMA Controller | This is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver |
 Quick Start Guide for PDC - Basic | This is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver |
 Peripheral DMA Controller Example | |
Document Revision History | |
Todo List | |
Deprecated List | |