In this use case, the USART module is configured for:
- Using USART0
- Baudrate: 9600
- Character length: 8 bit
- Parity mode: Disabled
- Stop bit: None
- RS232 mode
The use case waits for a received character on the configured USART and echoes the character back to the same USART.
Setup steps
Prerequisites
- System Clock Management (sysclock)
- Common IOPORT API (ioport)
Example code
The following configuration must be added to the project (typically to a conf_usart.h file, but it can also be added to your main application file.):
#define USART_SERIAL USART0
#define USART_SERIAL_ID ID_USART0 //USART0 for sam4l
#define USART_SERIAL_BAUDRATE 9600
#define USART_SERIAL_CHAR_LENGTH US_MR_CHRL_8_BIT
#define USART_SERIAL_PARITY US_MR_PAR_NO
#define USART_SERIAL_STOP_BIT US_MR_NBSTOP_1_BIT
A variable for the received byte must be added:
Add to application initialization:
USART_SERIAL_BAUDRATE,
US_MR_CHMODE_NORMAL
};
#if SAM4L
#else
#endif
Workflow
- Initialize system clock:
- Configure the USART Tx and Rx pins by call the board init function:
- Note
- Set the following define in conf_board.h file to enable COM port,it will be used in board_init() function to set up IOPorts for the USART pins. For SAM4L:
#define CONF_BOARD_COM_PORT
For other SAM devices: #define CONF_BOARD_UART_CONSOLE
- Create USART options struct:
USART_SERIAL_BAUDRATE,
US_MR_CHMODE_NORMAL
};
- Enable the clock to the USART module:
- Initialize the USART module in RS232 mode:
- Enable the Rx and Tx modes of the USART module:
Usage steps
Example code
Add to, e.g., main loop in application C-file:
Workflow
- Wait for reception of a character:
- Echo the character back: