#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(2)] |
uint8 | u8NumOfSlot |
uint8 | u8SlotTime |
uint8 tstrM2MScanOption::u8NumOfSlot |
The min number of slots is 2 for every channel,
every slot the soc will send Probe Req on air, and wait/listen for PROBE RESP/BEACONS for the u16slotTime
Referenced by m2m_wifi_set_scan_options().
uint8 tstrM2MScanOption::u8SlotTime |
the time that the Soc will wait on every channel listening to the frames on air when that time increaseed number of AP will increased in the scan results min time is 10 ms and the max is 250 ms
Referenced by m2m_wifi_set_scan_options().