#include <m2m_types.h>
Data Fields | |
uint8 | antenna1 |
uint8 | antenna2 |
uint8 | gpio_mode |
uint8 | mode |
uint8 tstrM2mAntDivParams::antenna1 |
Antenna1 WILC GPIO number selection
Referenced by m2m_wifi_set_antenna_mode().
uint8 tstrM2mAntDivParams::antenna2 |
Antenna2 WILC GPIO number selection
Referenced by m2m_wifi_set_antenna_mode().
uint8 tstrM2mAntDivParams::gpio_mode |
Antenna GPIO Switch mode - Single=1, Dual=2 or None=0
Referenced by m2m_wifi_set_antenna_mode().
uint8 tstrM2mAntDivParams::mode |
Antenna Selection mode
Referenced by m2m_wifi_set_antenna_mode().