Stack-internal timers implementation.
This file includes timer callbacks for stack-internal timers as well as functions to set up or stop timers and check for expired timers.
#include "lwip/opt.h"
#include "lwip/timers.h"
#include "lwip/tcp_impl.h"
#include "lwip/def.h"
#include "lwip/memp.h"
#include "lwip/tcpip.h"
#include "lwip/ip_frag.h"
#include "netif/etharp.h"
#include "lwip/dhcp.h"
#include "lwip/autoip.h"
#include "lwip/igmp.h"
#include "lwip/dns.h"
#include "lwip/nd6.h"
#include "lwip/ip6_frag.h"
#include "lwip/mld6.h"
#include "lwip/sys.h"
#include "lwip/pbuf.h"
Functions | |
static void | arp_timer (void *arg) |
Timer callback function that calls etharp_tmr() and reschedules itself. More... | |
static void | autoip_timer (void *arg) |
Timer callback function that calls autoip_tmr() and reschedules itself. More... | |
static void | dhcp_timer_coarse (void *arg) |
Timer callback function that calls dhcp_coarse_tmr() and reschedules itself. More... | |
static void | dhcp_timer_fine (void *arg) |
Timer callback function that calls dhcp_fine_tmr() and reschedules itself. More... | |
static void | dns_timer (void *arg) |
Timer callback function that calls dns_tmr() and reschedules itself. More... | |
if (timeout==NULL) | |
if (next_timeout==NULL) | |
if (next_timeout->time > msecs) | |
static void | ip6_reass_timer (void *arg) |
Timer callback function that calls ip6_reass_tmr() and reschedules itself. More... | |
static void | ip_reass_timer (void *arg) |
Timer callback function that calls ip_reass_tmr() and reschedules itself. More... | |
static void | mld6_timer (void *arg) |
Timer callback function that calls mld6_tmr() and reschedules itself. More... | |
static void | nd6_timer (void *arg) |
Timer callback function that calls nd6_tmr() and reschedules itself. More... | |
void | sys_timeouts_init (void) |
Initialize this module. More... | |
void | tcp_timer_needed (void) |
Called from TCP_REG when registering a new PCB: the reason is to have the TCP timer only running when there are active (or time-wait) PCBs. More... | |
static void | tcpip_tcp_timer (void *arg) |
Timer callback function that calls tcp_tmr() and reschedules itself. More... | |
Variables | |
timeout | arg = arg |
timeout | h = handler |
timeout | next = NULL |
static struct sys_timeo * | next_timeout |
The one and only timeout list. More... | |
static int | tcpip_tcp_timer_active |
global variable that shows if the tcp timer is currently scheduled or not More... | |
timeout | time = msecs |
timeout = (struct sys_timeo *)memp_malloc(MEMP_SYS_TIMEOUT) | |
void | |
Create a one-shot timer (aka timeout). More... | |
Timer callback function that calls etharp_tmr() and reschedules itself.
arg | unused argument |
References ARP_TMR_INTERVAL, etharp_tmr(), LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls autoip_tmr() and reschedules itself.
arg | unused argument |
References autoip_tmr(), AUTOIP_TMR_INTERVAL, LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls dhcp_coarse_tmr() and reschedules itself.
arg | unused argument |
References DHCP_COARSE_TIMER_MSECS, dhcp_coarse_tmr(), LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls dhcp_fine_tmr() and reschedules itself.
arg | unused argument |
References DHCP_FINE_TIMER_MSECS, dhcp_fine_tmr(), LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls dns_tmr() and reschedules itself.
arg | unused argument |
References dns_tmr(), DNS_TMR_INTERVAL, LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
References LWIP_ASSERT, and NULL.
if | ( | next_timeout | = = NULL | ) |
References timeout.
if | ( | next_timeout-> | time, |
msecs | |||
) |
References sys_timeo::next, next_timeout, sys_timeo::time, and timeout.
Timer callback function that calls ip6_reass_tmr() and reschedules itself.
arg | unused argument |
References ip6_reass_tmr(), IP6_REASS_TMR_INTERVAL, LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls ip_reass_tmr() and reschedules itself.
arg | unused argument |
References ip_reass_tmr(), IP_TMR_INTERVAL, LWIP_DEBUGF, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls mld6_tmr() and reschedules itself.
arg | unused argument |
References LWIP_DEBUGF, mld6_tmr(), MLD6_TMR_INTERVAL, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Timer callback function that calls nd6_tmr() and reschedules itself.
arg | unused argument |
References LWIP_DEBUGF, nd6_tmr(), ND6_TMR_INTERVAL, NULL, sys_timeout(), and TIMERS_DEBUG.
Referenced by sys_timeouts_init().
Initialize this module.
References arp_timer(), ARP_TMR_INTERVAL, autoip_timer(), AUTOIP_TMR_INTERVAL, DHCP_COARSE_TIMER_MSECS, DHCP_FINE_TIMER_MSECS, dhcp_timer_coarse(), dhcp_timer_fine(), dns_timer(), DNS_TMR_INTERVAL, ip6_reass_timer(), IP6_REASS_TMR_INTERVAL, ip_reass_timer(), IP_TMR_INTERVAL, mld6_timer(), MLD6_TMR_INTERVAL, nd6_timer(), ND6_TMR_INTERVAL, NULL, sys_now(), and sys_timeout().
Referenced by lwip_init().
Called from TCP_REG when registering a new PCB: the reason is to have the TCP timer only running when there are active (or time-wait) PCBs.
External function (implemented in timers.c), called when TCP detects that a timer is needed (i.e.
References NULL, sys_timeout(), tcp_active_pcbs, TCP_TMR_INTERVAL, tcp_tw_pcbs, tcpip_tcp_timer(), and tcpip_tcp_timer_active.
Timer callback function that calls tcp_tmr() and reschedules itself.
arg | unused argument |
References NULL, sys_timeout(), tcp_active_pcbs, tcp_tmr(), TCP_TMR_INTERVAL, tcp_tw_pcbs, and tcpip_tcp_timer_active.
Referenced by tcp_timer_needed().
timeout arg = arg |
timeout h = handler |
Referenced by tcpip_timeout(), and tcpip_untimeout().
Referenced by mld6_stop(), netif_set_ipaddr(), tcp_fasttmr(), tcp_oos_insert_segment(), tcp_receive(), and tcp_segs_free().
|
static |
global variable that shows if the tcp timer is currently scheduled or not
Referenced by tcp_timer_needed(), and tcpip_tcp_timer().
timeout time = msecs |
Referenced by nd6_new_neighbor_cache_entry().
timeout = (struct sys_timeo *)memp_malloc(MEMP_SYS_TIMEOUT) |
Referenced by chip_deinit(), dhcp_bind(), if(), spi_read(), spi_write(), and usart_set_rx_timeout().
void |
Create a one-shot timer (aka timeout).
Timeouts are processed in the following cases:
msecs | time in milliseconds after that the timer should expire |
handler | callback function to call when msecs have elapsed |
arg | argument to pass to the callback function |
Referenced by nd6_select_router(), netif_null_output_ip6(), pmc_enable_waitmode(), portTASK_FUNCTION(), prvHelpCommand(), prvInitialiseTCBVariables(), prvProcessExpiredTimer(), prvProcessReceivedCommands(), prvSwitchTimerLists(), prvTimerTask(), stdio_serial_init(), vTaskPrioritySet(), xQueueCreateMutex(), xQueueGenericCreate(), xQueueGenericReceive(), and xQueueGenericSend().