AP Configuration.
This structure holds the configuration parameters for the M2M AP mode. It should be set by the application when it requests to enable the M2M AP operation mode. The M2M AP mode currently supports only WEP security (with the NO Security option availabe of course).
#include <m2m_types.h>
uint8 tstrM2MAPConfig::__PAD__[PAD_SZ(2+M2M_MAX_SSID_LEN+5+sizeof(tuniM2MWifiAuth))] |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2MAPConfig::au8SSID[M2M_MAX_SSID_LEN] |
AP SSID
uint16 tstrM2MAPConfig::u16BeaconInterval |
< Configuration parameters for the WiFi AP. Time between two consecutive beacons in TUs (1024 usec). A value of 0 would use the FW default
uint8 tstrM2MAPConfig::u8IsPMKUsed |
set to true if the PMK is calculated on the host .
Referenced by m2m_wifi_enable_ap().
uint8 tstrM2MAPConfig::u8ListenChannel |
Wi-Fi RF Channel which the AP will operate on
uint8 tstrM2MAPConfig::u8MaxSupportedSta |
Max supported stations for AP. Val 0 considered as default 8 stations Val > 8 are considered upto 8 stations
uint8 tstrM2MAPConfig::u8SecType |
Security type: Open, WEP and WPA2 modes supported as defined in tenuM2mSecType
uint8 tstrM2MAPConfig::u8SsidHide |
SSID Status "Hidden(1)/Visible(0)"
tuniM2MWifiAuth tstrM2MAPConfig::uniAuth |
Union holding all possible authentication parameters corresponding the current security types.
Referenced by m2m_wifi_enable_ap().