Microchip® Advanced Software Framework

tstrM2MScan Struct Reference

Wi-Fi Scan Request.

See Also
tenuM2mScanCh

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [PAD_SZ(1+M2M_MAX_SSID_LEN)]
 
uint8 au8SSID [M2M_MAX_SSID_LEN]
 
uint8 u8ChNum
 

uint8 tstrM2MScan::__PAD__[PAD_SZ(1+M2M_MAX_SSID_LEN)]

Padding bytes for forcing 4-byte alignment

uint8 tstrM2MScan::au8SSID[M2M_MAX_SSID_LEN]

SSID of the favorite Ap. If this AP is found after scan is completed, WILC will connect to it.

Referenced by m2m_wifi_request_scan_ssid().

uint8 tstrM2MScan::u8ChNum

The Wi-Fi RF Channel number tenuM2mScanCh for possible channel values

Referenced by m2m_wifi_request_scan(), and m2m_wifi_request_scan_ssid().