Microchip® Advanced Software Framework

tstrM2mWifiscanResult Struct Reference

Wi-Fi Scan Result.

Information corresponding to an AP in the Scan Result list identified by its order (index) in the list.

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)]
 
uint8 au8BSSID [6]
 
uint8 au8DeviceName [M2M_DEVICE_NAME_MAX]
 
uint8 au8SSID [M2M_MAX_SSID_LEN]
 
sint8 s8rssi
 
uint8 u8AuthType
 
uint8 u8ch
 
uint8 u8index
 

uint8 tstrM2mWifiscanResult::__PAD__[PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)]

< P2P Device NamePadding bytes for forcing 4-byte alignment

uint8 tstrM2mWifiscanResult::au8BSSID[6]

BSSID of the AP.

uint8 tstrM2mWifiscanResult::au8DeviceName[M2M_DEVICE_NAME_MAX]
uint8 tstrM2mWifiscanResult::au8SSID[M2M_MAX_SSID_LEN]

AP ssid.

sint8 tstrM2mWifiscanResult::s8rssi

AP signal strength.

uint8 tstrM2mWifiscanResult::u8AuthType

AP authentication type.

uint8 tstrM2mWifiscanResult::u8ch

AP RF channel.

uint8 tstrM2mWifiscanResult::u8index

AP index in the scan result list.