Data Structures | |
struct | ip_addr |
struct | ip_addr2 |
struct | ip_addr_packed |
Macros | |
#define | IP4_ADDR(ipaddr, a, b, c, d) |
Set an IP address given by the four byte-parts. More... | |
#define | ip4_addr1(ipaddr) (((u8_t*)(ipaddr))[0]) |
#define | ip4_addr1_16(ipaddr) ((u16_t)ip4_addr1(ipaddr)) |
#define | ip4_addr2(ipaddr) (((u8_t*)(ipaddr))[1]) |
#define | ip4_addr2_16(ipaddr) ((u16_t)ip4_addr2(ipaddr)) |
#define | ip4_addr3(ipaddr) (((u8_t*)(ipaddr))[2]) |
#define | ip4_addr3_16(ipaddr) ((u16_t)ip4_addr3(ipaddr)) |
#define | ip4_addr4(ipaddr) (((u8_t*)(ipaddr))[3]) |
#define | ip4_addr4_16(ipaddr) ((u16_t)ip4_addr4(ipaddr)) |
#define | ip4_addr_get_u32(src_ipaddr) ((src_ipaddr)->addr) |
IPv4 only: get the IP address as an u32_t. More... | |
#define | ip4_addr_set_u32(dest_ipaddr, src_u32) ((dest_ipaddr)->addr = (src_u32)) |
IPv4 only: set the IP address given as an u32_t. More... | |
#define | IP4ADDR_STRLEN_MAX 16 |
#define | IP_ADDR_ANY ((ip_addr_t *)&ip_addr_any) |
IP_ADDR_ can be used as a fixed IP address for the wildcard and the broadcast address. More... | |
#define | IP_ADDR_BROADCAST ((ip_addr_t *)&ip_addr_broadcast) |
#define | ip_addr_cmp(addr1, addr2) ((addr1)->addr == (addr2)->addr) |
#define | ip_addr_copy(dest, src) ((dest).addr = (src).addr) |
Copy IP address - faster than ip_addr_set: no NULL check. More... | |
#define | ip_addr_debug_print(debug, ipaddr) |
#define | ip_addr_get_network(target, host, netmask) ((target)->addr = ((host)->addr) & ((netmask)->addr)) |
Get the network address by combining host address with netmask. More... | |
#define | ip_addr_isany(addr1) ((addr1) == NULL || (addr1)->addr == IPADDR_ANY) |
#define | ip_addr_isbroadcast(ipaddr, netif) ip4_addr_isbroadcast((ipaddr)->addr, (netif)) |
#define | ip_addr_islinklocal(addr1) (((addr1)->addr & PP_HTONL(0xffff0000UL)) == PP_HTONL(0xa9fe0000UL)) |
#define | ip_addr_ismulticast(addr1) (((addr1)->addr & PP_HTONL(0xf0000000UL)) == PP_HTONL(0xe0000000UL)) |
#define | ip_addr_netcmp(addr1, addr2, mask) |
Determine if two address are on the same network. More... | |
#define | ip_addr_netmask_valid(netmask) ip4_addr_netmask_valid((netmask)->addr) |
#define | ip_addr_set(dest, src) |
Safely copy one IP address to another (src may be NULL) More... | |
#define | ip_addr_set_any(ipaddr) ((ipaddr)->addr = IPADDR_ANY) |
Set address to IPADDR_ANY (no need for htonl()) More... | |
#define | ip_addr_set_hton(dest, src) |
Safely copy one IP address to another and change byte order from host- to network-order. More... | |
#define | ip_addr_set_loopback(ipaddr) ((ipaddr)->addr = PP_HTONL(IPADDR_LOOPBACK)) |
Set address to loopback address. More... | |
#define | ip_addr_set_zero(ipaddr) ((ipaddr)->addr = 0) |
Set complete address to zero. More... | |
#define | IP_BADCLASS(a) (((u32_t)(a) & 0xf0000000UL) == 0xf0000000UL) |
#define | IP_CLASSA(a) ((((u32_t)(a)) & 0x80000000UL) == 0) |
#define | IP_CLASSA_HOST (0xffffffff & ~IP_CLASSA_NET) |
#define | IP_CLASSA_MAX 128 |
#define | IP_CLASSA_NET 0xff000000 |
#define | IP_CLASSA_NSHIFT 24 |
#define | IP_CLASSB(a) ((((u32_t)(a)) & 0xc0000000UL) == 0x80000000UL) |
#define | IP_CLASSB_HOST (0xffffffff & ~IP_CLASSB_NET) |
#define | IP_CLASSB_MAX 65536 |
#define | IP_CLASSB_NET 0xffff0000 |
#define | IP_CLASSB_NSHIFT 16 |
#define | IP_CLASSC(a) ((((u32_t)(a)) & 0xe0000000UL) == 0xc0000000UL) |
#define | IP_CLASSC_HOST (0xffffffff & ~IP_CLASSC_NET) |
#define | IP_CLASSC_NET 0xffffff00 |
#define | IP_CLASSC_NSHIFT 8 |
#define | IP_CLASSD(a) (((u32_t)(a) & 0xf0000000UL) == 0xe0000000UL) |
#define | IP_CLASSD_HOST 0x0fffffff /* routing needn't know. */ |
#define | IP_CLASSD_NET 0xf0000000 /* These ones aren't really */ |
#define | IP_CLASSD_NSHIFT 28 /* net and host fields, but */ |
#define | IP_EXPERIMENTAL(a) (((u32_t)(a) & 0xf0000000UL) == 0xf0000000UL) |
#define | IP_LOOPBACKNET 127 /* official! */ |
#define | IP_MULTICAST(a) IP_CLASSD(a) |
#define | ip_ntoa(ipaddr) ipaddr_ntoa(ipaddr) |
For backwards compatibility. More... | |
#define | IPADDR2_COPY(dest, src) SMEMCPY(dest, src, sizeof(ip_addr_t)) |
MEMCPY-like copying of IP addresses where addresses are known to be 16-bit-aligned if the port is correctly configured (so a port could define this to copying 2 u16_t's) - no NULL-pointer-checking needed. More... | |
#define | IPADDR_ANY ((u32_t)0x00000000UL) |
0.0.0.0 More... | |
#define | IPADDR_BROADCAST ((u32_t)0xffffffffUL) |
255.255.255.255 More... | |
#define | IPADDR_LOOPBACK ((u32_t)0x7f000001UL) |
127.0.0.1 More... | |
#define | IPADDR_NONE ((u32_t)0xffffffffUL) |
255.255.255.255 More... | |
#define | IPADDR_STRLEN_MAX IP4ADDR_STRLEN_MAX |
Typedefs | |
typedef struct ip_addr_packed | ip_addr_p_t |
typedef typedefPACK_STRUCT_END struct ip_addr | ip_addr_t |
ip_addr_t uses a struct for convenience only, so that the same defines can operate both on ip_addr_t as well as on ip_addr_p_t. More... | |
Functions | |
u8_t | ip4_addr_isbroadcast (u32_t addr, const struct netif *netif) |
Determine if an address is a broadcast address on a network interface. More... | |
u8_t | ip4_addr_netmask_valid (u32_t netmask) |
Checks if a netmask is valid (starting with ones, then only zeros) More... | |
u32_t | ipaddr_addr (const char *cp) |
Ascii internet address interpretation routine. More... | |
int | ipaddr_aton (const char *cp, ip_addr_t *addr) |
Check whether "cp" is a valid ascii representation of an Internet address and convert to a binary address. More... | |
char * | ipaddr_ntoa (const ip_addr_t *addr) |
returns ptr to static buffer; not reentrant! More... | |
char * | ipaddr_ntoa_r (const ip_addr_t *addr, char *buf, int buflen) |
Same as ipaddr_ntoa, but reentrant since a user-supplied buffer is used. More... | |
Variables | |
const ip_addr_t | ip_addr_any |
const ip_addr_t | ip_addr_broadcast |
PACK_STRUCT_BEGIN struct ip_addr_packed | PACK_STRUCT_STRUCT |
#define IP4_ADDR | ( | ipaddr, | |
a, | |||
b, | |||
c, | |||
d | |||
) |
Set an IP address given by the four byte-parts.
Little-endian version that prevents the use of htonl.
Referenced by _tiny_ip4_addr(), autoip_bind(), ip_input(), netif_init(), and wifi_cb().
#define ip4_addr1 | ( | ipaddr | ) | (((u8_t*)(ipaddr))[0]) |
Referenced by dhcp_bind().
#define ip4_addr2 | ( | ipaddr | ) | (((u8_t*)(ipaddr))[1]) |
Referenced by etharp_output().
#define ip4_addr3 | ( | ipaddr | ) | (((u8_t*)(ipaddr))[2]) |
Referenced by etharp_output().
#define ip4_addr4 | ( | ipaddr | ) | (((u8_t*)(ipaddr))[3]) |
Referenced by etharp_output().
#define ip4_addr_get_u32 | ( | src_ipaddr | ) | ((src_ipaddr)->addr) |
IPv4 only: get the IP address as an u32_t.
Referenced by dhcp_arp_reply(), dhcp_bind(), dhcp_decline(), dhcp_handle_offer(), dhcp_reboot(), dhcp_select(), dns_lookup(), inet_chksum_pseudo(), inet_chksum_pseudo_partial(), ip4_addr_isbroadcast(), ip_input(), ipaddr_addr(), ipaddr_ntoa_r(), and udp_connect().
#define ip4_addr_set_u32 | ( | dest_ipaddr, | |
src_u32 | |||
) | ((dest_ipaddr)->addr = (src_u32)) |
IPv4 only: set the IP address given as an u32_t.
Referenced by autoip_create_addr(), dhcp_bind(), dhcp_handle_ack(), dhcp_handle_offer(), dns_gethostbyname(), ip4_addr_isbroadcast(), and ipaddr_aton().
#define IP4ADDR_STRLEN_MAX 16 |
#define IP_ADDR_ANY ((ip_addr_t *)&ip_addr_any) |
IP_ADDR_ can be used as a fixed IP address for the wildcard and the broadcast address.
Referenced by autoip_arp_probe(), dhcp_decline(), dhcp_discover(), dhcp_handle_nak(), dhcp_inform(), dhcp_release(), dhcp_select(), dhcp_start(), dns_alloc_random_port(), dns_getserver(), dns_init(), dns_setserver(), lwip_dhcpserver_start_threadsafe(), netconn_bind(), netconn_connect(), and netconn_join_leave_group().
#define IP_ADDR_BROADCAST ((ip_addr_t *)&ip_addr_broadcast) |
Referenced by dhcp_decline(), dhcp_discover(), dhcp_inform(), dhcp_rebind(), dhcp_reboot(), and dhcp_select().
#define ip_addr_cmp | ( | addr1, | |
addr2 | |||
) | ((addr1)->addr == (addr2)->addr) |
Referenced by autoip_arp_reply(), dhcp_arp_reply(), dns_recv(), etharp_arp_input(), etharp_find_entry(), etharp_output(), ip_input(), netif_set_ipaddr(), and udp_input().
#define ip_addr_copy | ( | dest, | |
src | |||
) | ((dest).addr = (src).addr) |
Copy IP address - faster than ip_addr_set: no NULL check.
Referenced by dhcp_bind(), dhcp_create_msg(), dhcp_handle_ack(), dhcp_handle_offer(), etharp_find_entry(), icmp_input(), icmp_send_response(), and ip_input().
#define ip_addr_debug_print | ( | debug, | |
ipaddr | |||
) |
Referenced by dns_lookup(), dns_recv(), icmp_send_response(), netif_add(), ping_function(), and ping_recv().
#define ip_addr_get_network | ( | target, | |
host, | |||
netmask | |||
) | ((target)->addr = ((host)->addr) & ((netmask)->addr)) |
Get the network address by combining host address with netmask.
Referenced by dhcp_bind().
#define ip_addr_isany | ( | addr1 | ) | ((addr1) == NULL || (addr1)->addr == IPADDR_ANY) |
#define ip_addr_isbroadcast | ( | ipaddr, | |
netif | |||
) | ip4_addr_isbroadcast((ipaddr)->addr, (netif)) |
Referenced by etharp_output(), etharp_query(), etharp_update_arp_entry(), icmp_input(), ip_input(), raw_input(), raw_sendto(), tcp_input(), and udp_input().
#define ip_addr_islinklocal | ( | addr1 | ) | (((addr1)->addr & PP_HTONL(0xffff0000UL)) == PP_HTONL(0xa9fe0000UL)) |
Referenced by etharp_arp_input(), etharp_output(), etharp_raw(), and netif_set_ipaddr().
#define ip_addr_ismulticast | ( | addr1 | ) | (((addr1)->addr & PP_HTONL(0xf0000000UL)) == PP_HTONL(0xe0000000UL)) |
Referenced by etharp_output(), etharp_query(), etharp_update_arp_entry(), icmp_input(), ip_input(), and udp_input().
#define ip_addr_netcmp | ( | addr1, | |
addr2, | |||
mask | |||
) |
Determine if two address are on the same network.
Referenced by etharp_output(), ip4_addr_isbroadcast(), ip_route(), and udp_input().
#define ip_addr_netmask_valid | ( | netmask | ) | ip4_addr_netmask_valid((netmask)->addr) |
#define ip_addr_set | ( | dest, | |
src | |||
) |
Safely copy one IP address to another (src may be NULL)
Referenced by netif_set_gw(), netif_set_ipaddr(), and netif_set_netmask().
#define ip_addr_set_any | ( | ipaddr | ) | ((ipaddr)->addr = IPADDR_ANY) |
Set address to IPADDR_ANY (no need for htonl())
Referenced by dhcp_discover(), and ip_input().
#define ip_addr_set_hton | ( | dest, | |
src | |||
) |
#define ip_addr_set_loopback | ( | ipaddr | ) | ((ipaddr)->addr = PP_HTONL(IPADDR_LOOPBACK)) |
Set address to loopback address.
Referenced by dns_gethostbyname(), and lwip_getaddrinfo().
#define ip_addr_set_zero | ( | ipaddr | ) | ((ipaddr)->addr = 0) |
Set complete address to zero.
Referenced by autoip_start(), dhcp_create_msg(), dhcp_handle_ack(), dhcp_release(), etharp_free_entry(), and netif_add().
#define IP_BADCLASS | ( | a | ) | (((u32_t)(a) & 0xf0000000UL) == 0xf0000000UL) |
#define IP_CLASSA | ( | a | ) | ((((u32_t)(a)) & 0x80000000UL) == 0) |
#define IP_CLASSA_HOST (0xffffffff & ~IP_CLASSA_NET) |
#define IP_CLASSA_MAX 128 |
#define IP_CLASSA_NET 0xff000000 |
#define IP_CLASSA_NSHIFT 24 |
#define IP_CLASSB | ( | a | ) | ((((u32_t)(a)) & 0xc0000000UL) == 0x80000000UL) |
#define IP_CLASSB_HOST (0xffffffff & ~IP_CLASSB_NET) |
#define IP_CLASSB_MAX 65536 |
#define IP_CLASSB_NET 0xffff0000 |
#define IP_CLASSB_NSHIFT 16 |
#define IP_CLASSC | ( | a | ) | ((((u32_t)(a)) & 0xe0000000UL) == 0xc0000000UL) |
#define IP_CLASSC_HOST (0xffffffff & ~IP_CLASSC_NET) |
#define IP_CLASSC_NET 0xffffff00 |
#define IP_CLASSC_NSHIFT 8 |
#define IP_CLASSD | ( | a | ) | (((u32_t)(a) & 0xf0000000UL) == 0xe0000000UL) |
#define IP_CLASSD_HOST 0x0fffffff /* routing needn't know. */ |
#define IP_CLASSD_NET 0xf0000000 /* These ones aren't really */ |
#define IP_CLASSD_NSHIFT 28 /* net and host fields, but */ |
#define IP_EXPERIMENTAL | ( | a | ) | (((u32_t)(a) & 0xf0000000UL) == 0xf0000000UL) |
#define IP_LOOPBACKNET 127 /* official! */ |
#define IP_MULTICAST | ( | a | ) | IP_CLASSD(a) |
#define ip_ntoa | ( | ipaddr | ) | ipaddr_ntoa(ipaddr) |
For backwards compatibility.
Referenced by lwip_gethostbyname().
#define IPADDR2_COPY | ( | dest, | |
src | |||
) | SMEMCPY(dest, src, sizeof(ip_addr_t)) |
MEMCPY-like copying of IP addresses where addresses are known to be 16-bit-aligned if the port is correctly configured (so a port could define this to copying 2 u16_t's) - no NULL-pointer-checking needed.
Referenced by autoip_arp_reply(), etharp_arp_input(), and etharp_raw().
#define IPADDR_ANY ((u32_t)0x00000000UL) |
0.0.0.0
Referenced by dhcp_bind(), and ip4_addr_isbroadcast().
#define IPADDR_BROADCAST ((u32_t)0xffffffffUL) |
255.255.255.255
Referenced by ip4_addr_isbroadcast().
#define IPADDR_LOOPBACK ((u32_t)0x7f000001UL) |
127.0.0.1
#define IPADDR_NONE ((u32_t)0xffffffffUL) |
255.255.255.255
Referenced by dns_gethostbyname(), dns_lookup(), and ipaddr_addr().
#define IPADDR_STRLEN_MAX IP4ADDR_STRLEN_MAX |
typedef struct ip_addr_packed ip_addr_p_t |
ip_addr_t uses a struct for convenience only, so that the same defines can operate both on ip_addr_t as well as on ip_addr_p_t.
Determine if an address is a broadcast address on a network interface.
addr | address to be checked |
netif | the network interface against which the address is checked |
References netif::flags, ip4_addr_get_u32, ip4_addr_set_u32, netif::ip_addr, ip_addr_netcmp, IPADDR_ANY, IPADDR_BROADCAST, NETIF_FLAG_BROADCAST, and netif::netmask.
Checks if a netmask is valid (starting with ones, then only zeros)
netmask | the IPv4 netmask to check (in network byte order!) |
References lwip_htonl().
u32_t ipaddr_addr | ( | const char * | cp | ) |
Ascii internet address interpretation routine.
The value returned is in network order.
cp | IP address in ascii representation (e.g. "127.0.0.1") |
References ip4_addr_get_u32, ipaddr_aton(), and IPADDR_NONE.
Referenced by dns_gethostbyname().
int ipaddr_aton | ( | const char * | cp, |
ip_addr_t * | addr | ||
) |
Check whether "cp" is a valid ascii representation of an Internet address and convert to a binary address.
Returns 1 if the address is valid, 0 if not. This replaces inet_addr, the return value from which cannot distinguish between failure and a local broadcast address.
cp | IP address in ascii representation (e.g. "127.0.0.1") |
addr | pointer to which to save the ip address in network order |
References htonl, ip4_addr_set_u32, isdigit, islower, isspace, isxdigit, and LWIP_ASSERT.
Referenced by ipaddr_addr().
char* ipaddr_ntoa | ( | const ip_addr_t * | addr | ) |
returns ptr to static buffer; not reentrant!
returns ptr to static buffer; not reentrant!
returns ptr to static buffer; not reentrant!
addr | ip address in network order to convert |
References ipaddr_ntoa_r().
Referenced by iperf_tcp_send(), and iperf_tcp_server().
char* ipaddr_ntoa_r | ( | const ip_addr_t * | addr, |
char * | buf, | ||
int | buflen | ||
) |
Same as ipaddr_ntoa, but reentrant since a user-supplied buffer is used.
addr | ip address in network order to convert |
buf | target buffer where the string is stored |
buflen | length of buf |
References ip4_addr_get_u32, and NULL.
Referenced by ipaddr_ntoa().
const ip_addr_t ip_addr_any |
const ip_addr_t ip_addr_broadcast |
PACK_STRUCT_BEGIN struct ip_addr2 PACK_STRUCT_STRUCT |