Wi-Fi Monitor Mode Filter.
This structure sets the filtering criteria for Wlan packets when monitoring mode is enable. The received packets matching the filtering parameters, are passed directly to the application.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(3+6+6+6+1)] |
uint8 | au8BSSID [6] |
uint8 | au8DstMacAddress [6] |
uint8 | au8SrcMacAddress [6] |
uint8 | u8ChannelID |
uint8 | u8EnRecvHdr |
uint8 | u8FrameSubtype |
uint8 | u8FrameType |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2MWifiMonitorModeCtrl::au8BSSID[6] |
Receive packets only with the specified BSSID. Set to zero to disable this filter.
Referenced by atCmd_MonEn_Handler().
uint8 tstrM2MWifiMonitorModeCtrl::au8DstMacAddress[6] |
Receive packets only with the specified destination mac address. Set to zero to disable this filter.
Referenced by atCmd_MonEn_Handler().
uint8 tstrM2MWifiMonitorModeCtrl::au8SrcMacAddress[6] |
Receive packets only with the specified source mac address. Set to zero to disable this filter.
Referenced by atCmd_MonEn_Handler().
uint8 tstrM2MWifiMonitorModeCtrl::u8ChannelID |
Referenced by atCmd_MonEn_Handler(), and m2m_wifi_enable_monitoring_mode().
uint8 tstrM2MWifiMonitorModeCtrl::u8EnRecvHdr |
Enable reception of the full mac header before the payload
Referenced by atCmd_MonEn_Handler().
uint8 tstrM2MWifiMonitorModeCtrl::u8FrameSubtype |
Receive packets with the specified frame subtype as per tenuSubType. Set to M2M_WIFI_FRAME_SUB_TYPE_ANY to disable this filter
Referenced by atCmd_MonEn_Handler().
uint8 tstrM2MWifiMonitorModeCtrl::u8FrameType |
Receive packets with the specified frame type as per tenuWifiFrameType. Set to M2M_WIFI_FRAME_TYPE_ANY to disable this filter
Referenced by atCmd_MonEn_Handler().