Sets the MAC address from application. It is only intended for testing purpose. This method is not used for production SW. Production SW reads MAC Address from EFUSE.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(6+6)] |
uint8 | au8Mac0 [6] |
uint8 | au8Mac1 [6] |
uint8 tstrM2mSetMacAddress::au8Mac0[6] |
MAC address array
Referenced by m2m_wifi_set_mac_address().
uint8 tstrM2mSetMacAddress::au8Mac1[6] |
MAC address 2 array
Referenced by m2m_wifi_set_mac_address().