Wi-Fi Connection State.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(4+6)] |
uint8 | u8Ch |
uint8 | u8CurrState |
uint8 | u8ErrCode |
uint8 | u8IfcId |
uint8 | u8MAcAddr [6] |
< Mac Address of the STA/AP involved in state changePadding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiStateChanged::u8Ch |
< Interface on which state was changed
uint8 tstrM2mWifiStateChanged::u8ErrCode |
Error type as in tenuM2mConnChangedErrcode