Wi-Fi Scan Result.
Information corresponding to an AP in the Scan Result list identified by its order (index) in the list.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)] |
uint8 | au8BSSID [6] |
uint8 | au8DeviceName [M2M_DEVICE_NAME_MAX] |
uint8 | au8SSID [M2M_MAX_SSID_LEN] |
sint8 | s8rssi |
uint8 | u8AuthType |
uint8 | u8ch |
uint8 | u8index |
uint8 tstrM2mWifiscanResult::__PAD__[PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)] |
< P2P Device NamePadding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiscanResult::au8DeviceName[M2M_DEVICE_NAME_MAX] |
uint8 tstrM2mWifiscanResult::au8SSID[M2M_MAX_SSID_LEN] |
AP ssid.
Referenced by wifi_cb().