queue.
h
portBASE_TYPE xQueueReceiveFromISR( xQueueHandle pxQueue, void *pvBuffer, portBASE_TYPE *pxTaskWoken );
Receive an item from a queue. It is safe to use this function from within an interrupt service routine.
pxQueue | The handle to the queue from which the item is to be received. |
pvBuffer | Pointer to the buffer into which the received item will be copied. |
pxTaskWoken | A task may be blocked waiting for space to become available on the queue. If xQueueReceiveFromISR causes such a task to unblock *pxTaskWoken will get set to pdTRUE, otherwise *pxTaskWoken will remain unchanged. |
Example usage:
xQueueHandle xQueue;
Function to create a queue and post some values. void vAFunction( void *pvParameters ) { char cValueToPost; const portTickType xBlockTime = ( portTickType )0xff;
Create a queue capable of containing 10 characters. xQueue = xQueueCreate( 10, sizeof( char ) ); if( xQueue == 0 ) { Failed to create the queue. }
...
Post some characters that will be used within an ISR. If the queue is full then this task will block for xBlockTime ticks. cValueToPost = 'a'; xQueueSend( xQueue, ( void * ) &cValueToPost, xBlockTime ); cValueToPost = 'b'; xQueueSend( xQueue, ( void * ) &cValueToPost, xBlockTime );
... keep posting characters ... this task may block when the queue becomes full.cValueToPost = 'c'; xQueueSend( xQueue, ( void * ) &cValueToPost, xBlockTime );}
ISR that outputs all the characters received on the queue. void vISR_Routine( void ) { portBASE_TYPE xTaskWokenByReceive = pdFALSE; char cRxedChar;
while( xQueueReceiveFromISR( xQueue, ( void * ) &cRxedChar, &xTaskWokenByReceive) ) { A character was received. Output the character now. vOutputCharacter( cRxedChar );
If removing the character from the queue woke the task that was posting onto the queue cTaskWokenByReceive will have been set to pdTRUE. No matter how many times this loop iterates only one task will be woken. }
if( cTaskWokenByPost != ( char ) pdFALSE; { taskYIELD (); } }