A_BLOCK_LINK | |
 api_msg | This struct contains a function to execute in another thread context and a struct api_msg_msg that serves as an argument for this function |
 api_msg_msg | This struct includes everything that is necessary to execute a function for a netconn in another thread context (mainly used to process netconns in the tcpip_thread context to be thread safe) |
 autoip | |
 client_hdr | |
 connect_ap_params | |
 connect_params | |
 corCoRoutineControlBlock | |
 dhcp | |
 dhcp_msg | Minimum set of fields of any DHCP message |
 dns_answer | DNS answer message structure |
 dns_api_msg | As lwip_netconn_do_gethostbyname requires more arguments but doesn't require a netconn, it has its own struct (to avoid struct api_msg getting bigger than necessary) |
 dns_hdr | DNS message header |
 dns_query | DNS query message structure |
 dns_req_entry | DNS request table entry: used when dns_gehostbyname cannot answer the request from the DNS table |
 dns_table_entry | DNS table entry |
 eth_addr | The ethernet address |
 eth_hdr | Ethernet header |
 etharp_entry | |
 etharp_hdr | ARP message, see RFC 826 ("Packet format") |
 genclk_config | Hardware representation of a set of generic clock parameters |
 hif_msg_t | |
 icmp6_echo_hdr | This is the ICMP6 header adapted for echo req/resp |
 icmp6_hdr | This is the standard ICMP6 header |
 icmp_echo_hdr | This is the standard ICMP header only that the u32_t data is split to two u16_t like ICMP echo needs it |
 in_addr | For compatibility with BSD code |
 init_params | |
 ip6_addr | |
 ip6_addr_packed | |
 ip6_frag_hdr | |
 ip6_hbh_hdr | |
 ip6_hdr | |
 ip6_reass_helper | This is a helper struct which holds the starting offset and the ending offset of this fragment to easily chain the fragments |
 ip6_reassdata | |
 ip_addr | |
 ip_addr2 | |
 ip_addr_packed | |
 ip_globals | |
 ip_hdr | |
 ip_pcb | |
 ip_reass_helper | This is a helper struct which holds the starting offset and the ending offset of this fragment to easily chain the fragments |
 ip_reassdata | |
 iperf_state | |
 iperf_stats | |
 ipX_addr_t | |
 label_t | |
 lladdr_option | |
 memp | |
 mld_group | |
 mld_header | Multicast listener report/query/done message header |
 mtu_option | |
 na_header | Neighbor advertisement message header |
 nd6_destination_cache_entry | |
 nd6_neighbor_cache_entry | |
 nd6_prefix_list_entry | |
 nd6_q_entry | Struct for queueing outgoing packets for unknown address defined here to be accessed by memp.h |
 nd6_router_list_entry | |
 netconn | A netconn descriptor |
 netif | Generic data structure used for all lwIP network interfaces |
 ns_header | Neighbor solicitation message header |
 params_dispatch | |
 pbuf | |
 pbuf_custom | A custom pbuf: like a pbuf, but following a function pointer to free it |
 pbuf_custom_ref | |
 pdc_packet | PDC data packet for transfer |
 pll_config | Hardware-specific representation of PLL configuration |
 prefix_option | |
 ptru8_params | |
 QUEUE_REGISTRY_ITEM | |
 QueueDefinition | |
 ra_header | |
 raw_pcb | |
 redirect_header | Redirect message header |
 redirected_header_option | |
 route_option | |
 rs_header | Router solicitation message header |
 s_interrupt_source | Describes a PIO interrupt source, including the PIO instance triggering the interrupt and the associated interrupt handler |
 sam_uart_opt | Option list for UART peripheral initialization |
 sam_usart_opt_t | |
 sd_mmc_card | SD/MMC card information structure |
 server_hdr | |
 set_max_tx_rate_params | |
 stats_ | |
 stats_igmp | |
 stats_mem | |
 stats_proto | |
 stats_sys | |
 stats_syselem | |
 StructCPtr | Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 StructCVPtr | Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 StructPtr | Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 StructVPtr | Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 sys_timeo | |
 tcp_hdr | |
 tcp_listen_pcbs_t | |
 tcp_pcb | |
 tcp_pcb_listen | |
 tcp_seg | |
 tcpip_msg | |
 tmrTimerControl | |
 tmrTimerQueueMessage | |
 tskTaskControlBlock | |
 tstr1xAuthCredentials | Credentials for the user to authenticate with the AAA server (WPA-Enterprise Mode IEEE802.1x) |
 tstrBuffer | |
 tstrEthInitParam | Structure to hold ethernet interface parameters |
 tstrHashContext | |
 tstrHifHdr | Structure to hold HIF header |
 tstrHifinitParam | Structure to hold HIF Init Param |
 tstrI2cMasterInitParam | I2C master configuration parameters |
 tstrM2mAntDiversityParams | Antena selection/switch mode |
 tstrM2mAntDivParams | |
 tstrM2MAPAssocInfo | M2M association information of the connected station in the AP mode |
 tstrM2MAPConfig | AP Configuration |
 tstrM2MAssocEntryInfo | M2M association information of of an assoicated entry in the AP mode |
 tstrM2MConnInfo | M2M Provisioning Information obtained from the HTTP Provisioning server |
 tstrM2MDataBufCtrl | Structure holding the incoming buffer's data size information, indicating the data size of the buffer and the remaining buffer's data size . The data of the buffer which holds the packet sent to the host is placed in the tstrEthInitParam structure in the au8ethRcvBuf attribute. This following information is retreived in the host when an event M2M_WIFI_RESP_ETHERNET_RX_PACKET is received in the wi-fi callback function tpfAppWifiCb |
 tstrM2MDeviceNameConfig | Device name |
 tstrM2MIfId | Set Intrface ID |
 tstrM2MIPConfig | Static IP configuration |
 tstrM2MIPConfig2 | |
 tstrM2mIpRsvdPkt | Received Packet Size and Data Offset |
 tstrM2mLsnInt | Listen interval |
 tstrM2MMulticastMac | M2M add/remove multicast mac address |
 tstrM2MP2PConnect | Set the device to operate in the Wi-Fi Direct (P2P) mode |
 tstrM2MP2pDevInfo | P2P Pin |
 tstrM2MPinInfo | PIN Number (input) |
 tstrM2mPsType | Power Save Configuration |
 tstrM2mReqHTEnable | HT (High Throughput) enable (default) or disable |
 tstrM2mReqScanResult | Scan Result Request |
 tstrM2mRev | |
 tstrM2MScan | Wi-Fi Scan Request |
 tstrM2mScanDone | Wi-Fi Scan Result |
 tstrM2MScanList | Wi-Fi channel list regulation |
 tstrM2MScanOption | |
 tstrM2MScanRegion | Wi-Fi channel regulation region information |
 tstrM2mSetMacAddress | Sets the MAC address from application. It is only intended for testing purpose. This method is not used for production SW. Production SW reads MAC Address from EFUSE |
 tstrM2mTxPwrLevel | Tx power level |
 tstrM2MUserMaxTxRate | User specified Max Tx Rate |
 tstrM2mWifiConnect | Wi-Fi Connect Request |
 tstrM2mWifiGetRevision | Structure holding firmware version parameters |
 tstrM2MWifiMonitorModeCtrl | Wi-Fi Monitor Mode Filter |
 tstrM2MWifiRxPacketInfo | Wi-Fi RX Frame Header |
 tstrM2mWifiscanResult | Wi-Fi Scan Result |
 tstrM2MWifiSecInfo | Authentication credentials to connect to a Wi-Fi network |
 tstrM2mWifiStateChanged | Wi-Fi Connection State |
 tstrM2MWifiTxPacketInfo | Wi-Fi Tx Packet Info |
 tstrM2mWifiWepParams | WEP security key parameters |
 tstrM2MWPSConnect | WPS Configuration parameters |
 tstrM2MWPSInfo | WPS Result |
 tstrNmBusCapabilities | Structure holding bus capabilities information |
 tstrNmI2cDefault | Structure holding I2C default operation parameters |
 tstrNmI2cSpecial | Structure holding I2C special operation parameters |
 tstrNmSdioCmd52 | |
 tstrNmSdioCmd53 | |
 tstrNmSpiRw | Structure holding SPI R/W parameters |
 tstrPerphInitParam | Peripheral module initialization parameters |
 tstrRSAPublicKey | |
 tstrSystemTime | Used for time storage |
 tstrWifiInitParam | Structure, holding the Wi-Fi configuration attributes such as the Wi-Fi callback, monitoring mode callback and Ethernet parameter initialization structure. |
 tuCtrlStruct | |
 tuniM2MWifiAuth | Wi-Fi Security Parameters for all supported security modes |
 uart_config_optical | |
 uart_rs232_options | Input parameters when initializing RS232 and similar modes |
 UDP_datagram | |
 udp_hdr | |
 udp_pcb | |
 uint8_uint8_params | |
 uint_params | |
 Union16 | 16-bit union |
 Union32 | 32-bit union |
 Union64 | 64-bit union |
 UnionCPtr | Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 UnionCVPtr | Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 UnionPtr | Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 UnionVPtr | Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 usart_iso7816_opt_t | |
 usart_spi_opt_t | |
 void_params | |
 wifi_enable_mac_mcast_params | |
 wifi_enable_monitoring_mode_params | |
 wifi_get_mac_address_params | |
 wifi_get_otp_mac_address_params | |
 wifi_p2p_params | |
 wifi_request_scan_ssid_params | |
 wifi_send_ethernet_pkt_params | |
 wifi_send_wlan_pkt_params | |
 wifi_set_cust_InfoElement_params | |
 wifi_set_device_name_params | |
 wifi_set_lsn_int_params | |
 wifi_set_mac_address_params | |
 wifi_set_pin_params | |
 wifi_set_receive_buffer_params | |
 wifi_set_scan_list_params | |
 wifi_set_scan_options_params | |
 wifi_set_sleep_mode_params | |
 wifi_wps_params | |
 xCOMMAND_INPUT_LIST | |
 xCOMMAND_LINE_INPUT | |
 xLIST | |
 xLIST_ITEM | |
 xMEMORY_REGION | |
 xMINI_LIST_ITEM | |
 xRTOS_HEAP | |
 xTASK_PARAMTERS | |
 xTIME_OUT | |