Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseCopyright (c) 2016-2018 Microchip Technology Inc
oQuick Start Guide for the SAM PIO driverThis is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oAdvanced use case - Interrupt driven edge detection
oExtra Information for Extensible Direct Memory Access Controller Driver
oExamples for Direct Memory Access Controller DriverThis is a list of the available Quick Start Guides (QSGs) and example applications for SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver
|\Quick Start Guide for the XDMAC driverThis is the quick start guide for the SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the XDMAC module
oDocument Revision History
oQuickstart guide for SAM SPI driverThis is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick Start Guide for the System Clock ManagementService (SAMV71)
oAdvanced use case - Peripheral Bus ClockManagement (SAMV71)
oQuick start guide for the common IOPORT serviceThis is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Advanced use case doing port accessIn this case we will read out the pins from one whole port and write the read value to another port
oQuick start guide for Serial Interface serviceThis is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases
|\Advanced use case - Send a packet of serial dataIn this use case, the USART module is configured for:
oQuick start guide for the SAM USART moduleThis is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|oUSART receive character and echo backIn this use case, the USART module is configured for:
|\USART receive character and echo back via interruptsIn this use case, the USART module is configured for:
o"SAMV71-XLTRA - Operating frequencies"This page lists several definition related to the board operating frequency
o"SAMV71-XLTRA - Board informations"This page lists several definition related to the board description
o"SAMV71-XPRO - CAN"This page lists definitions related to CAN0 and CAN1
oTodo List
oDeprecated List
\Bug List