Microchip® Advanced Software Framework

conf_tinyservices.h File Reference

Tiny DHCP/DNS service configuration.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

Macros

#define ADAY_DNS_TTL   (86400)
 
#define AP_ADDR   192, 168, 5, 1
 
#define AP_ADDR_IP   _tiny_ip4_addr(AP_ADDR)
 
#define DOMAIN_NAME   "iot.com"
 Default Domain Name supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define DOMAIN_NAME_LEN   (8)
 
#define GW_ADDR   192, 168, 5, 1
 Default gateway in provisioning mode. More...
 
#define GW_ADDR_IP   _tiny_ip4_addr(GW_ADDR)
 
#define HTTP_SRV_LOCAL_NAME   "smartconnect"
 
#define NAME_SERVER_FQDN   NAME_SERVER_HOST_NAME "." DOMAIN_NAME
 
#define NAME_SERVER_FQDN_LEN   (11)
 
#define NAME_SERVER_HOST_NAME   "ns"
 Default Name Server supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define SANE_DNS_TTL   (600)
 Default DNS Time To Live supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define SANE_LEASE_TIME   (ADAY_DNS_TTL)
 Default Lease Time supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define SANE_REBINDING_TIME   (ADAY_DNS_TTL)
 Default Rebinding Time supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define SANE_RENEWAL_TIME   (ADAY_DNS_TTL)
 Default Renewal Time supplied to the client by Tiny DHCP Server in provisioning mode. More...
 
#define SN_MASK   255, 255, 255, 0
 Default subnet mask in provisioning mode. More...
 
#define SN_MASK_IP   _tiny_ip4_addr(SN_MASK)
 
#define TWOHOUR_DNS_TTL   (7200)
 

#define ADAY_DNS_TTL   (86400)
#define AP_ADDR   192, 168, 5, 1
#define AP_ADDR_IP   _tiny_ip4_addr(AP_ADDR)
#define DOMAIN_NAME   "iot.com"

Default Domain Name supplied to the client by Tiny DHCP Server in provisioning mode.

Referenced by lwip_dhcp_server_fn().

#define DOMAIN_NAME_LEN   (8)

Referenced by lwip_dhcp_server_fn().

#define GW_ADDR   192, 168, 5, 1

Default gateway in provisioning mode.

#define GW_ADDR_IP   _tiny_ip4_addr(GW_ADDR)

Referenced by net_add_wilc_netif().

#define HTTP_SRV_LOCAL_NAME   "smartconnect"
#define NAME_SERVER_FQDN   NAME_SERVER_HOST_NAME "." DOMAIN_NAME
#define NAME_SERVER_FQDN_LEN   (11)
#define NAME_SERVER_HOST_NAME   "ns"

Default Name Server supplied to the client by Tiny DHCP Server in provisioning mode.

#define SANE_DNS_TTL   (600)

Default DNS Time To Live supplied to the client by Tiny DHCP Server in provisioning mode.

#define SANE_LEASE_TIME   (ADAY_DNS_TTL)

Default Lease Time supplied to the client by Tiny DHCP Server in provisioning mode.

Referenced by lwip_dhcp_server_fn().

#define SANE_REBINDING_TIME   (ADAY_DNS_TTL)

Default Rebinding Time supplied to the client by Tiny DHCP Server in provisioning mode.

Referenced by lwip_dhcp_server_fn().

#define SANE_RENEWAL_TIME   (ADAY_DNS_TTL)

Default Renewal Time supplied to the client by Tiny DHCP Server in provisioning mode.

Referenced by lwip_dhcp_server_fn().

#define SN_MASK   255, 255, 255, 0

Default subnet mask in provisioning mode.

#define SN_MASK_IP   _tiny_ip4_addr(SN_MASK)
#define TWOHOUR_DNS_TTL   (7200)