Ethernet output for IPv6.
Uses ND tables for link-layer addressing.
#include "lwip/opt.h"
#include "lwip/ethip6.h"
#include "lwip/nd6.h"
#include "lwip/pbuf.h"
#include "lwip/ip6.h"
#include "lwip/ip6_addr.h"
#include "lwip/inet_chksum.h"
#include "lwip/netif.h"
#include "lwip/icmp6.h"
#include <string.h>
Data Structures | |
struct | eth_addr |
The ethernet address. More... | |
struct | eth_hdr |
Ethernet header. More... | |
Macros | |
#define | ETHTYPE_IPV6 0x86DD |
#define | SIZEOF_ETH_HDR (14 + ETH_PAD_SIZE) |
Functions | |
err_t | ethip6_output (struct netif *netif, struct pbuf *q, ip6_addr_t *ip6addr) |
Resolve and fill-in Ethernet address header for outgoing IPv6 packet. More... | |
static err_t | ethip6_send (struct netif *netif, struct pbuf *p, struct eth_addr *src, struct eth_addr *dst) |
Send an IPv6 packet on the network using netif->linkoutput The ethernet header is filled in before sending. More... | |
Variables | |
PACK_STRUCT_BEGIN struct eth_addr | PACK_STRUCT_STRUCT |
#define ETHTYPE_IPV6 0x86DD |
Referenced by ethernet_input(), and ethip6_send().
#define SIZEOF_ETH_HDR (14 + ETH_PAD_SIZE) |
Referenced by etharp_arp_input(), etharp_raw(), etharp_send_ip(), ethernet_input(), and ethip6_output().
err_t ethip6_output | ( | struct netif * | netif, |
struct pbuf * | q, | ||
ip6_addr_t * | ip6addr | ||
) |
Resolve and fill-in Ethernet address header for outgoing IPv6 packet.
For IPv6 multicast, corresponding Ethernet addresses are selected and the packet is transmitted on the link.
For unicast addresses, ...
anycast addresses
netif | The lwIP network interface which the IP packet will be sent on. |
q | The pbuf(s) containing the IP packet to be sent. |
ip6addr | The IP address of the packet destination. |
References nd6_neighbor_cache_entry::counter, nd6_neighbor_cache_entry::delay_time, ERR_BUF, ERR_MEM, ETHARP_DEBUG, ethip6_send(), netif::hwaddr, ip6_addr_ismulticast, nd6_neighbor_cache_entry::lladdr, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_TRACE, LWIP_DEBUGF, ND6_DELAY, nd6_get_next_hop_entry(), ND6_PROBE, nd6_queue_packet(), ND6_REACHABLE, ND6_STALE, neighbor_cache, pbuf_header(), SIZEOF_ETH_HDR, and nd6_neighbor_cache_entry::state.
Referenced by wilc_netif_init().
|
static |
Send an IPv6 packet on the network using netif->linkoutput The ethernet header is filled in before sending.
netif the lwIP network interface on which to send the packet p the packet to send, p->payload pointing to the (uninitialized) ethernet header src the source MAC address to be copied into the ethernet header dst the destination MAC address to be copied into the ethernet header
References ETHARP_DEBUG, ETHTYPE_IPV6, netif::hwaddr_len, netif::linkoutput, LWIP_ASSERT, LWIP_DBG_TRACE, LWIP_DEBUGF, pbuf::payload, and PP_HTONS.
Referenced by ethip6_output().
PACK_STRUCT_END PACK_STRUCT_BEGIN struct eth_hdr PACK_STRUCT_STRUCT |