Modules | |
m2m_wifi_init | |
Synchronous initialization functions for the WILC driver. | |
m2m_wifi_deinit | |
Synchronous deinitialization function to the WILC1000 driver. | |
m2m_wifi_handle_events | |
Synchronous M2M event handler function, responsible for handling interrupts received from the WILC firmware. | |
m2m_wifi_connect | |
Asynchronous wi-fi connection function to a specific AP. | |
m2m_wifi_disconnect | |
Synchronous wi-fi disconnection function, requesting a Wi-Fi disconnect from the currently connected AP. | |
m2m_wifi_get_connection_info | |
Asynchronous connection status retrieval function, retrieves the status information of the currently connected AP. | |
m2m_wifi_set_mac_address | |
Synchronous dual MAC address assigning to the WILC1500 . | |
m2m_wifi_wps | |
Asynchronous WPS triggering function. | |
m2m_wifi_wps_disable | |
Disable the NMC1500 WPS operation. | |
m2m_wifi_p2p | |
Asynchronous Wi-Fi direct (P2P) enabling mode function. | |
m2m_wifi_p2p_disconnect | |
Disable the NMC1500 device Wi-Fi direct mode (P2P). | |
m2m_wifi_enable_ap | |
Asychronous wi-fi hotspot enabling function. | |
m2m_wifi_disable_ap | |
Synchronous wi-fi hotspot disabling function. | |
m2m_wifi_set_scan_options | |
Synchronous wi-fi scan settings function. | |
m2m_wifi_set_scan_region | |
Synchronous wi-fi scan region setting function. | |
m2m_wifi_request_scan | |
Asynchronous wi-fi scan request on the given channel. | |
m2m_wifi_get_num_ap_found | |
Synchronous function to retrieve the number of AP's found in the last scan request, The function read the number of AP's from global variable which updated in the wi-fi callback fucntion through the M2M_WIFI_RESP_SCAN_DONE event. | |
m2m_wifi_req_scan_result | |
Synchronous call to read the AP information from the SCAN Result list with the given index. | |
m2m_wifi_req_curr_rssi | |
Asynchronous request for the current RSSI of the connected AP. | |
m2m_wifi_get_otp_mac_address | |
Request the MAC address stored on the OTP (one time programmable) memory of the device. | |
m2m_wifi_get_mac_address | |
Function to retrieve the current MAC address. | |
m2m_wifi_set_sleep_mode | |
Synchronous power-save mode setting function for the NMC1500. | |
m2m_wifi_get_sleep_mode | |
Synchronous power save mode retrieval function. | |
m2m_wifi_set_lsn_int | |
Synchronous function for setting the wi-fi listen interval for power save operation. | |
m2m_wifi_enable_monitoring_mode | |
Asynchronous wi-fi monitoring enable mode (Promiscuous mode) function. | |
m2m_wifi_disable_monitoring_mode | |
Synchronous function to disable Wi-Fi monitoring mode (Promiscuous mode). | |
m2m_wifi_send_wlan_pkt | |
Synchronous function to transmit a WIFI RAW packet while the implementation of this packet is left to the application developer. | |
m2m_wifi_send_ethernet_pkt | |
Synchronous function to transmit an Ethernet packet. | |
m2m_wifi_set_cust_InfoElement | |
Synchronous function to Add/Remove user-defined Information Element to the WIFIBeacon and Probe Response frames while chip mode is Access Point Mode. | |