Synchronous power-save mode setting function for the NMC1500.
Functions | |
NMI_API sint8 | m2m_wifi_set_sleep_mode (uint8 PsTyp, uint8 BcastEn) |
Set the power saving mode for the WILC1000. More... | |
Set the power saving mode for the WILC1000.
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM beacon for receiving broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM beacon, but its wakeup depends only on the the configured Listen Interval. |
References hif_get_sleep_mode(), hif_send(), hif_set_sleep_mode(), M2M_INFO, M2M_NO_PS, M2M_REQ_GRP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SLEEP, NULL, tstrM2mPsType::u8BcastEn, and tstrM2mPsType::u8PsType.
Referenced by os_m2m_wifi_set_sleep_mode_imp().