#define CONF_METHOD_DISPLAY 0x0008 |
#define CONF_METHOD_KEYPAD 0x0100 |
#define CONF_METHOD_LABEL 0x0004 |
Referenced by sta_task(), and wifi_cb().
#define CONF_METHOD_PBC 0x0080 |
#define CONF_METHOD_PHYSICAL_DISPLAY 0x4008 |
#define CONF_METHOD_PHYSICAL_PBC 0x0480 |
Referenced by sta_task(), and wifi_cb().
#define CONF_METHOD_VIRTUAL_DISPLAY 0x2008 |
#define CONF_METHOD_VIRTUAL_PBC 0x0280 |
#define M2M_1X_PWD_MAX 41 |
The maximum size of the password including the NULL termination. It is used for RADIUS authentication in case of connecting the device to an AP secured with WPA-Enterprise.
#define M2M_1X_USR_NAME_MAX 21 |
The maximum size of the user name including the NULL termination. It is used for RADIUS authentication in case of connecting the device to an AP secured with WPA-Enterprise.
#define M2M_AP_CMD_BASE 80 |
The base value of all the Access Point mode host commands opcodes.
#define M2M_BUFFER_MAX_SIZE (1600UL - 4) |
Maximum size for the shared packet buffer.
#define M2M_CONFIG_CMD_BASE 1 |
The base value of all the host configuration commands opcodes.
#define M2M_CUST_IE_LEN_MAX 252 |
The maximum size of IE (Information Element).
#define M2M_DEVICE_NAME_MAX 48 |
Maximum Size for the device name including the NULL termination.
Referenced by m2m_wifi_set_device_name().
#define M2M_DRIVER_VERSION_MAJOR_NO (4) |
Driver Major release version number.
Referenced by nm_drv_init(), and nm_get_firmware_info().
#define M2M_DRIVER_VERSION_MINOR_NO (7) |
Driver Minor release version number.
Referenced by nm_drv_init(), and nm_get_firmware_info().
#define M2M_DRIVER_VERSION_PATCH_NO (2) |
Driver patch release version number.
Referenced by nm_drv_init(), and nm_get_firmware_info().
#define M2M_ENTERPRISE_CERT_MAX_LENGTH_IN_BYTES 4000 |
Maximum size for the Certificate that would be download to the WILC1000 Memory.
THIS VALUE CANNOT BE CHANGED
Referenced by m2m_wifi_download_cert().
#define M2M_ETH_PAD_SIZE 2 |
Pad size before the Ethernet header to keep the Ethernet data aligned
Referenced by m2m_wifi_cb(), and m2m_wifi_send_ethernet_pkt().
#define M2M_ETHERNET_HDR_LEN 14 |
Length of the Etherenet header in bytes.
Referenced by m2m_wifi_send_ethernet_pkt().
#define M2M_ETHERNET_HDR_OFFSET 36 |
The offset of the Ethernet header within the WLAN Tx Buffer.
Should be word aligned
Referenced by m2m_wifi_send_ethernet_pkt(), and wilc_netif_tx().
#define M2M_FIRMWARE_VERSION_MAJOR_NO (4) |
Firmware Major release version number.
#define M2M_FIRMWARE_VERSION_MINOR_NO (7) |
Firmware Minor release version number.
#define M2M_FIRMWARE_VERSION_PATCH_NO (2) |
Firmware patch release version number.
#define M2M_LISTEN_INTERVAL 1 |
The STA uses the Listen Interval parameter to indicate to the AP how many beacon intervals it shall sleep before it retrieves the queued frames from the AP.
#define M2M_MAC_ADDRES_LEN 6 |
The size fo 802 MAC address.
Referenced by m2m_wifi_enable_mac_mcast().
#define M2M_MAX_PMK_LEN 40 |
Maximum size for the PMK value.
#define M2M_MAX_PSK_LEN 65 |
Maximum size for the WPA PSK including the NULL termination.
Referenced by m2m_wifi_connect().
#define M2M_MAX_SSID_LEN 33 |
Maximum size for the Wi-Fi SSID including the NULL termination.
Referenced by m2m_wifi_connect().
#define M2M_P2P_CMD_BASE 90 |
The base value of all the P2P mode host commands opcodes.
#define M2M_SCAN_ERR_AP ((sint8)-4) |
currently not used.
#define M2M_SCAN_ERR_P2P ((sint8)-5) |
currently not used.
#define M2M_SCAN_ERR_WIFI ((sint8)-2) |
currently not used.
#define M2M_SCAN_ERR_WPS ((sint8)-6) |
currently not used.
#define M2M_SCAN_MIN_NUM_SLOTS (2) |
The min. number of scan slots performed by the WILC board.
Referenced by m2m_wifi_set_scan_options().
#define M2M_SCAN_MIN_SLOT_TIME (20) |
The min. duration in miliseconds of a scan slots performed by the WILC board.
Referenced by m2m_wifi_set_scan_options().
#define M2M_STA_CMD_BASE 40 |
The base value of all the station mode host commands opcodes.
#define M2M_WIFI_FRAME_SUB_TYPE_ANY 0xFF |
Set monitor mode to receive frames with any sub type
#define M2M_WIFI_FRAME_TYPE_ANY 0xFF |
Set monitor mode to receive any of the frames types
#define MAKE_VERSION | ( | major, | |
minor, | |||
patch | |||
) | (((uint16)(major) << 8) | ((minor << 4) | (patch) )) |
Referenced by nm_get_firmware_info().
#define P2P_DEFAULT_PIN 0X00 |
#define P2P_MAX_PIN_SIZE 8 |
The maxmimum pin size for P2P PIN Config method.
#define P2P_PUSHBUTTON 0X04 |
#define P2P_REGISTER_SPECIFIED 0X05 |
#define P2P_USER_SPECIFIED 0X01 |
#define RF_VERSION ("01.1") |
Firmware RF Version.
#define WEP_104_KEY_SIZE ((uint8)13) |
Indicate the wep key size in bytes for 104 bit hex passphrase.
#define WEP_104_KEY_STRING_SIZE ((uint8)26) |
Indicate the wep key size in bytes for 104 bit string passphrase.
Referenced by m2m_wifi_connect().
#define WEP_40_KEY_SIZE ((uint8)5) |
Indicate the wep key size in bytes for 40 bit hex passphrase.
#define WEP_40_KEY_STRING_SIZE ((uint8)10) |
Indicate the wep key size in bytes for 40 bit string passphrase.
Referenced by m2m_wifi_connect().
#define WEP_KEY_MAX_INDEX ((uint8)4) |
Indicate the max key index value for WEP authentication
Referenced by m2m_wifi_connect().