Macros | |
#define | SLIP_RX_FROM_ISR 0 |
Set this to 1 to enable functions to pass in RX bytes from ISR context. More... | |
#define | SLIP_RX_QUEUE SLIP_RX_FROM_ISR |
Set this to 1 (default for SLIP_RX_FROM_ISR) to queue incoming packets received by slipif_received_byte[s]() as long as PBUF_POOL pbufs are available. More... | |
#define | SLIP_USE_RX_THREAD !NO_SYS |
Set this to 1 to start a thread that blocks reading on the serial line (using sio_read()). More... | |
Functions | |
err_t | slipif_init (struct netif *netif) |
void | slipif_poll (struct netif *netif) |
#define SLIP_RX_FROM_ISR 0 |
Set this to 1 to enable functions to pass in RX bytes from ISR context.
If enabled, slipif_received_byte[s]() process incoming bytes and put assembled packets on a queue, which is fed into lwIP from slipif_poll(). If disabled, slipif_poll() polls the serial line (using sio_tryread()).
#define SLIP_RX_QUEUE SLIP_RX_FROM_ISR |
Set this to 1 (default for SLIP_RX_FROM_ISR) to queue incoming packets received by slipif_received_byte[s]() as long as PBUF_POOL pbufs are available.
If disabled, packets will be dropped if more than one packet is received.
#define SLIP_USE_RX_THREAD !NO_SYS |
Set this to 1 to start a thread that blocks reading on the serial line (using sio_read()).