Microchip® Advanced Software Framework

tstrM2MIPConfig Struct Reference

Static IP configuration.

Note
All member IP addresses are expressed in Network Byte Order (eg. "192.168.10.1" will be expressed as 0x010AA8C0).

#include <m2m_types.h>

Data Fields

uint32 u32DNS
 
uint32 u32Gateway
 
uint32 u32StaticIP
 
uint32 u32SubnetMask
 

uint32 tstrM2MIPConfig::u32DNS

IP for the DNS server.

uint32 tstrM2MIPConfig::u32Gateway

IP of the Default internet gateway.

uint32 tstrM2MIPConfig::u32StaticIP

The static IP assigned to the device.

Referenced by m2m_wifi_cb().

uint32 tstrM2MIPConfig::u32SubnetMask

Subnet mask for the local area network.