Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Callbacks

     Provides detail on the available callbacks for the Wlan APIs.

Typedefs

typedef void(* tpfAppEthCb )(uint8 u8MsgType, void *pvMsg, void *pvCtrlBuf)
 Ethernet (Bypass mode) notification callback function receiving Bypass mode events as defined in the Wi-Fi responses enumeration tenuM2mStaCmd. More...
 
typedef void(* tpfAppWifiCb )(uint8 u8MsgType, void *pvMsg)
 Wi-Fi's main callback function handler, for handling the M2M_WIFI events received on the Wi-Fi interface. Such notifications are received in response to Wi-Fi operations such as m2m_wifi_request_scan, m2m_wifi_connect_open, m2m_wifi_connect_wep, m2m_wifi_connect_psk, m2m_wifi_connect_1x_mschap2, m2m_wifi_connect_1x_tls. More...
 

void(* tpfAppEthCb)(uint8 u8MsgType, void *pvMsg, void *pvCtrlBuf)

Ethernet (Bypass mode) notification callback function receiving Bypass mode events as defined in the Wi-Fi responses enumeration tenuM2mStaCmd.

If bypass mode is enabled, applications must ensure this callback function is registered 
with the Wi-Fi driver by calling @ref m2m_wifi_init.
Parameters
[in]u8MsgTypeType of notification. Possible types are:
[in]pvMsgA pointer to a buffer containing the notification parameters (if any). It should be cast to the correct data type corresponding to the notification type.

For example, it could be a pointer to the buffer holding the received frame in case of M2M_WIFI_RESP_ETHERNET_RX_PACKET event.

Parameters
[in]pvControlBufA pointer to control buffer describing the accompanied message. To be cast to tstrM2mIpCtrlBuf in case of M2M_WIFI_RESP_ETHERNET_RX_PACKET event.
Warning
Make sure that the application defines ETH_MODE.
See Also
m2m_wifi_init
void(* tpfAppWifiCb)(uint8 u8MsgType, void *pvMsg)

Wi-Fi's main callback function handler, for handling the M2M_WIFI events received on the Wi-Fi interface. Such notifications are received in response to Wi-Fi operations such as m2m_wifi_request_scan, m2m_wifi_connect_open, m2m_wifi_connect_wep, m2m_wifi_connect_psk, m2m_wifi_connect_1x_mschap2, m2m_wifi_connect_1x_tls.

Wi-Fi operations are implemented in an asynchronous mode, and all incoming information/status
            are to be handled through this callback function when the corresponding notification is received.

Applications are expected to assign this wi-fi callback function by 
calling @ref m2m_wifi_init.
Parameters
[in]u8MsgTypeType of notification. Possible types are:
[in]pvMsgA pointer to a buffer containing the notification parameters (if any). It should be cast to the correct data type corresponding to the notification type.
See Also
tstrM2mWifiStateChanged tstrM2MWPSInfo tstrM2mScanDone tstrM2mWifiscanResult m2m_wifi_init