Introduction
This example demonstrates the use of the Wi-Fi module with the SAMD21 Xplained Pro board to connect AWS using the RSA Security.
It uses the following hardware:
- the SAMD21 Xplained Pro.
- the WINC1500 on EXT1.
Main Files
- main.c : Initialize the Wi-Fi module and connect to server using SSL.
Usage
- Configure below code in the config main.h for AP information to be connected.
- Build the program and download it into the board.
- On the computer, open and configure a terminal application as the follows.
* Baud Rate : 115200
* Data : 8bit
* Parity bit : none
* Stop bit : 1bit
* Flow control : none
*
- Start the application.
- Warning
* For using AWS connection, the AWS RSA certificate must be installed.
* Download the RSA certificate using the firmware upgrade. (Refer to WINC1500 Software User Guide.)
*
Compilation Information
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.
Contact Information
For further information, visit Microchip.