Macros | |
#define | BSP_MIN(x, y) ((x)>(y)?(y):(x)) |
#define | CONST const |
#define | NM_BSP_B_L_16(x) (x) |
#define | NM_BSP_B_L_32(x) (x) |
#define | NMI_API |
#define | NULL ((void*)0) |
#define BSP_MIN | ( | x, | |
y | |||
) | ((x)>(y)?(y):(x)) |
Computes the minimum value between x and y.
Referenced by spi_flash_write().
#define CONST const |
Used for code portability.
#define NM_BSP_B_L_16 | ( | x | ) | (x) |
Retain endianness of 16bit word (In the case that Host is LE)
Referenced by hif_isr(), hif_send(), m2m_ip_cb(), send(), and sendto().
#define NM_BSP_B_L_32 | ( | x | ) | (x) |
Retain endianness of 32bit word (In the case that Host is LE)
Referenced by m2m_wifi_set_static_ip(), recv(), and recvfrom().
#define NMI_API |
Attribute used to define the memory section to map Functions in host memory.
#define NULL ((void*)0) |
Void Pointer to '0' in case NULL is not defined.
Referenced by _http_client_clear_conn(), _http_client_handle_header(), _http_client_read_chuked_entity(), _http_client_recv_packet(), _http_client_request(), ASN1_GetNextElement(), ASN1_Read(), Base64_Decode(), bind(), BuildServerX509CertChain(), burn_certificates(), Cert_CompareTime(), Cert_ComputeTBSCertHash(), Cert_DecodeAlgID(), Cert_DecodeDistinguishedName(), Cert_DecodeECCPubKey(), Cert_DecodeRSAPubKey(), Cert_DecodeSignature(), Cert_DecodeSubjectPubKey(), Cert_DecodeTBSCertificate(), Cert_DecodeTime(), Cert_DecodeValidity(), Cert_DecodeX520Name(), close(), connect(), CryptoDecodeRsaPrivKey(), CryptoInternalMalloc(), CryptoX509CertDecode(), CryptoX509DeleteContext(), DecodeBase64File(), ECC_GetCurveInfo(), EcdsaBuildServerX509CertChain(), get_error_detail(), gethostbyname(), hif_receive(), hif_send(), HMAC_Vector(), http_client_close(), http_client_deinit(), http_client_get_config_defaults(), http_client_init(), http_client_register_callback(), http_client_send_request(), http_client_socket_event_handler(), http_client_socket_resolve_handler(), http_client_timer_callback(), http_client_unregister_callback(), listen(), m2m_ip_cb(), m2m_ota_abort(), m2m_ota_cb(), m2m_ota_host_file_erase(), m2m_ota_host_file_get(), m2m_ota_host_file_read_hif(), m2m_ota_host_file_read_spi(), m2m_ota_init(), m2m_ota_notif_check_for_update(), m2m_ota_notif_sched(), m2m_ota_notif_set_url(), m2m_ota_rollback(), m2m_ota_start_update(), m2m_ota_switch_firmware(), m2m_ping_req(), m2m_ssl_retrieve_hash(), m2m_ssl_retrieve_next_for_verifying(), m2m_ssl_send_certs_to_winc(), m2m_ssl_set_active_ciphersuites(), m2m_ssl_stop_retrieving(), m2m_validate_ap_parameters(), m2m_validate_scan_options(), m2m_wifi_1x_get_option(), m2m_wifi_1x_set_option(), m2m_wifi_cb(), m2m_wifi_conf_auto_rate(), m2m_wifi_configure_sntp(), m2m_wifi_connect_1x_mschap2(), m2m_wifi_connect_1x_tls(), m2m_wifi_connect_open(), m2m_wifi_connect_prepare_msg(), m2m_wifi_connect_psk(), m2m_wifi_connect_sc(), m2m_wifi_connect_wep(), m2m_wifi_default_connect(), m2m_wifi_deinit(), m2m_wifi_delete_sc(), m2m_wifi_disable_ap(), m2m_wifi_disable_roaming(), m2m_wifi_disconnect(), m2m_wifi_enable_ap_ext(), m2m_wifi_enable_dhcp(), m2m_wifi_enable_firmware_logs(), m2m_wifi_enable_roaming(), m2m_wifi_enable_sntp(), m2m_wifi_enable_XO_during_sleep(), m2m_wifi_get_connection_info(), m2m_wifi_get_system_time(), m2m_wifi_init_start(), m2m_wifi_p2p(), m2m_wifi_p2p_disconnect(), m2m_wifi_prng_get_random_bytes(), m2m_wifi_reinit_hold(), m2m_wifi_req_client_ctrl(), m2m_wifi_req_curr_rssi(), m2m_wifi_req_scan_result(), m2m_wifi_req_server_init(), m2m_wifi_request_scan(), m2m_wifi_request_scan_passive(), m2m_wifi_request_scan_ssid_list(), m2m_wifi_request_sleep(), m2m_wifi_send_crl(), m2m_wifi_send_ethernet_pkt(), m2m_wifi_set_battery_voltage(), m2m_wifi_set_cust_InfoElement(), m2m_wifi_set_device_name(), m2m_wifi_set_gain_table_idx(), m2m_wifi_set_gains(), m2m_wifi_set_lsn_int(), m2m_wifi_set_mac_address(), m2m_wifi_set_power_profile(), m2m_wifi_set_scan_options(), m2m_wifi_set_scan_region(), m2m_wifi_set_sleep_mode(), m2m_wifi_set_static_ip(), m2m_wifi_set_stop_scan_on_first(), m2m_wifi_set_system_time(), m2m_wifi_set_tx_power(), m2m_wifi_start_provision_mode_ext(), m2m_wifi_stop_provision_mode(), m2m_wifi_wps(), m2m_wifi_wps_disable(), main(), MD4_Hash(), MD4ProcessBlock(), MD5_HashSW(), nm_bsp_init(), nm_drv_init_download_mode(), nm_drv_init_hold(), nm_drv_init_start(), nm_get_firmware_full_info(), nm_get_ota_firmware_info(), nm_spi_rw(), nmi_spi_read(), nmi_spi_write(), ParsePrivKey(), ParseRsaPrivKey(), ReadServerX509Chain(), recv(), recvfrom(), RsaBuildServerX509CertChain(), secure(), send(), sendto(), set_alpn_list(), setsockopt(), SHA1_HashSW(), SHA224_HashSW(), SHA256_HashSW(), SHA512_HashSW(), Sha_HashFinish(), Sha_HashUpdate(), Socket_ReadSocketData(), socketDeinit(), spi_flexible_flash_find_section(), sslEnableCertExpirationCheck(), start_download(), stdio_serial_init(), store_file_packet(), TLS_BufferGetPos(), TLS_BufferRead(), TLS_BufferReadCurrEntry(), TLS_BufferSetPos(), TlsSrvSecFclose(), TlsSrvSecFopen(), TlsSrvSecFwrite(), TlsSrvSecWriteCertChain(), ValidateKeyMaterial(), writeRootCertEntry(), WriteTlsServerKeyMaterial(), X509_DecodeEcdsaSignature(), X509Cert_Decode(), and X509Cert_Dump().