Microchip® Advanced Software Framework

nmasic.h File Reference

This module contains NMC1500 ASIC specific internal APIs.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

Data Structures

struct  tstrGpRegs
 

Macros

#define BOOTROM_REG   (0xc000c)
 
#define EFUSED_MAC(value)   (value & 0xffff0000)
 
#define GET_CHIPID()   nmi_get_chipid()
 
#define ISNMC1000(id)   ((((id) & 0xfffff000) == 0x100000) ? 1 : 0)
 
#define ISNMC1500(id)   ((((id) & 0xfffff000) == 0x150000) ? 1 : 0)
 
#define ISNMC3000(id)   ((((id) & 0xfff00000) == 0x300000) ? 1 : 0)
 
#define M2M_ATE_FW_IS_UP_VALUE   (0xD75DC1C3) /*Also, Change this value in ATE (Burst) firmware if it will be changed here*/
 
#define M2M_ATE_FW_START_VALUE   (0x3C1CD57D) /*Also, Change this value in boot_firmware if it will be changed here*/
 
#define M2M_FINISH_BOOT_ROM   0x10add09eUL
 
#define M2M_FINISH_INIT_STATE   0x02532636UL
 
#define M2M_START_FIRMWARE   0xef522f61UL
 
#define M2M_START_PS_FIRMWARE   0x94992610UL
 
#define M2M_WAIT_FOR_HOST_REG   (0x207bc)
 
#define NMI_CHIPID   (NMI_PERIPH_REG_BASE)
 
#define NMI_PERIPH_REG_BASE   0x1000
 
#define NMI_REV_REG   (0x207ac) /*Also, Used to load ATE firmware from SPI Flash and to ensure that it is running too*/
 
#define NMI_REV_REG_ATE   (0x1048) /*Revision info register in case of ATE FW*/
 
#define NMI_STATE_REG   (0x108c)
 
#define REV(id)   (((id) & 0x00000fff ))
 
#define REV_2B0   (0x2B0)
 
#define REV_3A0   (0x3A0)
 
#define REV_B0   (0x2B0)
 
#define rHAVE_ETHERNET_MODE_BIT   (NBIT7)
 
#define rHAVE_EXT_PA_INV_TX_RX   (NBIT4)
 
#define rHAVE_LEGACY_RF_SETTINGS   (NBIT5)
 
#define rHAVE_LOGS_DISABLED_BIT   (NBIT6)
 
#define rHAVE_RESERVED1_BIT   (NBIT8)
 
#define rHAVE_RESERVED2_BIT   (NBIT9)
 
#define rHAVE_SDIO_IRQ_GPIO_BIT   (NBIT0)
 
#define rHAVE_SLEEP_CLK_SRC_RTC_BIT   (NBIT2)
 
#define rHAVE_SLEEP_CLK_SRC_XO_BIT   (NBIT3)
 
#define rHAVE_USE_PMU_BIT   (NBIT1)
 
#define rHAVE_XO_XTALGM2_DIS_BIT   (NBIT10)
 
#define rNMI_BOOT_RESET_MUX   (0x1118)
 
#define rNMI_GLB_RESET   (0x1400)
 
#define rNMI_GP_REG_0   (0x149c)
 
#define rNMI_GP_REG_1   (0x14A0)
 
#define rNMI_GP_REG_2   (0xc0008)
 

Functions

sint8 chip_apply_conf (uint32 u32conf)
 
sint8 chip_deinit (void)
 
void chip_idle (void)
 
sint8 chip_reset (void)
 
sint8 chip_reset_and_cpu_halt (void)
 
sint8 chip_sleep (void)
 
sint8 chip_wake (void)
 
sint8 cpu_halt (void)
 
sint8 cpu_start (void)
 
sint8 enable_interrupts (void)
 
sint8 get_gpio_val (uint8 gpio, uint8 *val)
 
uint32 nmi_get_chipid (void)
 
sint8 nmi_get_mac_address (uint8 *pu8MacAddr)
 
sint8 nmi_get_otp_mac_address (uint8 *pu8MacAddr, uint8 *pu8IsValid)
 
uint32 nmi_get_rfrevid (void)
 
void nmi_set_sys_clk_src_to_xo (void)
 
void nmi_update_pll (void)
 
sint8 pullup_ctrl (uint32 pinmask, uint8 enable)
 
void restore_pmu_settings_after_global_reset (void)
 
sint8 set_gpio_dir (uint8 gpio, uint8 dir)
 
sint8 set_gpio_val (uint8 gpio, uint8 val)
 
sint8 wait_for_bootrom (uint8)
 
sint8 wait_for_firmware_start (uint8)
 

#define BOOTROM_REG   (0xc000c)

Referenced by cpu_start(), and wait_for_bootrom().

#define EFUSED_MAC (   value)    (value & 0xffff0000)

Referenced by nmi_get_otp_mac_address().

#define GET_CHIPID ( )    nmi_get_chipid()
#define ISNMC1000 (   id)    ((((id) & 0xfffff000) == 0x100000) ? 1 : 0)
#define ISNMC1500 (   id)    ((((id) & 0xfffff000) == 0x150000) ? 1 : 0)
#define ISNMC3000 (   id)    ((((id) & 0xfff00000) == 0x300000) ? 1 : 0)
#define M2M_ATE_FW_IS_UP_VALUE   (0xD75DC1C3) /*Also, Change this value in ATE (Burst) firmware if it will be changed here*/
#define M2M_ATE_FW_START_VALUE   (0x3C1CD57D) /*Also, Change this value in boot_firmware if it will be changed here*/

Referenced by wait_for_bootrom().

#define M2M_FINISH_BOOT_ROM   0x10add09eUL

Referenced by wait_for_bootrom().

#define M2M_FINISH_INIT_STATE   0x02532636UL

Referenced by wait_for_firmware_start().

#define M2M_START_FIRMWARE   0xef522f61UL

Referenced by wait_for_bootrom().

#define M2M_START_PS_FIRMWARE   0x94992610UL
#define M2M_WAIT_FOR_HOST_REG   (0x207bc)

Referenced by wait_for_bootrom().

#define NMI_CHIPID   (NMI_PERIPH_REG_BASE)
#define NMI_PERIPH_REG_BASE   0x1000
#define NMI_REV_REG   (0x207ac) /*Also, Used to load ATE firmware from SPI Flash and to ensure that it is running too*/
#define NMI_REV_REG_ATE   (0x1048) /*Revision info register in case of ATE FW*/

Referenced by nm_get_firmware_info().

#define NMI_STATE_REG   (0x108c)
#define REV (   id)    (((id) & 0x00000fff ))
#define REV_2B0   (0x2B0)
#define REV_3A0   (0x3A0)
#define REV_B0   (0x2B0)
#define rHAVE_ETHERNET_MODE_BIT   (NBIT7)

Referenced by wait_for_bootrom().

#define rHAVE_EXT_PA_INV_TX_RX   (NBIT4)

Referenced by chip_apply_conf().

#define rHAVE_LEGACY_RF_SETTINGS   (NBIT5)

Referenced by chip_apply_conf().

#define rHAVE_LOGS_DISABLED_BIT   (NBIT6)

Referenced by chip_apply_conf().

#define rHAVE_RESERVED1_BIT   (NBIT8)

Referenced by chip_apply_conf().

#define rHAVE_RESERVED2_BIT   (NBIT9)
#define rHAVE_SDIO_IRQ_GPIO_BIT   (NBIT0)
#define rHAVE_SLEEP_CLK_SRC_RTC_BIT   (NBIT2)

Referenced by chip_apply_conf().

#define rHAVE_SLEEP_CLK_SRC_XO_BIT   (NBIT3)

Referenced by chip_apply_conf().

#define rHAVE_USE_PMU_BIT   (NBIT1)
#define rHAVE_XO_XTALGM2_DIS_BIT   (NBIT10)

Referenced by chip_apply_conf().

#define rNMI_BOOT_RESET_MUX   (0x1118)
#define rNMI_GLB_RESET   (0x1400)
#define rNMI_GP_REG_0   (0x149c)
#define rNMI_GP_REG_1   (0x14A0)

Referenced by chip_apply_conf().

sint8 chip_deinit ( void  )

stop the firmware, need a re-download

References M2M_ERR, M2M_SUCCESS, nm_read_reg_with_ret(), nm_write_reg(), and NMI_GLB_RESET_0.

Referenced by nm_drv_deinit().

void chip_idle ( void  )
sint8 chip_reset ( void  )
sint8 chip_reset_and_cpu_halt ( void  )
sint8 cpu_halt ( void  )
sint8 enable_interrupts ( void  )

interrupt pin mux select

interrupt enable

References M2M_SUCCESS, nm_read_reg_with_ret(), nm_write_reg(), NMI_INTR_ENABLE, and NMI_PIN_MUX_0.

Referenced by m2m_wifi_download_mode(), and nm_drv_init_start().

sint8 get_gpio_val ( uint8  gpio,
uint8 val 
)
uint32 nmi_get_rfrevid ( void  )

References M2M_SUCCESS, and nm_read_reg_with_ret().

Referenced by main().

void nmi_set_sys_clk_src_to_xo ( void  )
void nmi_update_pll ( void  )

References nm_read_reg(), and nm_write_reg().

Referenced by nmi_set_sys_clk_src_to_xo().

sint8 pullup_ctrl ( uint32  pinmask,
uint8  enable 
)
void restore_pmu_settings_after_global_reset ( void  )
sint8 set_gpio_dir ( uint8  gpio,
uint8  dir 
)
sint8 set_gpio_val ( uint8  gpio,
uint8  val 
)