Sets the MAC address from application. The WINC load the mac address from the effuse by default to the WINC configuration memory, but that function is used to let the application overwrite the configuration memory with the mac address from the host.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD16__ [2] |
uint8 | au8Mac [6] |
uint8 tstrM2mSetMacAddress::__PAD16__[2] |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2mSetMacAddress::au8Mac[6] |
MAC address array
Referenced by m2m_wifi_set_mac_address().