Microchip® Advanced Software Framework

tstrOtaInitHdr Struct Reference

This struct contains the OTA image header.

#include <m2m_types.h>

Data Fields

uint32 u32OtaMagicValue
 
uint32 u32OtaPayloadSize
 

uint32 tstrOtaInitHdr::u32OtaMagicValue
 Magic value kept in the OTA image after the

sha256 Digest buffer to define the Start of OTA Header.

uint32 tstrOtaInitHdr::u32OtaPayloadSize

The Total OTA image payload size, include the sha256 key size.