This IoT Qtouch sensor demo is configured to work with the SAM D21 Xplained Pro using the WINC1500 Wi-Fi module. It uses the following hardware:
The QTouch library was generated by QTouch Studio and the clock settings differs from other WINC1500 SAM D21 project.
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.
For further information, visit Microchip.