This IoT temperature sensor demo is configured to work with the SAM D21 Xplained Pro using the WINC1500 Wi-Fi module. It will basically report temperature sensor information to provided Android application via your home network. The Android application can be located in the android_app folder. It uses the following hardware:
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.
For further information, visit Microchip.