Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Provisioning

         Here are listed all the functions that implement the Wifi Provisioning APIs.

Functions

sint8 m2m_wifi_start_provision_mode (tstrM2MAPConfig *pstrM2MAPConfig, char *pcHttpServerDomainName, uint8 bEnableHttpRedirect)
 Asynchronous API for control of Wi-Fi provisioning functionality. More...
 
sint8 m2m_wifi_start_provision_mode_ext (tstrM2MAPModeConfig *pstrAPModeConfig, char *pcHttpServerDomainName, uint8 bEnableHttpRedirect)
 Asynchronous API for control of Wi-Fi provisioning functionality with extended options. More...
 
sint8 m2m_wifi_stop_provision_mode (void)
 Synchronous API for terminating provisioning mode on the WINC IC. More...
 

NMI_API sint8 m2m_wifi_start_provision_mode ( tstrM2MAPConfig pstrAPConfig,
char *  pcHttpServerDomainName,
uint8  bEnableHttpRedirect 
)

Asynchronous API for control of Wi-Fi provisioning functionality.

Asynchronous Wi-Fi provisioning function, which starts the WINC HTTP PROVISIONING mode.
The function triggers the WINC to activate the Wi-Fi AP (HOTSPOT) mode with the passed
configuration parameters and then starts the HTTP Provision WEB Server.

Provisioning status is returned in an event @ref M2M_WIFI_RESP_PROVISION_INFO.
Parameters
[in]pstrAPConfigAP configuration parameters as defined in tstrM2MAPConfig configuration structure. If a NULL value is passed in, the call will result in a negative error M2M_ERR_FAIL.
[in]pcHttpServerDomainNameDomain name of the HTTP Provision WEB server which others will use to load the provisioning Home page. The domain name can have one of the following 3 forms:
  • 1. "wincprov.com"
  • 2. "http://wincprov.com"
  • 3. "https://wincprov.com"

Forms 1 and 2 are equivalent, they will both start a plain http server, while form 3 will start a secure HTTP provisioning Session (HTTP over SSL connection).

Parameters
[in]bEnableHttpRedirectA flag to enable/disable the HTTP redirect feature. If Secure provisioning is enabled (i.e. the server domain name uses "https" prefix) this flag is ignored (no meaning for redirect in HTTPS). Possible values are:
  • ZERO value, which means DO NOT use HTTP Redirect. In this case, the associated device could open the provisioning page ONLY when the HTTP Provision URL of the WINC HTTP Server is correctly written on the browser.
  • Non-Zero value, means use HTTP Redirect. In this case, all http traffic (http://URL) from the associated device (Phone, PC, etc) will be redirected to the WINC HTTP Provisioning Home page.
Precondition
  • A Wi-Fi notification callback of type tpfAppWifiCb MUST be implemented and registered at startup. Registering the callback is done through passing it to the initialization m2m_wifi_init function.
  • The event M2M_WIFI_RESP_CONN_INFO must be handled in the callback to receive the requested connection info.
Warning
DO NOT use ".local" in the pcHttpServerDomainName.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
tpfAppWifiCb m2m_wifi_init M2M_WIFI_RESP_PROVISION_INFO m2m_wifi_stop_provision_mode tstrM2MAPConfig

Example

The example demonstrates a code snippet for how provisioning is triggered and the response event received accordingly.

#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
{
tstrM2MProvisionInfo *pstrProvInfo = (tstrM2MProvisionInfo*)pvMsg;
if(pstrProvInfo->u8Status == M2M_SUCCESS)
{
tstrNetworkId strNetworkId = {NULL, pstrProvInfo->au8SSID, (uint8)strlen((char*)(pstrProvInfo->au8SSID)), M2M_WIFI_CH_ALL};
tstrAuthPsk strAuthPsk = {NULL, pstrProvInfo->au8Password, (uint8)strlen((char*)(pstrProvInfo->au8Password))};
m2m_wifi_connect_psk(WIFI_CRED_SAVE_ENCRYPTED, &strNetworkId, &strAuthPsk);
printf("PROV SSID : %s\n",pstrProvInfo->au8SSID);
printf("PROV PSK : %s\n",pstrProvInfo->au8Password);
}
else
{
printf("(ERR) Provisioning Failed\n");
}
}
break;
default:
break;
}
}
int main()
{
param.pfAppWifiCb = wifi_event_cb;
if(!m2m_wifi_init(&param))
{
tstrM2MAPConfig apConfig;
uint8 bEnableRedirect = 1;
strcpy(apConfig.au8SSID, "WINC_SSID");
apConfig.u8ListenChannel = 1;
apConfig.u8SsidHide = 0;
// IP Address
apConfig.au8DHCPServerIP[0] = 192;
apConfig.au8DHCPServerIP[1] = 168;
apConfig.au8DHCPServerIP[2] = 1;
apConfig.au8DHCPServerIP[3] = 1;
m2m_wifi_start_provision_mode(&apConfig, "atmelwincconf.com", bEnableRedirect);
while(1)
{
}
}
}

References tstrM2MAPConfigExt::au8DefRouterIP, tstrM2MAPConfig::au8DHCPServerIP, tstrM2MAPConfigExt::au8DNSServerIP, tstrM2MAPConfigExt::au8SubnetMask, m2m_memcpy(), m2m_wifi_start_provision_mode_ext(), tstrM2MAPModeConfig::strApConfig, and tstrM2MAPModeConfig::strApConfigExt.

NMI_API sint8 m2m_wifi_start_provision_mode_ext ( tstrM2MAPModeConfig pstrAPModeConfig,
char *  pcHttpServerDomainName,
uint8  bEnableHttpRedirect 
)

Asynchronous API for control of Wi-Fi provisioning functionality with extended options.

Asynchronous Wi-Fi provisioning function, which starts the WINC HTTP PROVISIONING mode.
The function triggers the WINC to activate the Wi-Fi AP (HOTSPOT) mode with the passed
configuration parameters and then starts the HTTP Provision WEB Server.

Provisioning status is returned in an event @ref M2M_WIFI_RESP_PROVISION_INFO.
Parameters
[in]pstrAPModeConfigAP configuration parameters as defined in tstrM2MAPModeConfig configuration structure. A NULL value passed in, will result in a negative error M2M_ERR_FAIL.
[in]pcHttpServerDomainNameDomain name of the HTTP Provision WEB server which others will use to load the provisioning Home page. The domain name can have one of the following 3 forms:
  • 1. "wincprov.com"
  • 2. "http://wincprov.com"
  • 3. "https://wincprov.com"

The forms 1 and 2 are equivalent, they both will start a plain http server, while form 3 will start a secure HTTP provisioning Session (HTTP over SSL connection).

Parameters
[in]bEnableHttpRedirectA flag to enable/disable the HTTP redirect feature. If Secure provisioning is enabled (i.e. the server domain name uses "https" prefix) this flag is ignored (no meaning for redirect in HTTPS). Possible values are:
  • ZERO value, which means DO NOT use HTTP Redirect. In this case, the associated device could open the provisioning page ONLY when the HTTP Provision URL of the WINC HTTP Server is correctly written on the browser.
  • Non-Zero value, means use HTTP Redirect. In this case, all http traffic (http://URL) from the associated device (Phone, PC, etc) will be redirected to the WINC HTTP Provisioning Home page.
Precondition
  • A Wi-Fi notification callback of type tpfAppWifiCb MUST be implemented and registered at startup. Registering the callback is done through passing it to the initialization m2m_wifi_init function.
  • The event M2M_WIFI_RESP_CONN_INFO must be handled in the callback to receive the requested connection info.
Warning
DO Not use ".local" in the pcHttpServerDomainName.
See Also
tpfAppWifiCb m2m_wifi_init M2M_WIFI_RESP_PROVISION_INFO m2m_wifi_stop_provision_mode tstrM2MAPModeConfig
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.

Example

The example demonstrates a code snippet for how provisioning is triggered and the response event received accordingly.

#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
{
tstrM2MProvisionInfo *pstrProvInfo = (tstrM2MProvisionInfo*)pvMsg;
if(pstrProvInfo->u8Status == M2M_SUCCESS)
{
tstrNetworkId strNetworkId = {NULL, pstrProvInfo->au8SSID, (uint8)strlen((char*)(pstrProvInfo->au8SSID)), M2M_WIFI_CH_ALL};
tstrAuthPsk strAuthPsk = {NULL, pstrProvInfo->au8Password, (uint8)strlen((char*)(pstrProvInfo->au8Password))};
m2m_wifi_connect_psk(WIFI_CRED_SAVE_ENCRYPTED, &strNetworkId, &strAuthPsk);
printf("PROV SSID : %s\n",pstrProvInfo->au8SSID);
printf("PROV PSK : %s\n",pstrProvInfo->au8Password);
}
else
{
printf("(ERR) Provisioning Failed\n");
}
}
break;
default:
break;
}
}
int main()
{
param.pfAppWifiCb = wifi_event_cb;
if(!m2m_wifi_init(&param))
{
tstrM2MAPModeConfig apModeConfig;
uint8 bEnableRedirect = 1;
strcpy(apModeConfig.strApConfig.au8SSID, "WINC_SSID");
apModeConfig.strApConfig.u8ListenChannel = 1;
apModeConfig.strApConfig.u8SsidHide = 0;
// IP Address
apModeConfig.strApConfig.au8DHCPServerIP[0] = 192;
apModeConfig.strApConfig.au8DHCPServerIP[1] = 168;
apModeConfig.strApConfig.au8DHCPServerIP[2] = 1;
apModeConfig.strApConfig.au8DHCPServerIP[3] = 1;
// Default router IP
// DNS Server IP
// Subnet mask
apModeConfig.strApConfigExt.au8SubnetMask[0] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[1] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[2] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[3] = 0;
m2m_wifi_start_provision_mode_ext(&apModeConfig, "atmelwincconf.com", bEnableRedirect);
while(1)
{
}
}
}

References tstrM2MProvisionModeConfig::acHttpServerDomainName, gu8scanInProgress, hif_send(), M2M_ERR, M2M_ERR_FAIL, m2m_memcpy(), M2M_REQ_DATA_PKT, M2M_REQ_GROUP_WIFI, m2m_strlen(), M2M_SUCCESS, m2m_validate_ap_parameters(), M2M_WIFI_REQ_START_PROVISION_MODE, NULL, tstrM2MAPModeConfig::strApConfig, tstrM2MProvisionModeConfig::strApConfig, tstrM2MAPModeConfig::strApConfigExt, tstrM2MProvisionModeConfig::strApConfigExt, and tstrM2MProvisionModeConfig::u8EnableRedirect.

Referenced by m2m_wifi_start_provision_mode().

sint8 m2m_wifi_stop_provision_mode ( void  )

Synchronous API for terminating provisioning mode on the WINC IC.

This function will terminate any currently active provisioning mode on the WINC IC, returning the 
IC to idle.
Precondition
An active provisioning session must be active before it is terminated through this function.
Returns
The function returns M2M_SUCCESS for success and a negative value otherwise.
See Also
m2m_wifi_start_provision_mode

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_STOP_PROVISION_MODE, and NULL.