Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Asynchronous Events

Specific Enumeration used for asynchronous operations.

Data Structures

struct  tstrSocketAcceptMsg
 Socket accept status. More...
 
struct  tstrSocketBindMsg
 Socket bind status. More...
 
struct  tstrSocketConnectMsg
 Socket connect status. More...
 
struct  tstrSocketListenMsg
 Socket listen status. More...
 
struct  tstrSocketRecvMsg
 Socket recv status. More...
 

Enumerations

enum  tenuSocketCallbackMsgType {
  SOCKET_MSG_BIND = 1,
  SOCKET_MSG_LISTEN,
  SOCKET_MSG_DNS_RESOLVE,
  SOCKET_MSG_ACCEPT,
  SOCKET_MSG_CONNECT,
  SOCKET_MSG_RECV,
  SOCKET_MSG_SEND,
  SOCKET_MSG_SENDTO,
  SOCKET_MSG_RECVFROM,
  SOCKET_MSG_SECURE
}
 Asynchronous APIs make use of callback functions in-order to return back the results once the corresponding socket operation is completed. Hence resuming the normal execution of the application code while the socket operation returns the results. Callback functions expect event messages to be passed in, in-order to identify the operation they're returning the results for. The following enum identifies the type of events that are received in the callback function. More...
 

Asynchronous APIs make use of callback functions in-order to return back the results once the corresponding socket operation is completed. Hence resuming the normal execution of the application code while the socket operation returns the results. Callback functions expect event messages to be passed in, in-order to identify the operation they're returning the results for. The following enum identifies the type of events that are received in the callback function.

Application Use:
In order for application developers to handle the pending events from the network controller through the callback functions,
a function call must be made to the function @ref m2m_wifi_handle_events at least once for each socket operation.
See Also
bind
listen
accept
connect
send
recv
Enumerator
SOCKET_MSG_BIND 

Bind socket event.

SOCKET_MSG_LISTEN 

Listen socket event.

SOCKET_MSG_DNS_RESOLVE 

DNS Resolution event.

SOCKET_MSG_ACCEPT 

Accept socket event.

SOCKET_MSG_CONNECT 

Connect socket event.

SOCKET_MSG_RECV 

Receive socket event.

SOCKET_MSG_SEND 

Send socket event.

SOCKET_MSG_SENDTO 

Sendto socket event.

SOCKET_MSG_RECVFROM 

Recvfrom socket event.

SOCKET_MSG_SECURE 

Existing socket made secure event.